In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog [Firecracker Analyzer] Successful QFN Assembly
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
  • Author Author: ipv1
  • Date Created: 21 Feb 2015 12:59 PM Date Created
  • Views 2200 views
  • Likes 4 likes
  • Comments 7 comments
  • iot_firecracker
  • smd
  • ip_iot
  • bq25504
  • in_the_air
  • texas_instruments
Related
Recommended

[Firecracker Analyzer] Successful QFN Assembly

ipv1
ipv1
21 Feb 2015

Not a very complicated post just a few pics of the assembly.

1b824788fcbf19d45967c497d05217b1.jpg

I use some flux and copper wire strands and used it to sweep the extra solder out... The above is the result and I check with the DMM to see if any pins were bridged. They weren't image.

6453f6db76d69dfd1aeabd7a3bfeb3c3.jpg

I then moved on to solder the rest of the parts and...

image

Viola! All I need to do is mount the coil and connect the inputs and outputs. This should be fun...

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +2
    Indeed, your eyesight and steady hand are impressive. DAB
  • gadget.iom
    gadget.iom over 11 years ago +1
    Very impressive piece of hand-soldering.
  • tomaja
    tomaja over 11 years ago +1
    Your board looks great! Well done. Can you share the resistor values that you used to configure BQ25504?
Parents
  • tomaja
    tomaja over 11 years ago

    Your board looks great! Well done.

    Can you share the resistor values that you used to configure BQ25504?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • tomaja
    tomaja over 11 years ago

    Your board looks great! Well done.

    Can you share the resistor values that you used to configure BQ25504?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ipv1
    ipv1 over 11 years ago in reply to tomaja

    Thanks sir. I did a post and shared the entire schematic

     

    http://www.element14.com/community/community/design-challenges/in-the-air-design-challenge/blog/2014/12/11/firecracker-analyzer-making-the-power-pcb-with-eagle-ti-bq25504-tps62740-and-tps61200

     

    Hope this helps...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomaja
    tomaja over 11 years ago in reply to ipv1

    Yes, thanks.

    I just wanted to make sure I'm using the correct values.

    I was using the provided Excel spreadsheet for calculating resistor values. I'm not using the same values but they are close - I obviously have different voltage levels set.

     

    Dragan