In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog In-the-Air-Challenge: A sheet of laser light for 2D visualization of dust flow
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
  • Author Author: janisalnis
  • Date Created: 10 Jan 2015 6:21 PM Date Created
  • Views 1497 views
  • Likes 1 like
  • Comments 2 comments
Related
Recommended

In-the-Air-Challenge: A sheet of laser light for 2D visualization of dust flow

janisalnis
janisalnis
10 Jan 2015

Previous post: In-the-Air-Challenge: Dust counting with Beagle Bone Black and a webcam

Next post: In-the-Air-Challenge: Spending the 500 USD parts budget

 

Greetings with the New Year 2015!

I decided to compose a new blog post this week instead of adding material to the previous post. Because older blog posts people might not check over again.

 

My collegue Ilja Fescenko came up with an idea  to bounce light between two parallel mirrors allowing to recycle laser power and monitor scattered light by dust in relatively large area.

 

image

Green laser pointer 5 mW is OK, with a 30 mW laser visibility is better.

Front coated alu mirrors from an old scanner are used. One mirror is fixed. Second mirror and laser direction can be fine adjusted.

 

If both mirrors are parallel then the spots make equidistant straight pattern. One can make a parabolic pattern or a spiraling one just by tilting laser beam and one mirror.

 

A sheet of laser light shows that we are swimming is a see of dust. Dust very nicely visualizes air turbulences.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

We are testing now different filters.  HEPA13 from a vacuum cleaner, car air filters, cotton wool, electrostatic plastic spiral filter.

This method of observation from a 50 cm distance is sensitive to large dust particles. In order to see the fine dust one needs to use a macro lens (microscope) and then the observation gets smaller.

  • Sign in to reply
Parents
  • DAB
    DAB over 11 years ago

    Great idea.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    Great idea.

     

    DAB