In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog In-the-Air-Challenge: Spending the 500 USD parts budget
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
  • Author Author: janisalnis
  • Date Created: 28 Jan 2015 9:13 PM Date Created
  • Views 1323 views
  • Likes 2 likes
  • Comments 5 comments
Related
Recommended

In-the-Air-Challenge: Spending the 500 USD parts budget

janisalnis
janisalnis
28 Jan 2015

Previous post:  In-the-Air-Challenge: A sheet of laser light for 2D visualization of dust flow

Next post: In-the-Air-Challenge: Measuring CO2 levels during lectures with EXTECH CO2 monitor

 

Almoust at the last moment I compiled a list of 500 USD budget for the parts of the challenge that amounts ca 430 EUR in Jan. 2015.

 

I was very impressed that Christian Defeo at Element 14 ordered everything in a couple of hours after I sent him an email with the long list. I was mostly interested in optical CO2 meter. Price for it varied a lot at Farnell webshops in different countries. I used prices from Germany website http://de.farnell.com/ to add up to 430 EUR. And that was fine. No added VAT. Thanks a lot to Farnell.  The parts arrived to my home address with UPS truck in a couple of days. They were sent from UK location.

 

 

EXTECH INSTRUMENTS  CO100  METER, CO2, 9999PPM, 99.9%

197,71 €

http://de.farnell.com/extech-instruments/co100/meter-co2-9999ppm-99-9/dp/2081081?ost=co100&categoryId=700000005821

I will use this near-infrared non-dispersive type CO2 sensor to compare with electrochemical CO2 sensor module. NDIR sensor is callibrated against NIST traceable device, accuracy 75ppm or +-5%.

Good <800 ppm
Normal 800...1200 ppm
Bad >1200 ppm

image

First tests in the sleeping room at home showed that air was OK bad during the night 700...800ppm. In a confined space like a toilet CO2  content rised to 2000 ppm within 5 minutes. I will test the device during the lecture with ca 20 people this week.


This model has an empty battery compartment and USB hole is not populated. I will try to see if there is some place inside where analog voltage could be accessed with MSP430 or CC3200 and sent to IoT over Wi-Fi.

 

 

TEXAS INSTRUMENTS  OPA350UA  OP-VERST., HIGH-SPEED, R/R-I/O, SOIC 350

2,35 € * 4 pieces

http://de.farnell.com/texas-instruments/opa350ua/op-verst-high-speed-r-r-i-o-soic/dp/1106197

This single-supply OPamp I plan to solder this week in a home-made dust particle counter to amplify photodiode signal after schematics in paper:

A. Morpurgo et al , "A low-cost instrument for environmental particulate analysis based on optical scattering"

 

 

ANSMANN  1209-0000  STROMVERSORGUNG AC/DC, APS600 TRAVELLER

19,42 €

http://de.farnell.com/ansmann/1209-0000/stromversorgung-ac-dc-aps600-traveller/dp/1973938

Adjustable voltage 3...12V in steps. Current 600 mA. switching power supply adapter.

 

 

RASPBERRY-PI  RPI CAMERA BOARD  RPI KAMERA-BOARD, 5MP, MIT FLACHKABEL

19,25 €

http://de.farnell.com/raspberry-pi/rpi-camera-board/rpi-kamera-board-5mp-mit-flachkabel/dp/2302279?ost=RASPBERRY-PI+-+RPI+CAMERA+BOARD+-+RASPBERRY+PI+CAMERA+BOARD%2C

I would like to test this camera with RPi and compare with USB camera Logitech C270 that I use on Beagleboard/Rpi.

 

 

HAMMOND  1590B  DRUCKGUSS-GEHÄUSE, 60.5X112X31MM

7,01 € * 2 pieces

http://de.farnell.com/hammond/1590b/druckguss-geh-use-60-5x112x31mm/dp/3061590?ost=HAMMOND++1590B++ENCLOSURE%2C+INSTRUMENT%2C+ALUMINIUM

Nice shielded alu boxes.

 

 

IST INNOVATIVE SENSOR TECHNOLOGY  P1K0.0805.2P.A  SENSOR, PT1000, SMD0805, KLASSE A

7,16 €

http://de.farnell.com/ist-innovative-sensor-technology/p1k0-0805-2p-a/sensor-pt1000-smd0805-klasse-a/dp/1266951

This platin wire sensor is good for absolute callibration of other sensors.

 

 

SAMSUNG  MMCTR08GUBCH-RMLMK-FARN/KIT  SPEICHERKARTE, MICRO-SD, NOOBS, JAVA 8GB

7,58 €  * 3 pieces

http://de.farnell.com/samsung/mmctr08gubch-rmlmk-farn-kit/speicherkarte-micro-sd-noobs-java/dp/2428393

 

 

BELDEN  8723  KABEL, GESCHIRMT 2PAARIG 22AWG GRAU LF.M

1,39 €    * 5 meters

http://de.farnell.com/belden/8723/kabel-geschirmt-2paarig-22awg/dp/1218667?ost=BELDEN+-+8723+-+SHLD+CABLE%2C+2+PAIR%2C+22AWG%2C+GREY%2C+PER+M&categoryId=700000006049

Basically similar cable as used for USB.

  • Sign in to reply
Parents
  • michaelwylie
    michaelwylie over 11 years ago

    What's your elevation where the CO2 meter will be used?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • janisalnis
    janisalnis over 11 years ago in reply to michaelwylie

    Thanks for your question. My location is situated some 20 m above the see level.

    Your are right, air pressure is quite important. This can be demonstrated by the fact that  in conditions of low air pressure that happen during storms the see level can raise for almoust 1 meter above the normal level.


    NDIR optical CO2 meter measure light absorption from CO2 molecules in a given path length. So I think this meter needs to be corrected for atmospheric pressure. Do not know if it is done by some barometer internally.


    Pressure correction is probably why medical people (and car makers) like to characterise exhaled CO2 concentration in mg/m3 instead of ppm.  One can actually show that people loose weight by exhaling CO2 during physical exercises.


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to janisalnis

    I agree, but at 20 meters it will be insignificant. At about 1200 feet or so I think the error is about 5%, and of course it gets worse the higher up we go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelwylie
    michaelwylie over 11 years ago in reply to janisalnis

    I agree, but at 20 meters it will be insignificant. At about 1200 feet or so I think the error is about 5%, and of course it gets worse the higher up we go.