In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog In The Air: Episode 5 - PCB Design
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
  • Author Author: michaelwylie
  • Date Created: 2 Dec 2014 8:39 AM Date Created
  • Views 3551 views
  • Likes 4 likes
  • Comments 31 comments
  • iot_particle_counter
  • in_the_air
Related
Recommended

In The Air: Episode 5 - PCB Design

michaelwylie
michaelwylie
2 Dec 2014

Update

A Riddle: How many times in three weeks can a 1 year old child catch sick? The correct answer seems to be 3 times ...

 

Previous Posts

In The Air: Epidose 1: Introduction

In The Air: Episode 2 - Preparing for Surface Mount Work

In The Air: Episode 3 - Surface Mount Beginnings

In The Air: Episode 4 - Inductors

 

Introduction

I have finished my Booster Pack design. Figure 1 shows the top and bottom layers. Note, I am an Altium user so the display of the board layers may be unfamiliar to you if you are an Eagle user. If you are familiar with TI's Booster Packs, you'll recognize the characteristic 20 pin headers on opposing sides of the board. In my last post I discussed choosing inductors for filtering/decoupling grounds and power supplies. Accordingly, we will discuss the layout of those inductors and separating grounds for quiet sensor performance in this post.

 

Figure 1: Bottom (left) and top (right) layers for my Booster Pack design.image

 

Connecting Grounds

The general approach I have adopted is shown in Figure 3. The signal ground is like an island surrounded by the power ground, and the only way to get to the signal ground is through an inductor. The connector is on the boundary between the two grounds because the sensor requires both power and signal ground. I've created an annotated version of the board layout of Figure 1 and produced it in Figure 4. I have labelled the sensor interface, signal ground, and power ground. The power ground is directly connected to the ground of the C3200 through the Booster Pack header connections, and the signal ground is connected to the power ground through the aforementioned inductor.

 

image

Figure 3: Basic idea of the Particle Counter Booster Pack.

 

image

Figure 4: Annotated Figure 1 showing the sensor interface, signal ground, and power ground.

 

In Figure 5 I've zoomed in on the board so the signal ground is more visible, and the ground connecting inductor can be seen in the lower left (L2). You can't see the pads from the component because I used Seeedstudio Fusion for my PCBs, and Seeed Studio's design rules don't use a thermal relief pad connection by default. I'm not sure why, but that's the way it loaded. I didn't personally care for this project because I will be hand building the boards, so I left it alone. If I had loaded the rules before designing the board I may have changed it, but I loaded the design rules after. Disclaimer: especially in mass runs, use thermal reliefs on your ground connections to components as it will prevent tombstoning components during reflow.

 

image

Figure 5: Zoomed view of the top layer.

 

The 3D render of the board is shown in Figure 6. You can clearly see the pads for the inductor L2 in the lower left. I didn't bother using models for any components unless they were supplied by default, because I have no concern for height tolerances with this board. At this point in the design you may be wondering, why did he only use a single inductor, and not tie the grounds together at multiple points? The short answer is you'd be creating a ground loop, which can be a terrible problem to troubleshoot. You can look up the analysis for ground loops on PCBs, but if you only connect the grounds at one point you won't have to worry about it. You may have other issues, but a ground loop will not be one of them.

 

image

Figure 6: 3D Render of Particle Counter Booster Pack.

 

Power Supply Decoupling

In my last blog I spoke of decoupling power supplies as well as grounds. I've reproduced the schematic showing these decouplings in Figure 7.

You can see L2 is connecting the grounds, but what about L1; how is that implemented? In the same way. The inductor pads must straddle the gap between the power and signal ground. If you look back at Figure 5, you can clearly see L1 near the upper left straddling the ground boundary.

image

Figure 7: Decoupling inductors

 

Still Confused?

How about a video explaining it then!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Final Remarks

I ordered my board. It was only $10 USD from Seeed Studio for 10 pieces. No one else could compete with that price, so I had to choose them. I've got my bill of materials ready to go, I'm just waiting to hear back about the possibility of samples from TI. Every IC on this board is made by TI, which was a bit of a challenge for me. Hopefully everything can arrive in time to put it together and write some software.

  • Sign in to reply

Top Comments

  • michaelwylie
    michaelwylie over 11 years ago in reply to mcb1 +3
    Mark; Great point. Solder paste is like magic, in the sense that it can fix your mistakes. So, if you happen to slightly misplace a component, the surface tension of the liquifying solder paste will pull…
  • michaelwylie
    michaelwylie over 11 years ago in reply to ipv1 +2
    Yeah, I agree, because most people have already spent most of their budget on getting sensors.
  • michaelwylie
    michaelwylie over 11 years ago in reply to jw0752 +1
    Thanks John and Frederick!
Parents
  • tomaja
    tomaja over 11 years ago

    I finally got the time to watch the entire video image Excellent, this is very helpful to all of us who are not electronics professionals.

    I knew that vias are used to make more connected grounds (or to just transfer a trace to the other layer) but I was never thinking why do you need them on some specific positions (like those copper peninsulas.It's clear now). This challenge is an excellent place to learn more about electronics with the help of some great individuals. It's worth every second for me.

    Thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to tomaja

    Thanks Dragan;

     

    You know, the more I learn about laying out a PCB, the more I am convinced it's not really that complicated at face value. The problem is, there are a huge number of caveats just waiting. For example, why should I even care if that peninsula is grounded? With regard to the circuit I've designed, I don't care what happens to that strip of copper. But, we live in a world where our electromagnetic spectrum is crammed full. That strip is like a 1 centimeter antenna with a dielectric constant of 4 (1cm = 10 mm, Fiber glass board has a dielectric constant of about 4). If you do the calculations, that would pick up signals 15 GHz or higher. That's not a big issue, because I don't think there are any communications that commonly occur there, but could you imagine doing this calculation for every strip of copper? It's just easier to ground them.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomaja
    tomaja over 11 years ago in reply to michaelwylie

    Thanks for providing more interesting info in your reply image

    And it's Dragan pronounced as [dɾɑgɑn]. IPA pulmonic consonant chart with audio - Wikipedia, the free encyclopedia image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to tomaja

    I corrected the name, but I still have no idea how it's pronounced. Drey Gan?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomaja
    tomaja over 11 years ago in reply to michaelwylie

    It's pronounced similarly to dragon but just with a bit different R (you can click ɾ in that wiki link to hear it) and both A's are like the first A in dragon. Is't very simple to read and write as letters are almost always pronounced the same (do not depend on the context like they do in English).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to tomaja

    I think I got it. Drar-gan? Like the first R sound in Gerard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelwylie
    michaelwylie over 11 years ago in reply to tomaja

    I think I got it. Drar-gan? Like the first R sound in Gerard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • tomaja
    tomaja over 11 years ago in reply to michaelwylie

    Hehe, except there's no second R. More like Dra-gan. But never mind that, not too important image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to tomaja

    I think I got it image