In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog In The Air: Episode 7 - Still Getting Ready for PCBs
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
  • Author Author: michaelwylie
  • Date Created: 19 Dec 2014 1:24 AM Date Created
  • Views 1320 views
  • Likes 4 likes
  • Comments 5 comments
  • iot_particle_counter
  • in_the_air
Related
Recommended

In The Air: Episode 7 - Still Getting Ready for PCBs

michaelwylie
michaelwylie
19 Dec 2014

Previous Posts:

In The Air: Epidose 1: Introduction

In The Air: Episode 2 - Preparing for Surface Mount Work

In The Air: Episode 3 - Surface Mount Beginnings

In The Air: Episode 4 - Inductors

In The Air: Episode 5 - PCB Design

In The Air: Episode 6 - Getting Ready For PCBs

 

Update

Guess what came in the mail? Two things. First, my boards have arrived, and I've taken a picture to show you (Figure 1). It doesn't matter how many boards I've designed, when they arrive it's always like Christmas.

 

image

Figure 1: The Particle Counting PCB.

 

Secondly, the samples and the Newark order have not arrived yet. It's a pretty busy time of year, so they may not show up for a little while. I'm still working through Shabaz's (@shabaz) tutorials on the CC3200 (part1, part2). When I installed all the software and I plugged in my CC3200 Launch Pad the USB connection did not enumerate as a virtual com port, as it does in the tutorial. I think it may be due to a newer version of the software I installed. Anyway, if you experience this as well, you need to right click the CC3200LP items under the Universal Serial Bus Controllers in Device Manager and select properties. In these properties you need to set the device to use VCP. I'm at work right now, and I don't have the Launch Pad here, so I can't get a screen shot until later. This was pretty straight forward, and I found it by messing around with the settings.

  • Sign in to reply
Parents
  • shabaz
    shabaz over 11 years ago

    Hi Michael,

     

    I just saw your post, as you say it may be related to newer software. I didn't need to make changes in Device Manager. It might also be related to types of USB chipset on the PC perhaps. I used ports that were 3.0 compatible in 2.0 mode. With other (non-TI) boards in the past I found I needed to use USB 2.0-only ports.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 11 years ago

    Hi Michael,

     

    I just saw your post, as you say it may be related to newer software. I didn't need to make changes in Device Manager. It might also be related to types of USB chipset on the PC perhaps. I used ports that were 3.0 compatible in 2.0 mode. With other (non-TI) boards in the past I found I needed to use USB 2.0-only ports.