In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog In The Air: Episode 8
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
  • Author Author: michaelwylie
  • Date Created: 16 Feb 2015 11:15 PM Date Created
  • Views 1299 views
  • Likes 4 likes
  • Comments 3 comments
  • iot_particle_counter
  • in_the_air
Related
Recommended

In The Air: Episode 8

michaelwylie
michaelwylie
16 Feb 2015

Previous Posts:

In The Air: Epidose 1: Introduction

In The Air: Episode 2 - Preparing for Surface Mount Work

In The Air: Episode 3 - Surface Mount Beginnings

In The Air: Episode 4 - Inductors

In The Air: Episode 5 - PCB Design

In The Air: Episode 6 - Getting Ready For PCBs

In The Air: Episode 7 - Still Getting Ready for PCBs

 

Update

I have received some more parts recently, but unfortunately, I am still missing critical components. I'll provide some history of the procurement here so that you can understand why I have not written a blog post in over a month.

  • I placed my first order very quickly after being selected as a competitor. My design was going to include many surface mount components, so I ordered the appropriate tools as part of the budget. Everything arrived very quickly.
  • My circuit board design was complete, and I was ready to order components.. I placed my second order on Dec 4, 2014. Christmas came and went and I hadn't received any parts, but I figured that was typical of the holiday season. I have been in contact with Christian Defoe doctorcdf27 throughout the process. I'd like to thank Christian for doing all that he could up to this point to ensure I get my parts in time.
  • I also ordered some passives from Wurth, and Fed Ex says the parts have arrived, but I did not get them. I ordered some design kits and received those, but the headers and terminal blocks never arrived. Simon at Wurth remedied the situation and the parts are on their way again.
  • I used all TI ICs in my design because they are a sponsor of the challenge. I sampled those parts through E14 from TI, but they never showed up. Christian fixed this by ordering what parts he could from Newark for me, and I sampled the rest from TI under my own name.

 

Latest Work

 

I made a video showing the population procedure. I've only placed the components I have thus far.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Here's a photo of the board BEFORE cleaning up the extra solder from the reflow process.

image

 

Here are two pictures showing the board after removing excess solder. I've plugged it into the launchpad to show how it will look in the end.

 

imageimage

 

I have not powered my board yet because I was only able to sample a single piece for some components. If I destroy the component, it's game over for me! It's also possible I would damage the launchpad. I lack a current limiting power supply, so I'll have to come up with a solution.

 

Verification

As part of my last order I got an arbitrary function generator (AFG). I thought about it for quite a while, and decided that I indeed should get it. Hooking up a sensor up to an embedded system seems simple, but before anyone should consider doing so, the embedded system needs to be tested with a known signal. Sometimes this is as easy as using a DC voltage source, but for a particle counting system waveforms are required to test the electronics. So, I ordered the AFG because I need to verify that the system works.

 

I'll hopefully be testing the system soon.... Stay tuned!


  • Sign in to reply
Parents
  • jw0752
    jw0752 over 11 years ago

    Hi Michael,

    It was nice to see how your project is progressing. It is too bad that the supplies that you need have not come in a timely manner. This has to be very frustrating. I know as just a bystander it is frustrating to try to follow some of these interesting projects that can't be finished because of poor response from the suppliers, shipping problems, or other problems. I hope you hang in there as I am interested in seeing your conclusion.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 11 years ago

    Hi Michael,

    It was nice to see how your project is progressing. It is too bad that the supplies that you need have not come in a timely manner. This has to be very frustrating. I know as just a bystander it is frustrating to try to follow some of these interesting projects that can't be finished because of poor response from the suppliers, shipping problems, or other problems. I hope you hang in there as I am interested in seeing your conclusion.

    John