In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog In The Air: Episode 9: Pump Control
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
  • Author Author: michaelwylie
  • Date Created: 22 Feb 2015 5:46 AM Date Created
  • Views 2407 views
  • Likes 5 likes
  • Comments 6 comments
  • iot_particle_counter
  • pwm
  • in_the_air
Related
Recommended

In The Air: Episode 9: Pump Control

michaelwylie
michaelwylie
22 Feb 2015

Previous Posts:

In The Air: Epidose 1: Introduction

In The Air: Episode 2 - Preparing for Surface Mount Work

In The Air: Episode 3 - Surface Mount Beginnings

In The Air: Episode 4 - Inductors

In The Air: Episode 5 - PCB Design

In The Air: Episode 6 - Getting Ready For PCBs

In The Air: Episode 7 - Still Getting Ready for PCBs

In The Air: Episode 8

 

Update

Board is complete, and not destroying components ... anymore. I went through 4 inductors troubleshooting this one. I really should get a current limited supply. Here's a picture of the inductor graveyard.

image

I also lost a buck regulator in the process. In fact, it was the buck regulator that originally caused the first inductor to be destroyed. There was a short from power to ground under the regulator, and that's how the first inductor got destroyed. Then, somehow, the power supply leads got reversed, and that took out another inductor. Finally, four inductors later, the board is working. These inductors are quite handy when prototyping; they act like a fuse of sorts.

 

Oops


Below is the Booster Pack Header pin out. I made a mistake in my original layout, because I used the I²C lines, P1 - Ref 9 & 10, and I used the PWM available from P4 - Ref 1. I'm using the PWM signal to drive a pump. If you examine the Dev Pin numbers, you'll notice that the I2C_SDA pin is the same as the PWM pin for Ref 1. The * indicates a hardware modification is required to connect the PWM, but you can't use both at the same time. So, I made a hardware change; that is, I cut the trace for the PWM from Dev Pin 2 and soldered in a jumper wire for Dev Pin 64 instead.

 

Figure 1: CC3200 Header Pin Outimage

 

Figure 2 shows my modification. It's a yellow wire at the bottom of the figure. If you look closely you can also see where I cut the trace beside the resistor I jumpered to. There is a second modification as well, but that's just a voltage supply mod.

 

image

Figure 2: I²C & PWM Conflict Modification. The yellow wire at the bottom of the figure is the jumper.

 

Pump Control

 

Having fixed the hardware issue, the software to control PWM was next. The CC3200 offers example code from the SDK for PWM control. I started with that example and modified it to work for Pin 64 instead of the I²C pins. I started with the wlan example and started bringing in all the functions from the PWM example that I required:

  • void InitPWMModules()
  • void DeInitPWMModules()
  • void SetupTimerPWMMode(unsigned long ulBase, unsigned long ulTimer, unsigned long ulConfig, unsigned char ucInvert)
  • void UpdateDutyCycle(unsigned long ulBase, unsigned long ulTimer, unsigned char ucLevel)

 

You'll likely have to add a few includes and a few defines, but it's relatively simple.

 

pinmux.c should have these lines in it:

//
// Enable Peripheral Clocks
//
MAP_PRCMPeripheralClkEnable(PRCM_GPIOA1, PRCM_RUN_MODE_CLK);

//
// Configure PIN_64 for GPIOOutput
//
MAP_PinTypeGPIO(PIN_64, PIN_MODE_0, false);
MAP_GPIODirModeSet(GPIOA1_BASE, 0x2, GPIO_DIR_MODE_OUT);

 

Your main program will have something like this implemented:

InitPWMModules();
UpdateDutyCycle(TIMERA2_BASE, TIMER_B, pwmValue);

 

I wanted to be able to control the PWM duty cycle from one of the kit's switches, so I used the button_if example from the common directory in the SDK, and this is where all my problems started. I could read the button pin, but not get any interrupt from it. I searched for quite a while on this topic, and I happened upon a forum where a guy said that in order for his interrupts to work he had to use UniFlash to completely clear the ROM on his board. So, I did this and the interrupts now work. Apparently, there can be conflict between using the OSI examples and mixing them with the examples from common. I'm not sure what happens or why, but just be warned.

 

Demo

 

Here's a video of the interrupt driven PWM control working.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

And a video of my modification explanation.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Until next time ...

  • Sign in to reply

Top Comments

  • michaelwylie
    michaelwylie over 11 years ago in reply to clem57 +1
    Thanks. It's funny you should mention that. In the lab where I studied we would work with small stuff all the time (high frequency work). One of the students who worked there before me went to med school…
  • michaelwylie
    michaelwylie over 11 years ago in reply to tomaja +1
    Some of them weren't obvious. I did a continuity check across it to test. Too much rework can be a problem, sometimes you gotta get a new board ...
  • fvan
    fvan over 11 years ago

    Glad you got your board and pump to work, well done image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<