In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Files Components - In the Air Challenge
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
Related
Recommended

Components - In the Air Challenge

Components to be used by the competitors in the In the Air Challenge.

  • in
  • components
  • the
  • air
  • challenge
joeman
joeman
  • 19 Sep 2014
  • 0 Downloads
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 12 years ago in reply to shabaz +2
    element14 have one of these. Pre Heater Pre Heater which I'm told makes it a lot easier when you use a Hot Air reworking station and are soldering parts on. Mark
  • michaelkellett
    michaelkellett over 11 years ago in reply to ravi_butani +2
    I have one of these and it's quite useful but it heats up much too fast for reliable soldering of parts using solder paste. The temperature control is very rough and ready. If you are trying to use it…
  • ravi_butani
    ravi_butani over 11 years ago +2
    Hii doctorcdf ... does we need to put sample request in TI and WE or element14 for component listed in this document... regards, Ravi
Parents
  • hlipka
    hlipka over 12 years ago

    Wow, apart from the TMP112 everything listed here is in QFN or BGA package. If its really a requirement for the challenge this will be fun for everybody. Or will there be evaluation boards available (the LMP910x0 ones look interesting)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to hlipka

    Hi!

     

    I think solder paste will be mandatory as one of the component purchases. Either that, or use evaluation boards. Will be interesting to see what methods people use to solder these. michaelkellett has mentioned using a hot plate to solder these. Another method I've heard is a hot air gun, but that sounds more difficult to get right without toasting the chip, but I could be wrong.

    Flux would be another good thing to purchase (and tweezers, and a magnifier and very fine solder, and desoldering braid, and spare chips to experiment with) and then they may be hand-solderable with a fine tipped soldering iron (some youtube videos show a few procedures), if the pads are created with space to place the soldering iron tip right up against the edge of the ic and exposed copper on the pcb.

     

    (There is an SMT discussion here that may help people).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to shabaz

    Here's a picture of the processor on the board, I won't have time to do some step by step video or pictures for a couple of weeks.

    image

     

    The chip is a bit hidden by the test connector. You can see the sparse pinning on the two Lattice 132 pin footprints. The pads are about 0.27mm diameter.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to shabaz

    element14 have one of these.

    Pre HeaterPre Heater which I'm told makes it a lot easier when you use a Hot Air reworking station and are soldering parts on.

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to mcb1

    Hi Mark,

     

    Thanks for finding this. I've just ordered one, it's a good price It might need some sort of jig made to position the PCB over the hot spot, but I can manage that.

    It's so low cost it's worth the attempt anyway, even if I can't get used to this method. I I have some thermocouples so I can measure the temperature as Michael mentioned,

    and also ordered a few of the the cheapest QFN parts with a center pad too, to practice with.

    Now I'm really looking forward to trying this out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to shabaz

    It comes with two magnetic board holders, so save the looking.

     

    I haven't used mine, but the person I suggested it to (he got tired of waiting for a cheap chinese version), said its brilliant for desoldering parts, since you preheat from the bottom, and a bit more on top, and its off.

     

    Yes it's a very cheap tool to add to your collection at NZ $93.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ravi_butani
    ravi_butani over 11 years ago in reply to mcb1

    I think this preheater can be used as hot plate soldering for smd parts as it support 350C temperature... With this preheater We need solder paste and stencils for different smd footprints....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ravi_butani
    ravi_butani over 11 years ago in reply to mcb1

    I think this preheater can be used as hot plate soldering for smd parts as it support 350C temperature... With this preheater We need solder paste and stencils for different smd footprints....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett over 11 years ago in reply to ravi_butani

    I have one of these and it's quite useful but it heats up much too fast for reliable soldering of parts using solder paste. The temperature control is very rough and ready. If you are trying to use it for re-flowing paste then initially set the temperature quite low - (check up the paste spec) to drive off the volatile stuff. Then turn the temperature up to the reflow  temperature. Using  a thermocouple to monitor temperate is a really good idea if you can. I get better results with the big iron hotplates because they heat up more slowly. If you don't drive the volatile stuff out of the paste it can end up boiling away under the chip for ages and you get voids or even unsoldered pins.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to michaelkellett

    I would agree that it would be too fast.

     

    I'm wondering if a project to alter its characteristics could be worthwhile, using a Hotplate as the interface to the board.

    There is a very good profile in the EnOcean specs (TCMxx from memory) which is probably a good starting point.

     

    Regardless it's certainly a very good starting point, and is priced right.

     

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to mcb1

    I hadn't thought about controlling the temperature - I have a salvaged temperature controller somewhere - I must dig it out.

    You can buy a name brand controller from Farnell for £100 - £150, or one from ebay for £30 - I wonder if you can build one for less, ST Nucleo board, solid state relay, display, box, thermocouple and input amp - it would be very tight and a lot of effort - I'll look for the old one.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to michaelkellett

    MK

    I was thinking about interfacing a simple temperature probe, to some form of micro and controlling the heating element.

    I haven't opened up the one linked above, so I'm not sure if it has any sort of feedback loop, or the method used to interrupt the element (if at all).

     

    Surely an SSR, Micro and Temperature Probe isn't going to add very much at all to the build, and could even be a standalone device.

     

    I've seen some of the ovens, and while I'm not suggesting this is for large boards or BGA's, its probably suitable for a few one off situations.

    Like it or not SMD is here to stay, so we better get the tools to deal with it.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to mcb1

    It's more the time it takes to get such things going. I've found the reclaimed controller - it's a CAL9500 - can work with PTR or thermocouples. One SSR output and two relay outputs. I've often found the least cost route (including the cost of time) is to use an old PC as the controller - I have a PC controlled fridge.

     

    MK