In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Files Components - In the Air Challenge
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
Related
Recommended

Components - In the Air Challenge

Components to be used by the competitors in the In the Air Challenge.

  • in
  • components
  • the
  • air
  • challenge
joeman
joeman
  • 19 Sep 2014
  • 0 Downloads
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to shabaz +2
    element14 have one of these. Pre Heater Pre Heater which I'm told makes it a lot easier when you use a Hot Air reworking station and are soldering parts on. Mark
  • michaelkellett
    michaelkellett over 11 years ago in reply to ravi_butani +2
    I have one of these and it's quite useful but it heats up much too fast for reliable soldering of parts using solder paste. The temperature control is very rough and ready. If you are trying to use it…
  • ravi_butani
    ravi_butani over 11 years ago +2
    Hii doctorcdf ... does we need to put sample request in TI and WE or element14 for component listed in this document... regards, Ravi
Parents
  • hlipka
    hlipka over 12 years ago

    Wow, apart from the TMP112 everything listed here is in QFN or BGA package. If its really a requirement for the challenge this will be fun for everybody. Or will there be evaluation boards available (the LMP910x0 ones look interesting)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to hlipka

    Hi!

     

    I think solder paste will be mandatory as one of the component purchases. Either that, or use evaluation boards. Will be interesting to see what methods people use to solder these. michaelkellett has mentioned using a hot plate to solder these. Another method I've heard is a hot air gun, but that sounds more difficult to get right without toasting the chip, but I could be wrong.

    Flux would be another good thing to purchase (and tweezers, and a magnifier and very fine solder, and desoldering braid, and spare chips to experiment with) and then they may be hand-solderable with a fine tipped soldering iron (some youtube videos show a few procedures), if the pads are created with space to place the soldering iron tip right up against the edge of the ic and exposed copper on the pcb.

     

    (There is an SMT discussion here that may help people).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to shabaz

    I've got my boards ( a bit later than I hoped) with the 0.5mm pitch BGAs. I've so far soldered 2 of the 64 pin parts down (STM32F100RBH6B). One I broke off to look at the quality of the joints - the other is working as far as I can test it without completing the board.

    The tools required for this were: microscope, sticky flux, tweezers, thermocouple based thermometer, Kapton tape and the domestic hotplate I posted a picture of in the other thread.

    If any one is interested in actually doing this I'll try to find time to post some pictures.

    (BTW the biggest expense so far is the boards with 6 layers and  0.075mm track and gap rules - about £400 min order quantity. I have a feeling that it is possible to layout  a board for the Lattice 132 pin 0.5mm BGA using OSH Park's 0.125mm process because Lattice leave some rows unpopulated which makes 'escape' tracks much easier.)


    MK

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to michaelkellett

    Wow, that would be very useful to see, indeed!

     

    For those interested:

    This is the page with the hot plate photo, scroll down to the comments section.

    Also, this page has some discussions in the comments section too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 11 years ago in reply to michaelkellett

    Wow, that would be very useful to see, indeed!

     

    For those interested:

    This is the page with the hot plate photo, scroll down to the comments section.

    Also, this page has some discussions in the comments section too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett over 11 years ago in reply to shabaz

    Here's a picture of the processor on the board, I won't have time to do some step by step video or pictures for a couple of weeks.

    image

     

    The chip is a bit hidden by the test connector. You can see the sparse pinning on the two Lattice 132 pin footprints. The pads are about 0.27mm diameter.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to shabaz

    element14 have one of these.

    Pre HeaterPre Heater which I'm told makes it a lot easier when you use a Hot Air reworking station and are soldering parts on.

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to mcb1

    Hi Mark,

     

    Thanks for finding this. I've just ordered one, it's a good price It might need some sort of jig made to position the PCB over the hot spot, but I can manage that.

    It's so low cost it's worth the attempt anyway, even if I can't get used to this method. I I have some thermocouples so I can measure the temperature as Michael mentioned,

    and also ordered a few of the the cheapest QFN parts with a center pad too, to practice with.

    Now I'm really looking forward to trying this out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to shabaz

    It comes with two magnetic board holders, so save the looking.

     

    I haven't used mine, but the person I suggested it to (he got tired of waiting for a cheap chinese version), said its brilliant for desoldering parts, since you preheat from the bottom, and a bit more on top, and its off.

     

    Yes it's a very cheap tool to add to your collection at NZ $93.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ravi_butani
    ravi_butani over 11 years ago in reply to mcb1

    I think this preheater can be used as hot plate soldering for smd parts as it support 350C temperature... With this preheater We need solder paste and stencils for different smd footprints....