IoT on Wheels Design Challenge
  • Challenges & Projects
  • Design Challenges
  • IoT on Wheels Design Challenge
  • More
  • Cancel
IoT on Wheels Design Challenge
Blog CycleOps Blog #4 - Finally We Get To IoT!
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
  • Author Author: RParkerE
  • Date Created: 17 Oct 2017 7:49 PM Date Created
  • Views 1054 views
  • Likes 4 likes
  • Comments 3 comments
  • ionic
  • android development
  • android iot
  • ios iot
  • ios app
  • ios development
  • mobile app
  • iot design
  • iot bicycle
  • android app
  • iotonwheels
Related
Recommended

CycleOps Blog #4 - Finally We Get To IoT!

RParkerE
RParkerE
17 Oct 2017

PREVIOUS BLOG

NEXT BLOG

IoT Platforms and Connections

image

Choosing A Platform

To connect my bike lock to the Internet of Things, I needed to find a platform which allowed me to easily upload and control the data that I push from the STM32 Nucleo board to the Internet and eventually the users device. After looking into multiple options, such as Amazon's AWS, Microsoft's Azure, and IBM's Watson/Bluemix. Based on my experiences with the sign up processes and amount of documentation I chose to use Microsoft's platform moving forward. After making this choice I was also lucky enough to have $100 in free Microsoft Azure credit given to me at a tech talk I attended.

 

You can find more information about all 3 platforms with the following links:

IBM Watson/Bluemix

Amazon AWS

Microsoft Azure

 

Microsoft Azure and IoT Capabilities

I started connecting to Microsoft Azure by following the documentation. I first created an IoT Hub, and Event Hub and a Device Provisioning Service, and linked the three services/hubs together. Once this was done I went into the IoT Hub and added a device, which allowed me to get my connection string and keys which I will use to connect the STM32 Nucleo to the IoT Hub.

image

I will now be focusing my work on linking my STM32 Nucleo, sending data from the sensor board, and pushing that through to my Ionic application.

 

 

Ionic Code

As requested I have made a GitHub repository for my Ionic Application. I have opted to only upload the files that I am editing, as GitHub limits each upload to only 100 files and it would take me awhile to upload the entire project, however I will add a detailed ReadMe file that will allow one to add the proper supporting files and libraries used to get a working and functioning app.

  • Sign in to reply

Top Comments

  • RParkerE
    RParkerE over 8 years ago in reply to e14phil +2
    Phil, I was lucky enough to get a tutorial of the Azure platform when receiving my credit, so I am finding it useful. Also the fact that ST Micro has a library that allows the STM32 L476RG board to communicate…
  • e14phil
    e14phil over 8 years ago +1
    Hey Parker, I also have some Azure credit, how are you finding it? I was going to just use it as webspace. Also that comic at the top is too close to home for comfort haha!
  • carmelito
    carmelito over 8 years ago in reply to RParkerE +1
    Nice blog post.. Just a word of caution on using Azure IoT, I was also one of those lucky folks who was given 100$ credit to try out Azure IoT about 3 months ago and can only advice you to keep an eye…
Parents
  • e14phil
    e14phil over 8 years ago

    Hey Parker,

     

    I also have some Azure credit, how are you finding it?

    I was going to just use it as webspace.

     

    Also that comic at the top is too close to home for comfort haha!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RParkerE
    RParkerE over 8 years ago in reply to e14phil

    Phil,

     

    I was lucky enough to get a tutorial of the Azure platform when receiving my credit, so I am finding it useful. Also the fact that ST Micro has a library that allows the STM32 L476RG board to communicate directly with the platform is also part of the reason I went this direction.

     

    And yes the comic I found very relatable and scarily true!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • carmelito
    carmelito over 8 years ago in reply to RParkerE

    Nice blog post..

    Just a word of caution on using Azure IoT, I was also one of those lucky folks who was given 100$ credit to try out Azure IoT about 3 months ago and can only advice you to keep an eye on the dashboard, and have the things that you don't need shutdown as I have seen the credit get used up at an exponential rate after a couple of weeks..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • carmelito
    carmelito over 8 years ago in reply to RParkerE

    Nice blog post..

    Just a word of caution on using Azure IoT, I was also one of those lucky folks who was given 100$ credit to try out Azure IoT about 3 months ago and can only advice you to keep an eye on the dashboard, and have the things that you don't need shutdown as I have seen the credit get used up at an exponential rate after a couple of weeks..