IoT on Wheels Design Challenge
  • Challenges & Projects
  • Design Challenges
  • IoT on Wheels Design Challenge
  • More
  • Cancel
IoT on Wheels Design Challenge
Blog IOT on Wheels Design Challenge - Smart Drive - Introduction - Blog #1
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
  • Author Author: vlasov01
  • Date Created: 20 Sep 2017 2:08 AM Date Created
  • Views 1698 views
  • Likes 6 likes
  • Comments 7 comments
  • iot on wheels design challenge
  • iot on wheels
  • ride
  • iot design
  • iot bicycle
  • smartdrive
Related
Recommended

IOT on Wheels Design Challenge - Smart Drive - Introduction - Blog #1

vlasov01
vlasov01
20 Sep 2017

IOT on Wheels Design Challenge - Smart Drive - Project Index

Smart Drive

Introduction

Thank you for stopping at my first blog post for IoT on Wheels Design Challenge!

I like exploring different ideas and I'm very happy that the idea of my project has been selected for this challenge.

STM32L4 is a new MCU for me. It has a very impressive specs in terms of performance and power consumption. I think it should be a good fit for my Smart Drive project, where processing power as important as power consumption..

Synopsis

I'd like to build a collaborative system, that will connect different participants on the wheels. They will be able to share data collected during their travels, Especially valuable will be data related to events like emergency breaking, collisions, crashes, this data will be linked to the position, speed and other information collected from the sensors.

 

Description - What and Why

There are different types of wheals on the road. You may ride your bike, drive a car, commute by bus/train or getting around in a wheelchair. The road may be full of surprises. Not all of them are good for you.. It will be great to be prepared for unexpected. How about to be advised by a friend or community in advance?

image

These drawing illustrates a high level idea of sharing information with community, where all participants going to benefit from the shared data. On-board Processing component is using on-board sensors and data shared by community to generate real-time alerts. These alerts then get passed to the community.

 

How

image

These drawing illustrates how real-time processing should work. The real-time processing is enabled by on-board components.Once a condition is detected the notification will be created. In case of "false alarm" it will be manually suppressed. In addition to sharing valid alerts with community emergency contacts may be notified in case of dangerous situations.

The components provided by Element14 and the sponsor will be complemented by a GNSS receiver, a buzzer, lights, rechargeable battery and a button.

Key Principles

1. Protect privacy (not share any personal identifiable information)

2. Keep it open and transparent

     a. Open APIs for data sharing

     b. Open source (all code is open source)

     c. Open for ideas

3. Do not distract from the road (minimize false positives as much as possible)

4. Keep it simple (interface should be as simple as possible)

 

Feedback

Thank you for being with me so far. As I'm still early in the design process you can very well influence it. I'd like to ask for a constructive feedback.

How do you feel about the idea?

Tell me about your experience of being in a dangerous situation while on the wheels.

What do you like and dislike about the design?

What would you like to change in the design?

How would you feel about sharing this type of information (without providing any personal details)?

I'll really appreciate if you can provide some input.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +3
    Nice start, I look forward to seeing you flesh out the design and get into the implementation. DAB
  • janousv@stm
    janousv@stm over 8 years ago in reply to vlasov01 +1
    Thank you very much for clarification. I have some additional question about the Fall detection still. This MotionFD library was designed to detect the falls when a person is walking, standing and suddenly…
Parents
  • janousv@stm
    janousv@stm over 8 years ago

    Promising progress, I like it.  I am very curious to understand the sensing features of this project, in particular, the way you plan to detect breaking, emergency breaking, abnormal road condition and the fall detection, since the fall detection example available in ST SW package is a free fall detection caused by the Earth gravity for example when a device would fall freely from a table . Thx for comments. Vladimir

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vlasov01
    vlasov01 over 8 years ago in reply to janousv@stm

    Thank you for the feedback. I've described my exploration of Fall Detection in the following post: IOT on Wheels Design Challenge - Smart Drive - Exploring MEMS board X-NUCLEO-IKS01A2 with Unicleo-GUI - Blog #3

    I still need to explore breaking/emergency breaking detection options as I can use X-NUCLEO-IKS01A2 sensors as well GPS velocity data. I hope to detect abnormal road condition by reading data from X-NUCLEO-IKS01A2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vlasov01
    vlasov01 over 8 years ago in reply to janousv@stm

    Thank you for the feedback. I've described my exploration of Fall Detection in the following post: IOT on Wheels Design Challenge - Smart Drive - Exploring MEMS board X-NUCLEO-IKS01A2 with Unicleo-GUI - Blog #3

    I still need to explore breaking/emergency breaking detection options as I can use X-NUCLEO-IKS01A2 sensors as well GPS velocity data. I hope to detect abnormal road condition by reading data from X-NUCLEO-IKS01A2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • janousv@stm
    janousv@stm over 8 years ago in reply to vlasov01

    Thank you very much for clarification. I have some additional question about the Fall detection still. This MotionFD library was designed to detect the falls when a person is walking, standing and suddenly falls down (e.g. social alarm for elderly people). In your case I believe you consider it for bike riding fall detection, maybe for the wheelchairs but not at all for cars. It will be quite interesting to see how the MotionFD can handle these cases while you experiment, I would expect much different dynamics of a bike rider vs. MotionFD capabilities. Thank you for additional comments and looking forward to see your next blog post.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vlasov01
    vlasov01 over 8 years ago in reply to janousv@stm

    Thank you for the insight! I'm getting close for the outdoor testing. I need to implement some offline capabilities as WiFi connection has a limited range.I'll definitely share my results.