About this Challenge | Dates | The Judges | The Kit | The Prizes | Technical Resources | Example Application | Terms & Conditions | The Challengers | The Winners
Join us, in congratulating the winners of the Just Encase with Hammoned Enclosures
Make IoT work in industry, using Infineon’s low-power compute, connectivity, and sensing technology!
68 Blogs, 28 Videos and a whole lot of blood sweat and tears.
The winners will win the following prizes and anyone who hit the Finisher criteria will get the finisher prize.
Winners will be sent prizes to the address on their application and will be contacted by danzima
The Winners
Grand Prize Winner
milosrasic98 - OrbWeaver Rover
/search?q=just%20encase#serpauthor=46770&serpcategory=blog&serpgroup=354&serpsort=date%20desc
- Showing the case working in different environments was good.
- the cases where well utilized with all the components used in the enclosures.
- The data collected was shown well.
- The complexity and design of this project was well thought through. The sensor alone was complexed enough but to add the rover to this project put it over the top.
- The report was easy to follow, well laid out, and was a fun read.
- One thing I didn’t like to see in the report was, they mentioned to use Loctite to seal holes. this will destroy the plastic and should not be used on our plastic enclosures.
- This guy is a stellar designer. Very impressed he was able to turn our box into a fully functioning rover!
- He also made a temp, humidity and air pressure logger and showed the enclosure being used outside in the elements which shows its intended function.
- I also liked the rover just because it was so thorough with nice photos and videos.
- So different and an unusual to use the enclosure as the main body of a rover.
- Googly eyes for style points.
Runner Up Winner
christopherskala – Garden Pond Monitor /search?q=just%20encase#serpauthor=244264&serpcategory=blog&serpgroup=354&serpsort=date%20desc
- Use of the case in the elements was good.
- The report was easy to follow and I enjoyed read it.
- The data collected was display well
- It also solved a problem that lots of people have.
- This project was well thought out and showed our cases provided protection against the elements
- A complicated project that can measure Water temp at various depths, Total dissolved solids, Water level, pH, Air temp, humidity, light levels, air pressure
- I love the testing he did on the enclosures. The one passed 96+ hr submersion test!
- Very clear results in conclusion. The system works and is useful
Pratyush_ceteb – Wind Turbine Monitoring /search?q=just%20encase#serpauthor=221647&serpcategory=blog&serpgroup=354&serpsort=date%20desc
- The use of the pole mount kit was great.
- Good use of the enclosure in the elements.
- The blog was a good read but I would like to see more of the data collected shown.
- All around good project, but it left me wanting more from the blog.
- Neat project measuring conditions of a wind turbine during operation.
- I liked that he used the pole mount straps and did some vibration testing on the enclosures during use.
- He also did some basic water testing which I liked.
- DougW - Just Encase Solar Super Capacitor Weather Station
- Simple project to monitor outdoor temperatures, but is solar powered and can send data via Bluetooth.
- Well described and executed, nice finished look on end result. Clearly operates as intended.
- Tested the enclosure outside and good comments on the benefits of our IP rating, etc..
Finishers:
Pratyush_ceteb – Wind Turbine Monitoring
/search?q=just%20encase#serpauthor=221647&serpcategory=blog&serpgroup=354&serpsort=date%20desc
DougW - Just Encase Solar Super Capacitor Weather Station
/search?q=just%20encase#serpauthor=16637&serpcategory=blog&serpgroup=354&serpsort=date%20desc
Feiticeir0 - Pool Water Monitoring
/search?q=just%20encase#serpauthor=241826&serpcategory=blog&serpgroup=354&serpsort=date%20desc
skruglewicz – Case Enclosure Reliability Monitor
/search?q=just%20encase#serpauthor=285493&serpcategory=blog&serpgroup=354&serpsort=date%20desc
vishwasn – Air Quality Monitor Project
/search?q=just%20encase#serpauthor=70356&serpcategory=blog&serpgroup=354&serpsort=date%20desc
milosrasic98 - OrbWeaver Rover
/search?q=just%20encase#serpauthor=46770&serpcategory=blog&serpgroup=354&serpsort=date%20desc
dwinhold – Winter Driving Safety
/search?q=just%20encase#serpauthor=12642&serpcategory=blog&serpgroup=354&serpsort=date%20desc
rsjawale24 - Landslide monitoring for the Himalayan region
/search?q=just%20encase#serpauthor=230652&serpcategory=blog&serpgroup=354&serpsort=date%20desc
RedCharly - Monitoring an irrigation canal using LoRa
/search?q=just%20encase#serpauthor=270692&serpcategory=blog&serpgroup=354&serpsort=date%20desc
gracemcnally - Particulate Matter Monitoring System for Wildfires
/search?q=just%20encase#serpauthor=423219&serpcategory=blog&serpgroup=354&serpsort=date%20desc
christophersky – Garden Pond Monitor
/search?q=just%20encase#serpauthor=244264&serpcategory=blog&serpgroup=354&serpsort=date%20desc
Taifur - Biofloc Monitoring System
/search?q=just%20encase#serpauthor=35163&serpcategory=blog&serpgroup=354&serpsort=date%20desc
guillengap - Monitoring and Protection an Ecological Area
/search?q=*#serpauthor=362384&serpcategory=blog&serpsort=date%20desc&serpgroup=354
Hammond Manufacturing Technical Judge Team |
![]() |
element14 Community Judges element14 Community Team |
The Sponsored Kit | The Specs |
---|---|
PSoC
PSoC (CY8CKIT-062S2-43012) |
• Ultra-low-power PSoC • The Murata 1LV Module hosting the ultra-pow-power Infineon AIROC • CapSense capacitive touch sensing enabled buttons and sliders • PSoC 5LP MCU for program/debug • Excelon |
Infineon Technical Judge Team |
![]() |
element14 Community Judges element14 Community Team |