Light Up Your Life
  • Challenges & Projects
  • Design Challenges
  • Light Up Your Life
  • More
  • Cancel
Light Up Your Life
Forum AuraAlert - Part 3 - Industrial Design
  • News
  • Forum
  • Projects
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Light Up Your Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 49 subscribers
  • Views 599 views
  • Users 0 members are here
Related

AuraAlert - Part 3 - Industrial Design

arvindsa
arvindsa over 1 year ago

Hello everyone. I have been traveling so, couldn't do justice to the development but i managed to think the basic design. Now, My Professor at my University said i suck at sketching but my concepts and ideas were strong, so i decided to not stop sketching not until i perfect the skill or some good designer get a heart attack looking at my terrible skills.

Evaluating Requirements of Handheld device

Handheld devices are means not always in hand, but also maybe in pocket or ladies purse or sometimes on the table. It should be small, versatile, easy to hold, easy to charge. More importantly, the light should signify the type of alert as well it's urgency when on table and the haptics should be strong enough to catch the attention of the user when he is engaged with some other work. This was designed by talking to couple of people with hearing difficulty.  The device should also have a screen to let the user know of the message if any so OLED should be present and finally to navigate the menu, change settings etc, 3 button system will be used. One button to navigate up and down and third to select. Back will be presented as a menu item itself. It is a pretty standard way to make a menu using minimal number of buttons. 

image

image

The High power though it light ups in only one primary direction, can remain hidden and unnoticed if it is kept facing downwards. In such a case, the LED Strip will come into play for catching attention. In the picture the they are shown with different colors but they can be the same color as well to indicate the type of sound and it's urgency to attention. I went with a charcoal/graphite/grey color body for a neutral look.

Evaluating Requirements of Halo Device

Halo Device is meant to be put up on the wall. Therefore it should play well with any paint color, any wallpaper or wood grain it might be kept against. Therefore I selected white to be the device color.  The halo has to be visible from the front and side. Why side? Because if it is kept in a some rooms such as long hallway, then most of the time people can only see the side of the device. Now, regarding the number of buttons, i am going with two. Maybe i will make it 3. But i need only one for turning on the configuration via esp32's WiFi and other to turn off the notification. I could have gotten away with one button, using long press for Configuration mode, but maybe during usage i may find a requirement for another button. When i looked into the Alexa Dot's tear down, i found that they were able to achieve the beautiful halo using 12 LED's and that included the circular running pattern. The only difference is that echo is not visible from the side. The central hole will accommodate the powerful LEDs

image

image

Evaluating Requirements of Wall Mountable Tile Device

Now, The Tile-able system is gonna be inspired from Nano-leaf's but instead of Triangle's i will go with Hexagon. The reason being, nano-leafs are always used in a bunch but  my device should remain solo. and when used solo, only geometry that looks good and projects enough surface area for catching attention is a Hexagon.  I might even have to say that i was slightly inspired from an Youtube Channel i Follow - CCP Grey's Hexagons are the bestagons https://www.youtube.com/watch?v=thOifuHs6eY 

Putting a button in this device is harder, as i cannot visibly put any switches on the front, which will affect the uniform look of the tiles. And if it is going to be tiled, i cant put any on the side also. So the only way is to make the entire face of the hexagon lit by the LED as the switch cap itself. This will be a major engineering design, but it will be worth it. 

image

image

Here is a video of the same things. Will start posting the engineering aspects soon. It is almost done.

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 1 year ago +1
    Nice update. I like the hexagon tiles.
Parents
  • embeddedguy
    embeddedguy over 1 year ago

    Believe me or not but I have Alexa in my room and while watching your video, it got activated couple of times.SmileySmileySmiley
    BTW, I did not get much from the writings that you have but, I understood the video more. Interesting concept.!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • embeddedguy
    embeddedguy over 1 year ago

    Believe me or not but I have Alexa in my room and while watching your video, it got activated couple of times.SmileySmileySmiley
    BTW, I did not get much from the writings that you have but, I understood the video more. Interesting concept.!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • arvindsa
    arvindsa over 1 year ago in reply to embeddedguy

    Ya, Maybe i wrote in haste. Will reword.