Light Up Your Life
  • Challenges & Projects
  • Design Challenges
  • Light Up Your Life
  • More
  • Cancel
Light Up Your Life
Forum How's the kit?
  • News
  • Forum
  • Projects
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Light Up Your Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 49 subscribers
  • Views 493 views
  • Users 0 members are here
  • working with the kit
Related

How's the kit?

cstanton
cstanton 11 months ago

I'm seeing a lot of photo's showing the inside of boxes, and screenshots of software, how're you finding the kit, what do you think about it so far? Is it what you expected?

I'm interested in seeing some discussions and opinions, and hearing any difficulties anyone's having (or finding it surprisingly manageable!)

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui 11 months ago +2
    The Wurth Elektronik WL-ICLEDs in the 5050-size are probably the easiest to work with given the breakouts supplied - getting them working on a breadboard is not too difficult if you can master the SMD…
  • JoRatcliffe
    JoRatcliffe 11 months ago in reply to arvindsa +2
    Yes we are extending the final deadline to midnight UK time on Sunday 16th November to give everyone extra time with the kit, receive additional parts they have ordered, and make their final updates
  • Anthocyanina
    Anthocyanina 11 months ago +1
    very comprehensive kit. quite difficult to work with with universal prototyping boards(for the smallest ones), and no tests yet with custom PCBs. I wish the examples Würth provided in their Github were…
Parents
  • Gough Lui
    Gough Lui 11 months ago

    The Wurth Elektronik WL-ICLEDs in the 5050-size are probably the easiest to work with given the breakouts supplied - getting them working on a breadboard is not too difficult if you can master the SMD soldering. But the logic shifter being supplied as the bare IC means that users are likely either to have to rely on others they may already have (as I did) or they may need to go without (in which case, I've actually had some success with omitting it, even though it is technically not supposed to work for one of them).

    The other sizes are the domain of a custom PCB - that's not necessarily hard to do, but waiting on a manufacturer to make it and shipping is probably the more annoying part. On a software level, all of them with the exception of the 1312121320437 are signalling compatible with the WS2812B (one-wire type) and APA102 (two-wire type). From some research, I believe the 1312121320437 which is a 48-bit variety one-wire type would be compatible with WS2816 "high definition LED", meaning FastLED could work with them all, but this is yet to be confirmed.

    I'm working a little bit ahead of what I've been able to blog - lots of commitments on my plate all-round, but I think I should be able to make it to the finish line ... but I'll have to face the (potentially daunting) aspect of unknown-unknowns and more software-related issues assuming my PCBs arrive in time and my soldering techniques work for the other smaller types.

    As for what I expected ... well, I didn't expect it to be practically a drop-in for other popular RGB integrated-controller LEDs, which has both pros and cons, as it might be easy for manufacturers to make component substitutions without us knowing, but it does mean it's easy to put them into existing designs if we're interested in having that "Wurth-quality".

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui 11 months ago

    The Wurth Elektronik WL-ICLEDs in the 5050-size are probably the easiest to work with given the breakouts supplied - getting them working on a breadboard is not too difficult if you can master the SMD soldering. But the logic shifter being supplied as the bare IC means that users are likely either to have to rely on others they may already have (as I did) or they may need to go without (in which case, I've actually had some success with omitting it, even though it is technically not supposed to work for one of them).

    The other sizes are the domain of a custom PCB - that's not necessarily hard to do, but waiting on a manufacturer to make it and shipping is probably the more annoying part. On a software level, all of them with the exception of the 1312121320437 are signalling compatible with the WS2812B (one-wire type) and APA102 (two-wire type). From some research, I believe the 1312121320437 which is a 48-bit variety one-wire type would be compatible with WS2816 "high definition LED", meaning FastLED could work with them all, but this is yet to be confirmed.

    I'm working a little bit ahead of what I've been able to blog - lots of commitments on my plate all-round, but I think I should be able to make it to the finish line ... but I'll have to face the (potentially daunting) aspect of unknown-unknowns and more software-related issues assuming my PCBs arrive in time and my soldering techniques work for the other smaller types.

    As for what I expected ... well, I didn't expect it to be practically a drop-in for other popular RGB integrated-controller LEDs, which has both pros and cons, as it might be easy for manufacturers to make component substitutions without us knowing, but it does mean it's easy to put them into existing designs if we're interested in having that "Wurth-quality".

    - Gough