Light Up Your Life
  • Challenges & Projects
  • Design Challenges
  • Light Up Your Life
  • More
  • Cancel
Light Up Your Life
Forum How's the kit?
  • News
  • Forum
  • Projects
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Light Up Your Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 49 subscribers
  • Views 490 views
  • Users 0 members are here
  • working with the kit
Related

How's the kit?

cstanton
cstanton 11 months ago

I'm seeing a lot of photo's showing the inside of boxes, and screenshots of software, how're you finding the kit, what do you think about it so far? Is it what you expected?

I'm interested in seeing some discussions and opinions, and hearing any difficulties anyone's having (or finding it surprisingly manageable!)

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui 11 months ago +2
    The Wurth Elektronik WL-ICLEDs in the 5050-size are probably the easiest to work with given the breakouts supplied - getting them working on a breadboard is not too difficult if you can master the SMD…
  • JoRatcliffe
    JoRatcliffe 11 months ago in reply to arvindsa +2
    Yes we are extending the final deadline to midnight UK time on Sunday 16th November to give everyone extra time with the kit, receive additional parts they have ordered, and make their final updates
  • Anthocyanina
    Anthocyanina 11 months ago +1
    very comprehensive kit. quite difficult to work with with universal prototyping boards(for the smallest ones), and no tests yet with custom PCBs. I wish the examples Würth provided in their Github were…
  • Anthocyanina
    Anthocyanina 11 months ago

    very comprehensive kit. quite difficult to work with with universal prototyping boards(for the smallest ones), and no tests yet with custom PCBs. I wish the examples Würth provided in their Github were more platform agnostic, but driving them hasn't been too difficult with other libraries. I'll be posting my first entries in the next few days expanding on all this

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui 11 months ago

    The Wurth Elektronik WL-ICLEDs in the 5050-size are probably the easiest to work with given the breakouts supplied - getting them working on a breadboard is not too difficult if you can master the SMD soldering. But the logic shifter being supplied as the bare IC means that users are likely either to have to rely on others they may already have (as I did) or they may need to go without (in which case, I've actually had some success with omitting it, even though it is technically not supposed to work for one of them).

    The other sizes are the domain of a custom PCB - that's not necessarily hard to do, but waiting on a manufacturer to make it and shipping is probably the more annoying part. On a software level, all of them with the exception of the 1312121320437 are signalling compatible with the WS2812B (one-wire type) and APA102 (two-wire type). From some research, I believe the 1312121320437 which is a 48-bit variety one-wire type would be compatible with WS2816 "high definition LED", meaning FastLED could work with them all, but this is yet to be confirmed.

    I'm working a little bit ahead of what I've been able to blog - lots of commitments on my plate all-round, but I think I should be able to make it to the finish line ... but I'll have to face the (potentially daunting) aspect of unknown-unknowns and more software-related issues assuming my PCBs arrive in time and my soldering techniques work for the other smaller types.

    As for what I expected ... well, I didn't expect it to be practically a drop-in for other popular RGB integrated-controller LEDs, which has both pros and cons, as it might be easy for manufacturers to make component substitutions without us knowing, but it does mean it's easy to put them into existing designs if we're interested in having that "Wurth-quality".

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • embeddedguy
    embeddedguy 11 months ago

    Hi,

    I have not applied for the kit, but I got some PCB/A and I can say something based on that. So some of the LEDs are quite small in size and they might be hard to solder without expertise to do so. Hence, I decided to do a PCB design so that I can reduce the amount of soldering that is required. Also, I learned that many improvements are possible in my PCB design. 

    One nice thing is that Wurth has many different kinds of LEDs for various use cases. For example, some LEDs have higher color depth. i.e. number of bits are up to 12 bits for each R, G, B channel. Other thing is that some LEDs have bypass function, that makes it possible to bypass a specific LEDs in case they are damaged or not functioning as expected. This will keep the other LEDs on despite malfunctioning of individual LED. 

    I think that these LEDs have different use cases based on various factors such as size, application, cost, power budget, complexity, etc. One can use this challenge kit to address this. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • arvindsa
    arvindsa 11 months ago

    Things are going pretty good. I did have issues driving the LEDs via STM32 as the FAST LED's support for stm32 was not there. But managed to get it working via Neopixel and Dotstar libraries. But i am looking for some extension in the deadline. Say 15 days. I hope other participants also join in the request.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton 11 months ago in reply to arvindsa
    arvindsa said:
    But i am looking for some extension in the deadline. Say 15 days

    I believe JoBatcliffeBat (joratcliffe)  is considering an extension Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JoRatcliffe
    JoRatcliffe 11 months ago in reply to arvindsa

    Yes we are extending the final deadline to midnight UK time on Sunday 16th November to give everyone extra time with the kit, receive additional parts they have ordered, and make their final updates Slight smile