Light Up Your Life
  • Challenges & Projects
  • Design Challenges
  • Light Up Your Life
  • More
  • Cancel
Light Up Your Life
Forum Smart car chamber #5 Solder Method for WL-ICLEDs
  • News
  • Forum
  • Projects
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Light Up Your Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 49 subscribers
  • Views 493 views
  • Users 0 members are here
Related

Smart car chamber #5 Solder Method for WL-ICLEDs

fyaocn
fyaocn 11 months ago

1 Solder method for WL-ICLED

Just briefing the solder method for WL-ICLED with the 4-pin production,  1312020030000, 1313210530000, 1315050930002, since there are  still some problems driving 6-pin.But the principle are the same.

The soldering methods include using a soldering iron, hot air gun, and soldering station.

1.1 Characteristics of the LEDs

  • Package Type: All are 4-Pin SMDs – 1313210530000 (Side View SMD), 1312020030000 and 1315050930002 (PLCC4 package). They feature standard pin pitch (typically 2.0-2.5mm, no ultra-fine pitch) and a small number of pins, resulting in moderate soldering difficulty.
  • Key Sensitivity: LED chips are heat-sensitive (maximum tolerance: ≤260℃ for ≤10 seconds). Pins are prone to oxidation; cold solder joints and bridging must be avoided.

1.2 Pre-Soldering Preparation

  • PCB Preprocessing: Clean pads with anhydrous ethanol to remove oil and oxide layers. The new PCB is OK, but check first.
  • Solder Selection: Use lead-free solder wire (0.3-0.5mm diameter) with no-clean flux (reduces soldering temperature and prevents oxidation). Or use solder paste with appropriate character, most of which start from 183 ℃
  • Tool Calibration: Calibrate the soldering iron/soldering station to 280-320℃; match the hot air gun’s temperature and airflow (to avoid blowing off components). Use solder plate the temperature setting shall be low enough. In this case, 220 ℃ for solder plate and 280℃ for solder iron

2 Solder iron used for 1315050930002

2.1 Soldering Iron Method (Manual Point-to-Point Soldering)

Soldering Steps

  1. Component Positioning: Place the WL-ICLED SMD accurately on the PCB pads, ensuring all 4 pins align with the pads (note the pin orientation of the Side View product 1313210530000 to avoid reverse mounting).
  2. Temporary Fixing: Hold the component with tweezers, dip the soldering iron in a small amount of solder, and solder one pin to temporarily secure the component. Check for misalignment.
  3. Full Soldering: Solder the remaining 3 pins sequentially. Touch both the pin and pad with the iron tip, feed solder wire after 1-2 seconds, and remove the solder wire first, then the iron once the solder uniformly wets the pin-pad junction (forming a smooth solder joint).
  4. Cleaning & Trimming: Use desoldering braid to remove excess solder (preventing bridging) and wipe residual flux with anhydrous ethanol.

Like this, this is photo for capacitor, same to the 1315050930002.

image

2.2 Short circuit and bug detection

I am too quick in put everything in place. But  it frustrated me with the five WL-ICLED black out. It is liable to overtemperature and break the LED with solder iron. I have to remove them all to check one by one.

image

Before I start to remove them I chech with multimeter, I found out that the Vcc and GND is short-circuited. I guess there may be the short circuit but capacitor. I remove all capacitors and check one by one. Capacitor can withstand high temperature, so it is easy to do it even prolong the heating time.

image

Yes, it works. The solding for LED is OK, save lots of time for me.

image

This video shows one bug from software, there are two LED skipped. Only three ones blinks. I shall explain later in next post. That is ineresting foundout. Anyway, solder is Good.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The solder iron is quick and easy to use. Even for smaller parts, that is OK. But temperature control need skill and experience.

Advantages Disadvantages
1. Low tool cost (affordable soldering irons under $20), low entry barrier – ideal for small-batch production or repairs.
2. Localized heating minimizes thermal shock to the LED chip (chip temperature ≤200℃, reducing damage risk).
3. Easy solder volume control reduces bridging; high soldering precision (simpler for 4-pin components).
4. No complex equipment debugging – suitable for on-site quick soldering.
1. Low efficiency (30-60 seconds per component) – unsuitable for mass production.
2. Skill-dependent; beginners may experience cold solder joints (insufficient heating) or dry joints (poor pad wetting).
3. The Side View product 1313210530000 may have obscured pins due to packaging, requiring angle adjustments for visibility.

I prefer to solder iron in most cases.

3 Solder plate for  1312020030000, 1313210530000

3.1 Solder plate -Soldering Station Method (Temperature-Controlled Platform + Auxiliary Tools – Nearly Professional-Grade Soldering)

It is not difficult to buy one solder plate and solder paste. This is mini-version of solder station, in fact it is just one normal solder plate.

image

Steps

  1. PCB Fixing: Secure the PCB on the temperature-controlled soldering station with clamps (to prevent movement during heating).
  2. Preheating: Set the soldering station to 220-250℃ to preheat the pad area (ensures uniform heating and reduces temperature differences during soldering).
  3. Solder Paste Application: Apply a small amount of lead-free solder paste (preferrable Sn-Ag-Cu, particle size 20-45μm) to the pads using a stencil or dispenser.
  4. Component Mounting: Place the WL-ICLED SMD accurately on the solder paste with tweezers or a pick-and-place machine.
  5. Heating & Soldering: Raise the station temperature to 280-300℃, hold for 5-8 seconds, and cool to room temperature once the paste melts and wets the pins.
  6. Inspection & Trimming: Inspect solder quality with a magnifying glass (focus on bridging/dry joints) and touch up with a soldering iron if needed.

Since this is small PCB and mini solder plate is enough. Normally steel mesh for LED can be ordered with PCB at the same time. So as to apply the solder paster one time only and evenly without any problems.

In fact, I just dip the solder paste with hand. This lead to low quality in soldering by unevenly distributed solder paster.

3.2 For 1312020030000

Prepare the PCB and apply solder paste, put first capacitor in place.

image

Position all the 1313210530000 leds,

image

no need to worry about the precise position. If the paste applied evenly, the melted paste can pull the led in right position in the end.

image

It is preferrable to finish one LED first to confirm the polarization

image

as the video shows,

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Then put all others in same manner. But things is not always go easy , the middle one(the 3nd ) led is not blinking .

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

After visual inspection, I find out that there paste is not evenly applied on all four-pin. So, it is pull off original position and off-load one of the pin. 

I use simple solution to fix it. Put it on solder plate and heating again and take off the solder plate and cooling the PCB. AND, press the LED in right position  on PCB with a tweezer until it cool down.

3.3 For 1313210530000

This is smallest PCB of all six LEDs, and it is side view LED. 

image

I have made a mistake in PCB design. I select wrong model and the arrangement of PIN pad is different. the PIN  pad 2 and 3 shall be in opposition side. 

Once I appliy solder paste bit by bit and finish routine solder process, the LED is always black.

What a mistake. I do not have enough time to revise the design and order new PCB again.

I have to use one silly step again. apply minimum solder paste and solder 1313210530000 led one by one. As described above, repositoin the LED with tweezer during cooling down.

And finally, all positioned.

image

And luckly, all work fine.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

3.4 A little summary on to and pro

Advantages Disadvantages
1. Precise temperature control (±5℃ error) minimizes thermal shock to the LED chip – highest soldering yield (≥99%).
2. Extremely high efficiency; supports simultaneous soldering of multiple components (e.g., arrays of WL-ICLEDs) – ideal for mass production.
3. Stable soldering quality; eliminates human error for uniform, durable solder joints with strong long-term reliability.
4. Compatible with all three products (Side View 1313210530000 and PLCC4 packages) – no visibility or heating blind spots.
1. High equipment cost ($200-$1000 for professional stations) – significant initial investment.
2. Requires supporting consumables (solder paste, stencils, clamps) and complex workflows (preheating, temperature control, cooling).
3. Low cost-effectiveness for small-batch production or repairs (time-consuming setup/debugging).

4 Solder method of hot air gun

This is the most popular choice for all. And high efficiency for refurbishment and repair in all situation. 

Here is routine for hot air gun heating,

Soldering Steps

  1. Flux Application: Apply a thin layer of flux evenly on the PCB pads (enhances solder fluidity and prevents oxidation).
  2. Component Positioning: Place the WL-ICLED SMD accurately on the pads and hold it with tweezers.
  3. Hot Air Heating: Equip the hot air gun with a dedicated SMD nozzle (5-8mm diameter, matching the 4-pin package). Set the temperature to 300-330℃ and airflow to appropriete levels (tavoid blowing off the component). Hold the nozzle 3-5mm above the component at a 45° angle and heat in a circular motion.
  4. Touch-Up & Trimming: Once the pre-applied solder/paste melts and wets the pins, continue heating for 1-2 seconds, then remove the gun. After cooling to room temperature, check for bridging and clean excess solder with desoldering braid.

While I skip this choice , since

Advantages Disadvantages
1. Uniform heating solders all  pins simultaneously – high efficiency  suitable for medium-batch production.
2. Lower skill requirement than a soldering iron.
1. Tool cost something and requires dedicated nozzles.
2. Improper temperature/airflow control may damage the LED chip

5 Comparation of Solder method

Simple suggesion below

Soldering Method Core Advantages Applicable Scenarios Not Recommended For
Soldering Iron Low cost, simple operation, minimal thermal shock Small-batch production, repairs, DIY Mass production, Side View packages
Hot Air Gun High efficiency, uniform heating, compatible with Side View packages Medium-batch production, repairing soldering defects PCBs with nearby thermosensitive components
Soldering Station Stable quality, high yield, suitable for mass production(Steel mesh needed) Mass production, high-reliability requirements Small-batch production, repairs, DIY

6 Some Hints

6.1 Visual inspection is important

Prepare on mini magnifier with near-view illumination. This is view of1313210530000, the IC-chip and RGB leds is easily read out.

image

6.2 Software matters, demo code shall be used during solder process.

The clock sequence may affect the one-wire WL-ICLED protocol. The 6-pins WL-ICLED equipped with clock pin, it would be more stable.

6.3 Placement of  Capacitor can be re-designed in small PCB. In some PCB, not all capacitor is soldered on. But the LED blink GOOD. In one hand, the WL-ICLED is robust in harsh state. On the other hand, not all capacitor is mandatory.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur 11 months ago +1
    Just to confirm my understanding. You soldered all LED's and capacitors to a PCB to discover a short between ground and VCC. Later you make mention of a PCB board design error. It appears you got the…
Parents
  • colporteur
    colporteur 11 months ago

    image

    Just to confirm my understanding. You soldered all LED's and capacitors to a PCB to discover a short between ground and VCC.

    Later you make mention of a PCB board design error.  It appears you got the circuit to work. What the short one issue or a combination?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fyaocn
    fyaocn 11 months ago in reply to colporteur

    One of capacitor is broken due to overheating. Find and remove it make the ICLED works again.

    The wrong PCB design is for  side view of 1313210530000 , put pad in wrong side, and can not soldering well with hotplate. Have to adjust manually. It solved with hand solder skill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fyaocn
    fyaocn 11 months ago in reply to colporteur

    One of capacitor is broken due to overheating. Find and remove it make the ICLED works again.

    The wrong PCB design is for  side view of 1313210530000 , put pad in wrong side, and can not soldering well with hotplate. Have to adjust manually. It solved with hand solder skill