Very good designed challenge. Hope will get selected.
Powerful processor MiniZed running Ubuntu OS, PetaLinux is what I need for personal R&D.
Very good designed challenge. Hope will get selected.
Powerful processor MiniZed running Ubuntu OS, PetaLinux is what I need for personal R&D.
Good luck with your application, I have been trying to install the course material in some of the machines I have and I still have not succeeded. I'm having a lot of problems for the installation of the virtual machine, I thought it would be simpler, but there are many hours of downloads and installations and they do not go well. I don't know if in the end I will be able to participate.
Good luck with your application, I have been trying to install the course material in some of the machines I have and I still have not succeeded. I'm having a lot of problems for the installation of the virtual machine, I thought it would be simpler, but there are many hours of downloads and installations and they do not go well. I don't know if in the end I will be able to participate.
Hello Javagoza
Both Vivado ML Edition - 2022.2 Full Product Installation and Vitis Core Development Kit - 2022.2 Full Product Installation
AMD-Xilinx Vitis Core Development Kit Xilinx Unified Installer 2022.2 SFD , TAR/GZIP is 89.4 GB
Update 1 is Xilinx Unified 2022.2.1 : All OS installer Single-File Download ,TAR/GZIP -is 8.65 GB
Update 2 isXilinx Unified 2022.2.2 : All OS installer Single-File Download, TAR/GZIP - 18.88 GB
Only Xilinx Unified Installer 2022.2: Linux Self Extracting Web Installer is 271.02 MB
My four hard disks 1 Tb and 2Tb hard disk already dead with laptop dead, after crash. Now using less GB hdd, I will need to buy new for this HDD.
It is huge file that's why. Some downloaded web installer might have corrupted files. Your download might be corrupted .
Good luck too with your application.
Abhishek Bansal
Hello Javagoza
Can you tell you were trying to install on Windows or LInux.
I have installed the virtual machine on Windows 11. On the second attempt I have already managed to create the virtual machine, installed Ubuntu and Vitis complete with the version indicated for the course. Anyway I think I will follow the course from Vitis/Vivado for windows and I will use the Linux virtual machine only for Petalinux.
Thanks.
I will make shortly video of installation and post link here.
I will make after selection or rejection.
If selected, it will be in the Blog otherwise here.
Good luck
That's great.
Thanks and hope will be in the selection list.
Good luck to you also.
I m selected, so will upload installation video in Blog, Youtube