Very good designed challenge. Hope will get selected.
Powerful processor MiniZed running Ubuntu OS, PetaLinux is what I need for personal R&D.
Very good designed challenge. Hope will get selected.
Powerful processor MiniZed running Ubuntu OS, PetaLinux is what I need for personal R&D.
My this application is on Ultra96-V2. I have switched from Minized to Ultra96 for my projects.
The other three applications if I submit would be part of my patent and it is also on Ultra96.
The projects presented on Path Programmable II used a lot of applications from PYNQ platform. Hopefully, I will see more different ideas from Path Programmable III.
Thanks, I didn't knew that. I logged on element14 after 2018 in 2023 (except to see some components from here or other for Delhi cheaper shipping charge).
I saw there were 10 trainees but I didnt found your name.
I found PYNQ supports Zynq based boards (Zynq, Zynq Ultrascale+, Zynq RFSoC). Glad PYNQ is an open-source on pyhton. If selected, I will like to explore Ultra96.
I specially liked Micron 2 GB LPDDR4 Memory, Boyd Heatsink. My second project which is personal R&D needs both these and also Pynq wouldbe addon. Looks linux commands can be used in handling it. If so and no add of extra hardware components, except jupiter notebooks, I will like to explore and also will make videos.
why my reply on PYNQ discussion is marked as spam/abusive by whom
I wrote this.
Thanks, I didnt knew this.
I saw Path Programmable II and there were 10 trainees but I didnt found your name.
Glad PYNQ is an open-source project on python.
I specially liked Micron 2 GB LPDDR4 Memory and Boyd Heatsink, and my second project need it. If linux commands can be run on it, I will also explore with jupter notebooks and make videos of it.
How it is spam and abusive. Typical jealous
I was not there because I was too shy to join the game back in 2019. Just joking. I was too busy in 2019.
ok
Did you put external links in your reply? That can cause a catch by the filter sometimes.
Till now, as such no external links, Only 2 lines were more there where I mentioned like when i last login and pynq boards. But board name I copied paste, may be that caused.
Admin must be having that post as got message to submit "appeal". No issue as such. No issue if someone or filter. I was worried if banned or debarred from participation.
External links would be there lateron or embedded of youtube for Xilinx installation on linux.
And if selected, there would be more videos on my youtube channel. I assume such links would not be banned.
No issues .
I got notification"Your abuse appeal for your post has been accepted."
They have uploaded post as it is. You can see what I had written.