Path to Programmable 3
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable 3
  • More
  • Cancel
Path to Programmable 3
Forum Question about Zynq Software installation
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Path to Programmable 3 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 129 subscribers
  • Views 4907 views
  • Users 0 members are here
  • petalinux
  • vivado_version
  • Path Programmable III
  • minized
Related

Question about Zynq Software installation

taifur
taifur over 3 years ago

From Lab 0 I understand that for completing the training course I need to install AMD-Xilinx Vitis and Vivado ML Edition 2021.1. For installing the tools an Ubuntu Linux LTS 18.04.04 running on a windows virtual machine is recommended. My question is may I use Ubuntu Linux LTS 18.04.04 OS directly without running it in a virtual machine? I have a Ubuntu OS installed on my PC.

  • Sign in to reply
  • Cancel

Top Replies

  • saadtiwana_int
    saadtiwana_int over 3 years ago +3
    That should not be an issue as such. The only thing that can happen is if your VITIS installation goes bad (and you're not a Linux wizard). It has happened to me in past and the easiest way out was to…
  • rscasny
    rscasny over 3 years ago +1
    You should not need to purchase a license. If you are being asked to purchase a license. Don't respond here and I'll contact someone to help. Randall element14
  • saadtiwana_int
    saadtiwana_int over 3 years ago in reply to taifur +1
    I'm curious to know if you can go through all the labs using the latest version of tools and petalinux. The training is based on 2021.2 and sometimes things don't work across different versions so well…
Parents
  • saadtiwana_int
    saadtiwana_int over 3 years ago

    That should not be an issue as such. The only thing that can happen is if your VITIS installation goes bad (and you're not a Linux wizard). It has happened to me in past and the easiest way out was to start over with an earlier VM snapshot. But if it's installed on the PC directly then you can't do that.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • saadtiwana_int
    saadtiwana_int over 3 years ago

    That should not be an issue as such. The only thing that can happen is if your VITIS installation goes bad (and you're not a Linux wizard). It has happened to me in past and the easiest way out was to start over with an earlier VM snapshot. But if it's installed on the PC directly then you can't do that.

    • Cancel
    • Vote Up +3 Vote Down