Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Path to Programmable - Blog 1 - MiniZed Enclosure
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
  • Author Author: rsc
  • Date Created: 28 Sep 2018 6:44 PM Date Created
  • Views 1503 views
  • Likes 5 likes
  • Comments 7 comments
  • path to programmable
  • enclosure
  • 3d design
  • minized
Related
Recommended

Path to Programmable - Blog 1 - MiniZed Enclosure

rsc
rsc
28 Sep 2018

While waiting for the official training package to arrive, I decided to make a couple of MiniZed enclosures using the 3D printer.

I purchased another MiniZed board so I could have one at home, and one at work

 

Manuel Alejandro Iglesias Abbatemarco designed an enclosure, and I tried to print his design, although the cutouts for fasteners and cooling holes turned out to be a problem.

His files can be found on Hackster here: https://www.hackster.io/mhanuel/minized-linux-tutorial-part-i-e2fa9d

 

So after a few tries at printing his part, I designed my own "ZedBox" with posts instead of holes for fasteners.

image

The top plate has a 1mm grove around the perimeter to lock it onto the bottom, and the size is designed to have the GPIO pins flush with the top surface.

I left the clear rubber bumpers on the board as spacers.

This ZedBox was printed using translucent PLA material so the LEDs can still be seen with the top installed.

image

Here are the .STL files if you'd like to print your own.

Attachments:
MiniZed.zip
  • Sign in to reply

Top Comments

  • rscasny
    rscasny over 7 years ago in reply to genebren +3
    I am hoping to email the first module today to the official trainees. Randall
  • aspork42
    aspork42 over 7 years ago +3
    Ok - first pass. The encloselure was a tight fit! I also found that my printer bed is a little out of square as the top was slightly out of square with the bottom. cant wait for rev 2 with button access…
  • aspork42
    aspork42 over 7 years ago +2
    Nice enclosure, Scott! I might print one based on your files for myself as well!
Parents
  • aspork42
    aspork42 over 7 years ago

    Ok - first pass. The encloselure was a tight fit! I also found that my printer bed is a little out of square as the top was slightly out of square with the bottom.

    cant wait for rev 2 with button access and some extra holes.

     

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 7 years ago

    Ok - first pass. The encloselure was a tight fit! I also found that my printer bed is a little out of square as the top was slightly out of square with the bottom.

    cant wait for rev 2 with button access and some extra holes.

     

    image

    • Cancel
    • Vote Up +3 Vote Down