Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Path to Programmable - Blog 3 - First Light
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
  • Author Author: rsc
  • Date Created: 17 Oct 2018 5:40 PM Date Created
  • Views 924 views
  • Likes 4 likes
  • Comments 3 comments
  • path to programmable
  • minized
Related
Recommended

Path to Programmable - Blog 3 - First Light

rsc
rsc
17 Oct 2018

Here are the objectives for the first few labs:

image

image

 

 

image

The instructions were very clear, although I'm not sure of all the why yet, I managed to output some ASCII

image

The lab pdfs link to a 790pg technical reference manual for your reading pleasure.....ug585-Zynq-7000-TRM.pdf

Once Vivado and the SDK are configured for the MiniZed hardware, the actual code is minimal.

image

Time to watch some more videos......

  • Sign in to reply

Top Comments

  • gecoz
    gecoz over 7 years ago in reply to Fred27 +3
    Hi David, I would stick with 2018.2 you have installed. I don't know if there are particular requirements for this course to force you to use version 2017.4, but I would think it is OK if you use 2018…
  • Fred27
    Fred27 over 7 years ago +2
    Do you know if Vivado 2017.4 is a necessity, or just links up nicely with the course? I've installed 2018.2 for use with an Arty S7 and don't really want to have 2 versions - especially with the ridiculous…
Parents
  • Fred27
    Fred27 over 7 years ago

    Do you know if Vivado 2017.4 is a necessity, or just links up nicely with the course? I've installed 2018.2 for use with an Arty S7 and don't really want to have 2 versions - especially with the ridiculous size of the installs!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gecoz
    gecoz over 7 years ago in reply to Fred27

    Hi David,

     

    I would stick with 2018.2 you have installed. I don't know if there are particular requirements for this course to force you to use version 2017.4, but I would think it is OK if you use 2018.2 instead. The only problems could be caused if you had to import a project created with an earlier version of Vivado, mostly due to slight differences in the IP libraries of the 2 versions, but usually you can solve them by upgrading all the IP modules used in the projects (which is usually successful for such close versions of Vivado).

     

    Fabio

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • gecoz
    gecoz over 7 years ago in reply to Fred27

    Hi David,

     

    I would stick with 2018.2 you have installed. I don't know if there are particular requirements for this course to force you to use version 2017.4, but I would think it is OK if you use 2018.2 instead. The only problems could be caused if you had to import a project created with an earlier version of Vivado, mostly due to slight differences in the IP libraries of the 2 versions, but usually you can solve them by upgrading all the IP modules used in the projects (which is usually successful for such close versions of Vivado).

     

    Fabio

    • Cancel
    • Vote Up +3 Vote Down