Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Path to Programmable - Blog 6 - The TCL script
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
  • Author Author: rsc
  • Date Created: 19 Nov 2018 4:20 PM Date Created
  • Views 1107 views
  • Likes 2 likes
  • Comments 5 comments
  • path to programmable
  • minized
Related
Recommended

Path to Programmable - Blog 6 - The TCL script

rsc
rsc
19 Nov 2018

I spent the weekend figuring out Lab 9.  It turns out that my file system wasn't in line with the TCL script.  The instructions are as follows:

***NOTE*** If you receive an error running the Tcl command above please delete your entire ZynqDesign project and ip repo. Then start from Experiment 1 step 1 in which you unzip a pre-built lab 8 project and ip repo to the correct location. The reason you received an error was most likely due to an incorrect naming convention that was done in a previous lab.

So, instead of starting over with Lab 1 with a new file structure, I used the pre-formatted Lab 8 output found in "Solutions_MiniZed".

I created the new file structure at C:/Speedway/ZynqHW/2017_4/ and copied the training material to that folder also.

Here's the new structure:

image

The ip_repo and ZynqDesign folders were extracted from "ZynqHW_Lab8_Solution.zip"

When I ran Vivado with the new workspace I got a few messages:

image

image

2018.2.2 Vivado complained about IP upgrades, so I upgraded them.

image

Then Vivado wanted to re-generate outputs and run synthesis and implementation again.

image

After all was complete, I am down to 1 Critical Warning:

image

image

  • Sign in to reply
Parents
  • aspork42
    aspork42 over 7 years ago

    Doesnt sound like much fun! I'm not using C:\Speedway so I hope I don't run into similar issues...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 7 years ago

    Doesnt sound like much fun! I'm not using C:\Speedway so I hope I don't run into similar issues...