Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Path to Programmable - Blog 8 - Module 2, ZynqSW Labs 4-7
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
  • Author Author: rsc
  • Date Created: 30 Dec 2018 2:22 AM Date Created
  • Views 1195 views
  • Likes 6 likes
  • Comments 3 comments
  • path to programmable
  • minized
Related
Recommended

Path to Programmable - Blog 8 - Module 2, ZynqSW Labs 4-7

rsc
rsc
30 Dec 2018

I ran into a problem right away, my Xilinx software licenses were all expired for some reason, and the SDK would not start.

Because of this, I downloaded Xilinx_Vivado_SDK_Web_2018.3_1207_2324_Win64 and installed a new image.

I can now run the SDK again.  Maybe someone can instruct me how to "clean up" the license files.

image

Vivado 2018.3 seems to start up faster BTW. image

The flow of the SW training modules is shown below.

 

image

 

 

The Objectives for SW Lab4 were similar to the HW Lab2:

image

There is example code for using the various peripherals attached to the driver descriptions listed in the .mss file.

image

You can cut and paste from these example files for use in your own applications.

The Zynq platform has various memories for program and data storage.  The MiniZed does not have all of these implemented.

The example code was loaded into QSPI memory and executed using a FSBL (First Stage Boot Loader).

 

image

 

Lab 5 objectives:

image

image

Lab 6  objectives:

 

 

image

 

 

image

image

 

 

 

 

 

image

 

 

Lab 7 objectives:

 

image

 

At the end of Lab 7, the FSBL was loaded with a BSP for the MiniZed and an application to test peripherals that would load and run at power-on.

The output is shown using a terminal program on COM5.

image

So at this point, I should know how to write some code and install it such that it runs at power on.

I'm still a bit confused at how I would develop a program like this and run it (or interact) with an OS like Petalinux.

Onward......

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +1
    Nice update. You have confirmed my fears as to why I did not apply for this challenge. With my ADD issues, there is no way I could do this anymore. DAB
  • rscasny
    rscasny over 7 years ago +1
    I saw your comment about the licenses expiring: " I ran into a problem right away, my Xilinx software licenses were all expired for some reason, and the SDK would not start." Sorry about that. I wasn't…
Parents
  • rscasny
    rscasny over 7 years ago

    I saw your comment about the licenses expiring: "I ran into a problem right away, my Xilinx software licenses were all expired for some reason, and the SDK would not start."

     

    Sorry about that. I wasn't aware that this would be an issue. Glad to see you got it going.

     

    Randall

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rscasny
    rscasny over 7 years ago

    I saw your comment about the licenses expiring: "I ran into a problem right away, my Xilinx software licenses were all expired for some reason, and the SDK would not start."

     

    Sorry about that. I wasn't aware that this would be an issue. Glad to see you got it going.

     

    Randall