• Products and Partners
    Products and Partners
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
Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Path to Programmable Blog 13 - Xilinx Libraries, the TE Sensor PMOD & Next Steps
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
  • Author Author: avnrdf
  • Date Created: 31 Dec 2018 9:32 AM Date Created
  • Views 1146 views
  • Likes 2 likes
  • Comments 1 comment
  • soc
  • avnet
  • path to programmable
  • xilinx
  • xilinx sdk
  • fpga
  • avnet minized
  • arm
  • minized
Related
Recommended

Path to Programmable Blog 13 - Xilinx Libraries, the TE Sensor PMOD & Next Steps

avnrdf
avnrdf
31 Dec 2018

Chapter 10 Video - Xilinx Libraries

 

This video explored the system libraries that Xilinx includes with SDK. These can be configured and initialized from the BSP settings eg- the Flash library allows users to select the manufacturer (Atmel, Microchip, Micron etc.) and the different interfaces. Xilinx libraries also comes bundled with example code.

imageimage

Lab 10 - Xilinx Libraries

 

In this lab, the flash library was used to read & write configuration data - which in this particular case was a MAC address.

A new BSP was generated and 'xilisf' (Xilinx In-system and serial flash library) was enabled. For the application, import the provided code.

 

The second part of the lab explored the provided code which used the xilisf API - which involved using functions to initialize, read, write & erase the contents of the flash. The provided application allows users to store and recall a MAC address over the serial (UART) interface.

 

Chapter 11 Video - TE Sensor PMOD

 

At the end of Module 1: Developing Zynq Hardware, we executed a TCL script that added a bunch of hardware to the block diagram - one of which was the AXI - I2C interface. The Avnet example for the TE Sensor PMOD uses this interface that resides in the PL via Xilinx provided drivers. This video briefly went over the AXI-I2C interface, the documentation, the HTU21DHTU21D PMOD and other PMODs that are available.

imageimage

image

 

Lab 11 - TE Sensor PMOD

 

This lab first explored the documentation for the AXI-I2C interface's peripheral drivers.

Application code is provided, but I did not run it as I did not have access to the PMOD.

 

image image

The lab instruction document lists out the files and their functions.

image

Chapter 12 Video - Next Steps

 

The video went over hardware and software that is available from Xilinx and its partners and how (and where) to get help and support.

It concluded with a review of what was covered in the Developing Zynq Software course.

imageimage

 

With this, Module 2 (Developing Zynq Software) of Path to Programmable is complete!

 

To recap:

Path to Programmable started with hardware: an overview of Zynq, the design tool flow, configuring the PS, creating a custom PL peripheral, using AXI and TCL scripting.

In the software module, we learnt how to use the board support package, the Zynq boot process, SDK project management and how to use Xilinx libraries.

 

The Path to Programmable courses cover a very small part of the entire Zynq software/hardware ecosystem, but serve as a very good introduction by functioning as a crash course to the Zynq Design flow.

Xilinx documentation covers everything that there is to know, but it is simply too overwhelming to start with. The Path to Programmable course did a very good job of explaining the important details in a concise manner, and skipping (yet referring to) the more complicated parts.

  • Sign in to reply
Parents
  • DAB
    DAB over 7 years ago

    Nice update.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 7 years ago

    Nice update.

     

    DAB