Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog [PP-02] First run of the reference Linux distribution
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
  • Author Author: kk99
  • Date Created: 17 Oct 2018 6:02 PM Date Created
  • Views 933 views
  • Likes 2 likes
  • Comments 2 comments
  • path to programmable
Related
Recommended

[PP-02] First run of the reference Linux distribution

kk99
kk99
17 Oct 2018

image

The PetaLinux provides a reference Linux distribution which is integrated and tested for Xilinx devices. This distribution includes:
- boot loader,

- CPU-optimized kernel,

- Linux applications and libraries,

- Debug,

- Thread and FPU support,

- Web server for easy management of network or firmware configuration.

 

After plug in of the micro-USB cable to the USB0JTAG/UART port on the MiniZed board we are able to login to PetaLinux.

Here are serial connection parameters:

- Port: COM1,

- Baud rate: 115200,

- Data: 8 bit

- Parity: None

- Stop: 1 bit,

- Flow control: None

We are able to login into the system with following credentials:

- Username: root

- Password: root

The Linux image creates a ramdisk file system in the DDR3 on MiniZed. In the system by the default are available basic commands.

 

Below there is example output from run of example application called: i2csensor which is included in image for easy testing of several peripherals devices on the MiniZed board.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This application allow to read the temperature and acceleration from sensor.

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +1
    I was wondering how to install this, but I see that it's running by default out of the box.
Parents
  • Fred27
    Fred27 over 7 years ago

    I was wondering how to install this, but I see that it's running by default out of the box.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kk99
    kk99 over 7 years ago in reply to Fred27

    Yes, it is awesome idea with ready out of the box development environment

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kk99
    kk99 over 7 years ago in reply to Fred27

    Yes, it is awesome idea with ready out of the box development environment