Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog [PP-04] Lab 1 - building a basic Zynq design
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
  • Author Author: kk99
  • Date Created: 27 Oct 2018 5:45 PM Date Created
  • Views 710 views
  • Likes 1 like
  • Comments 1 comment
  • path to programmable
  • fpga
  • minized
Related
Recommended

[PP-04] Lab 1 - building a basic Zynq design

kk99
kk99
27 Oct 2018

The main purpose of this lab is to illustrate how to create a new Zynq project using UltraFast Design Methodology within Vivado Webpack.

 

Zynq Proccesing System (PS) has a configurable set of built-in peripherals and direct access to Programmable Logic (PL) that can build any custom IP. So, I we need we could create dedicated soft IP in PL and use it in PS.

 

1. Create a new Zynq project in Vivado

Below there is gallery with step-by-step instructions how to create a new project. Each step is described in image description.

 

{gallery} Creation of new project in Vivado

image

Click on Create Project.

image

Set the project name and project location.

image

This will be a RTL-based project, so please leave the radio button for RTL project selected.

image

Select VHDL as target language. Click Next two times.

image

Select target device: xc7z007sclg225-1.

image

Click Finish button.

image

There is Vivado design cockpit.

2. Create a new block design in Vivado

Below there is gallery with step-by-step instructions how to create a block design. Each step is described in image description.

{gallery} Creation of a new block design

image

Select Create Block Design.

image

Enter the block design name.

image

Select Add IP from the top bar of Diagram window. From search window choose ZYNQ7 Processing System.

image

Click Run Block Automation to perform automatic connection of IPs in block design.

image

This wizard automatically detects if is required to connect external interfaces for FIXED_IO and DDR. FIXED_IO are dedicated peripherals in the Zynq PS like UARTs, USB or Ethernet. Click Ok.

image

Click the Save Block Design button to save the block design. You could launch customizations by double-click on the ZYNQ7 PS IP block.

image

At this screen you could reconfigure ale PS features.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +1
    Nice update. DAB
Parents
  • DAB
    DAB over 7 years ago

    Nice update.

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 7 years ago

    Nice update.

    DAB