Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog [PP-12] Control a single segment display by MiniZed board
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
  • Author Author: kk99
  • Date Created: 21 Nov 2018 6:01 PM Date Created
  • Views 2210 views
  • Likes 7 likes
  • Comments 5 comments
  • path to programmable
  • fpga
  • avnet minized
  • minized
Related
Recommended

[PP-12] Control a single segment display by MiniZed board

kk99
kk99
21 Nov 2018

During roadtest of Arty S7 I have created a simple PMOD module with single segment display. So, I decided to use it with MiniZed SoC to create example application. I have a driver for single segment display written in Verilog. I used a top module to generate test pattern for this display module. ZYNQ7 processing system is required in this case in design to generate system clock used by top and display modules. Seven segment display is connected to PMOD1 connector. There are pinouts:
- L15 -> D,

- M15 -> C,

- L14 -> B,

- M14 -> A,

- K13 -> DP,

- L14 -> G,

- N13 -> F,

- N14 -> E.

 

First we need to create a empty project for MiniZed board. You could use a MiniZed board definitions available at Avnet page. Then please choose "Create Block Design" and add a ZYNQ7 PS. Please edit ZYNQ7 PS properties:

- change FCLK_CLK0 to 100 MHz,

- disable M AXI GPO interface.

Then please run "Run Block Automation" and "Create HDL Wrapper" for design.

image

Now you need to import top.v and display.v sources and top.xdc constraints. They are available in attachment. Please put top design at diagram and connect "FCLK_CLK0" to "clock". Then please generate output products and bitstream.

After that please export hardware with included bitstream and launch sdk. In SDK you need to create a empty application. Then please run application and program FPGA. You should be able to see digits on display. Here is video from test run:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Attachments:
sources.zip
  • Sign in to reply

Top Comments

  • aspork42
    aspork42 over 7 years ago +2
    Nice job!
  • rscasny
    rscasny over 7 years ago in reply to aspork42 +2
    This is a simple project that is what I had in mind for this P to P project. Randall
  • genebren
    genebren over 7 years ago +1
    Very cool, I really like your seven segment driver logic. Gene
Parents
  • genebren
    genebren over 7 years ago

    Very cool, I really like your seven segment driver logic.

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago

    Very cool, I really like your seven segment driver logic.

    Gene