Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Week 1: MiniZed ZYNQ Concept and basics
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
  • Author Author: snidhi
  • Date Created: 7 Oct 2018 1:18 PM Date Created
  • Views 2179 views
  • Likes 7 likes
  • Comments 5 comments
  • minized architecture
  • fpga development kit
  • fpga pwer
  • avnet minized
  • fpga developement
Related
Recommended

Week 1: MiniZed ZYNQ Concept and basics

snidhi
snidhi
7 Oct 2018

While I am reading the necessary Dokus I thought it would be a good idea to look into some basics of the MiniZed FPGA board and what it offers to the users and potential programmers.

 

When compared to other suppliers FPGAs development board such as from Digilent; the Avent MiniZedAvent MiniZed is reasonably priced at 80 euros (rather low end price). And can be bought off the internet easily.

A good amount of support documentation also exists on the MiniZed | Zedboard Support Forum for self starters.

 

  • What is MiniZed?
  • Block Diagram of the MiniZed Board
  • MiniZed Power Architecture
  • Conclusion

 

What is MiniZed?

MiniZed is a single-core Zynq 7Z007S development board with USB, Wi-Fi and Bluetooth features. It has Arduino-compatible shield interface to reuse the Arduino sensors. The Zynq-7Z007S fpga together with the Cortex A9 processor core (which can be used for signal processing) gives it a good processing power. There is also an on-board digital microphone to implement FIR filters, FFT’s etc.

 

Main Features of the MiniZed Board

 

  1. Xilinx Zynq XC7Z007S SoC
  2. Micron 512 MB DDR3L
  3. Micron 128 Mb QSPI flash
  4. Micron 8GB eMMC mass storage
  5. On-board USB to JTAG and debug UART circuit
  6. Murata "Type 1DX" wireless module with 802.11b/g/n Wi-Fi and Bluetooth 4.1 plus EDR and BLE (Bluetooth Low Energy)
  7. USB 2.0 host interface with Microchip USB3320 PHY
  8. Dialog Semiconductor DA9062 PMIC (Power Management IC)

 

The other good to have parts on the MiniZed Board

 

  1. Arduino-compatible shield interface
  2. 2 x Pmod-compatible interfaces
  3. ST Micro  LIS2DS12LIS2DS12 Accelerometer and Temperature sensor
  4. ST Micro MP34DT05 digital MEMS microphone
  5. Reset button, user button, user switch, 2 x user bi-element LEDs
  6. Microchip Low-Power Precision CMOS Oscillators

 

Block Diagram of the MiniZed Board

 

 

image

A descriptive Block Diagram of the MiniZed

 

MiniZed Power Architecture

Coming from an analog side of engineering if I see a PCB I feel an itch image to know its power consumption and to see if it offers a balanced perspective with regards to power consumption. Having a power efficient product has become very important specially if it wants to have a fair chance to make it to the product line. And of course look its schematics.

 

image

A current and voltage requirements Overview

 

Board Level Power Budgeting on the MiniZed Board. Reference

 

 

image

Fig: The generic power consumption of the dev-board

 

From this analysis one can see that the total power consumption of the internal parts of the MiniZed is around 8watt. But ofcourse the total power consumption of my project will depend on how many of the parts on board are in use. This rough estimate is a good indication of the current requirements of the FPGA.

 

 

Also I downloaded the famous Xilinx Power Estimator (XPE) from the MiniZED website and gave it a go.

 

imageFig: Summary of the XPE for the MiniZED board

 

I had a feeling that the Minized board was getting hotter after I had left it on continuously for sometime. Looking at the graphs below it seems that the board is designed to get heated upto 70 degC for a total power consumption of around 3watts (mind it which is less than half of the full power 8Watt Minized). I suppose under such intense use a need for heat sink or proper heat dissipation will arise.

Power vs Temperature Graphsimage

 

Xilinx Power Estimator (XPE) is a good tool to play around with. I also looked into the other tabs such as clock, logic etc. in the XPE excel-sheet

 

Conclusion

 

From a quick feature review and look into the power analysis and the schematics the MiniZed board it seems to be a resourceful development board. Although the power consumption of the board is not extraordinary but keeping the price-point I can say it is a good balance.

  • Sign in to reply

Top Comments

  • snidhi
    snidhi over 7 years ago in reply to mu.udhay +3
    udhay; power should be considered when designing your device or product. Also most important consideration for portable devices. The above mentioned power is what the board will need to be supplied with…
  • DAB
    DAB over 7 years ago +2
    Nice overview of the MiniZed power issues. DAB
  • aspork42
    aspork42 over 7 years ago +2
    Nice review of power consumption. How did they get Excel '97 graphs? I haven't seen those in ages
Parents
  • DAB
    DAB over 7 years ago

    Nice overview of the MiniZed power issues.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 7 years ago

    Nice overview of the MiniZed power issues.

     

    DAB