Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Xilinx ZYNQ - Blog 2 - Getting Code Running on the SoC
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
  • Author Author: shabaz
  • Date Created: 23 Oct 2018 12:21 PM Date Created
  • Views 6229 views
  • Likes 10 likes
  • Comments 10 comments
  • zedboard
  • soc
  • path to programmable
  • zynq
  • fpga
  • path_to_programmable
  • avnet minized
  • zynq-7000
  • zynq 7z007s
  • minized
Related
Recommended

Xilinx ZYNQ - Blog 2 - Getting Code Running on the SoC

shabaz
shabaz
23 Oct 2018

Note: This is part 2 of a series on working with FPGAs and in particular the Xilinx Zynq-7000S Programmable System-on-Chip with ARM Cortex-A9 processing core. For part 1, click here: Xilinx ZYNQ System-on-Chip - Getting to know the MiniZed Board

For all parts, click here: Path to Programmable

 

  • Introduction
  • Creating an Example Project
  • Zynq-7000 Programmable Logic and DSP Scale
  • Exploring Vivado
  • Adding the Processor System
  • Configuring the Processing System
    • Configuring the UART
    • Configuring the Clocks
    • Configuring the Memory (RAM)
  • A Glimpse of VHDL: Wrapper for the Processing System
  • Building the Design
  • Exploring the Design
  • Software Development Environment (Xilinx SDK)
  • Creating a Software Project
  • Running the Project
  • Summary

 

Introduction

This blog post is part of the Path to Programmable series. It documents my journey as a beginner with a Xilinx Programmable System-on-Chip which contains programmable logic and an ARM Cortex-A9 processor system. It comes on a development board called MiniZed.

 

In the previous blog post the MiniZed board was introduced. This blog post covers my experience with the first couple of training sessions. I’m rarely really impressed at the pace of training courses, but I have to say I was really impressed this time. It was like taking the red pill in the Matrix : ) It was like discovering a wormhole. I got further in a few hours than I imagined possible!

 

If you’re interested in using programmable SoCs, it is highly recommended to pick up a MiniZedMiniZed and try to join in, so we can bounce ideas off each other during the next two months.

 

I have to be careful not to trivialize the effort, because a lot was covered in a couple of the virtual training sessions. And I’m aware there is a huge journey to continue on. However, I was happy with the initial progress made so far – it was a big leap, and worth it.

 

So, this blog post covers the big leap (for me at least), hopefully in a concise and understandable way if anyone wants to follow along. Hopefully combined with the rest of the virtual Path to Programmable team’s blog posts, things should make sense.

 

What is the big leap? It is getting from a fresh Programmable SoC chip to the situation that it is successfully interfaces to DDR3 RAM and some C code is running inside the SoC’s processor and generating console output over a UART. This blog post discusses how all that was achieved from scratch, using Xilinx Vivado 2017.4 HLx WebPack and the MiniZed board. If you wish to follow along and replicate, then the software can be downloaded for free from the Xilinx website.

 

 

Creating an Example Project

Once Vivado was installed, I fired it up and created a project selecting VHDL as the language that would be used. You can use the screenshots below to do this if you’re following along (click to zoom the screenshot).

image

 

The precise Zynq part also needs to be specified when using the Create Project wizard. To find that out, the MiniZed hardware documentation can be consulted and it specifies the part as XC7Z007S-1CLG225C.

image

 

According to the Zynq-7000 PDF datasheet, that indicates a speed grade 1 part, in CL package, with 225 pins and commercial temperature range. This information was used to select the correct part in the Create Project wizard, although it specifies the part code as xc7z007sclg225-1 once the correct family, package and speed has been selected.

 

Zynq-7000 Programmable Logic and DSP Scale

There are 10 devices in the Zynq-7000 range, each with various speed grades and operational temperature ranges. They are lined up in the chart below to get a rough idea about the scale across the range. From left to right, the first three are have a single-core processor and the remainder are dual-cored. In terms of programmable logic (PL) and blocks of memory available to the PL, there is more than tenfold increase across the range. The MiniZed board uses the leftmost, smallest device in the range.

image

 

There is more than 30 times the DSP performance (see the DSP Slices and DSP GMAC bars in the chart above) going from left to right.

 

I doubt I’m going to be pushing the limits of the MiniZed : ) but it is nice to know that there are members of the Zynq-7000 for massively larger designs too. It is one of the great benefits of programmable logic, that it can be scaled in huge ways (allowing for parallel processing of data).

 

Exploring Vivado

Once the project was created, the panes for Vivado appeared as shown below. The key areas that were later used are highlighted.  The left area, under Project Manager, contains various tasks that need, mainly from top to bottom, but tasks can be skipped and the system will automatically run any previous tasks that are dependant on the current task.

 

The bottom area mainly contains reports and log output. From what I can see, it looks like Vivado’s tasks have an API in TCL, and therefore the Design Suite may not be essential; it could be possible to script everything in TCL for power users. I’m just speculating until I know more!

The main body of the Design Suite, circled in green, initially shows the Project Summary after the Create Project wizard was executed, but it can show many other things as will be discovered later. The red circled area shows a symbol which means ‘expand all’. It is sometimes clicked, within other windows that may appear when the Design Suite is used.

 

In summary I was pleasantly surprised that on initial appearance, Vivado didn’t seem as scary as the quite abstract name suggests! It all seemed logical.

image

 

Adding the Processor System

The next step was to add the processor to the design. Vivado treats it like any other design component (known as intellectual property or IP). Vivado comes equipped with perhaps 200 different IP components, including things like digital audio blocks, video blocks and of course the processor subsystem. IP in general is a great resource because it should be guaranteed working programmable hardware components!

 

IP in the FPGA world is like the digital logic equivalent of vendor code libraries in the computer software world. Adding (say) a video block IP into the design will allow a complete hardware state machine and other digital logic that would implement the video function to be available in the FPGA.  For this initial exercise, just the processor subsystem IP is added.

image

 

Once the Create Block Design task is clicked and a name is given to the design block being created, the ‘+’ icon can be clicked in the main large pane, and a large list of available IP is shown. It can be searched and the Processing System found and double-clicked.

 

It was very cool that a graphical object then got placed in the center pane. The green bar above it allows the object (the Processing System) to be configured!

 

It can be imagined that the configuration needed will include things like configuring what type of memory is attached to the Zync SoC, and also adding any peripherals that could be desired, such as serial buses to complete the processor system. All that is done by clicking on the Run Block Automation text in the green bar.

 

Configuring the Processing System

As discussed, the configuration of the processing system entails doing things like configuring the memory, clock and I/O, to get a fully functioning compute capability for the Zync SoC. By clicking through, it was very quick to get to a nice graphical diagram which showed all the possible things that could be configured. 

image

 

Any of the pink items in the block diagram could be clicked on to configure them, or the list just to the left of the diagram could be used. The blue circled item gets you back to the block diagram. At a minimum, things like the clock and memory need configuring. The pink circled items were configured, and they are discussed below.

 

Configuring the UART

A single asynchronous serial interface (known as a UART) was configured. This is the near-standard way to access any computer in the absence of a graphical user interface. Often electrically they are based on the RS232 standard on a full computer, but in the case of small processor chips, the voltage levels are quite often set to 3.3V. The UART can be brought out to different possible pins, so the configuration system allows the pins to be chosen (much like other ARM chips, there are only finite combinations available, so it is highly recommended to configure things from the left-side list in top-down order, to get the most awkward items configure first). After it was all completed, a tiny check-mark was visible on the green block diagram, showing that UART1 in this case was configured.

image

 

Another part of the UART is configured in the General Settings area of the block diagram, which is part of the PS-PL (Processing System to Programmable Logic) configuration. There, the baud rate was confirmed to be 115200.

 

This was all surprisingly smooth, and I can’t imagine how it could be simplified further by Xilinx.

 

Configuring the Clocks

Moving on down the list of stuff to be configured to enable the processing system to function, the next thing was to configure the clocks. Most processors internally have several clocks (all generated from a single external clock) implemented using a technology known as phased locked loops (PLL). This allows for the external clock to be multiplied or divided inside the chip, to clock different parts of the chip at different rates. This allows for slow things (like long connections off-chip to perform input/output) to run at a slower (and hence more energy-efficient) speed compared to the things that can be run at far higher rates (such as memories close to the chip). Some things like DDR memory require clocks within certain ranges, otherwise data is corrupted.

image

 

For the current exercise, since the programmable logic (PL) portion is unused, the clock to it is disabled and the interface is disconnected. The last couple of steps in the screenshots above are used to perform the disabling.

 

Configuring the Memory (RAM)

The final bit of mandatory config to get the processor system functioning is to set up the memory access details. In the case of the MiniZed board, this consists of instructing Vivado that DDR3 memory is on-board, and specifying the part details (custom information can also be configured if the memory chip was an unusual one). Delay settings are configured so Vivado is aware of PCB trace lengths out to the high speed memory.

image

 

Once it is all configured and saved, in the main pane the graphical design can be validated. Once that’s done, we’re actually ready to work with the very first piece of VHDL!

 

A Glimpse of VHDL: Wrapper for the Processing System

Now that the IP for the Processing System has been fully configured, it is time to let Vivado create some VHDL code for it. This was quite straightforward, it is just a few clicks! At the end of the process, the generated file (in this case Z_system_wrapper.vhd because at the start of this exercise we gave the IP the name Z_system) can be double-clicked and the main pane will display the VHDL output with syntax highlighting. 

image

 

Just for reference, the entire VHDL output is listed here – it is described further below.

 

--Copyright 1986-2017 Xilinx, Inc. All Rights Reserved.
----------------------------------------------------------------------------------
--Tool Version: Vivado v.2017.4 (win64) Build 2086221 Fri Dec 15 20:55:39 MST 2017
--Date        : Mon Oct 22 01:38:58 2018
--Host        : DESKTOP-SHABAZ1 running 64-bit major release  (build 9200)
--Command     : generate_target Z_system_wrapper.bd
--Design      : Z_system_wrapper
--Purpose     : IP block netlist
----------------------------------------------------------------------------------
library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
library UNISIM;
use UNISIM.VCOMPONENTS.ALL;
entity Z_system_wrapper is
  port (
    DDR_addr : inout STD_LOGIC_VECTOR ( 14 downto 0 );
    DDR_ba : inout STD_LOGIC_VECTOR ( 2 downto 0 );
    DDR_cas_n : inout STD_LOGIC;
    DDR_ck_n : inout STD_LOGIC;
    DDR_ck_p : inout STD_LOGIC;
    DDR_cke : inout STD_LOGIC;
    DDR_cs_n : inout STD_LOGIC;
    DDR_dm : inout STD_LOGIC_VECTOR ( 1 downto 0 );
    DDR_dq : inout STD_LOGIC_VECTOR ( 15 downto 0 );
    DDR_dqs_n : inout STD_LOGIC_VECTOR ( 1 downto 0 );
    DDR_dqs_p : inout STD_LOGIC_VECTOR ( 1 downto 0 );
    DDR_odt : inout STD_LOGIC;
    DDR_ras_n : inout STD_LOGIC;
    DDR_reset_n : inout STD_LOGIC;
    DDR_we_n : inout STD_LOGIC;
    FIXED_IO_ddr_vrn : inout STD_LOGIC;
    FIXED_IO_ddr_vrp : inout STD_LOGIC;
    FIXED_IO_mio : inout STD_LOGIC_VECTOR ( 31 downto 0 );
    FIXED_IO_ps_clk : inout STD_LOGIC;
    FIXED_IO_ps_porb : inout STD_LOGIC;
    FIXED_IO_ps_srstb : inout STD_LOGIC
  );
end Z_system_wrapper;


architecture STRUCTURE of Z_system_wrapper is
  component Z_system is
  port (
    DDR_cas_n : inout STD_LOGIC;
    DDR_cke : inout STD_LOGIC;
    DDR_ck_n : inout STD_LOGIC;
    DDR_ck_p : inout STD_LOGIC;
    DDR_cs_n : inout STD_LOGIC;
    DDR_reset_n : inout STD_LOGIC;
    DDR_odt : inout STD_LOGIC;
    DDR_ras_n : inout STD_LOGIC;
    DDR_we_n : inout STD_LOGIC;
    DDR_ba : inout STD_LOGIC_VECTOR ( 2 downto 0 );
    DDR_addr : inout STD_LOGIC_VECTOR ( 14 downto 0 );
    DDR_dm : inout STD_LOGIC_VECTOR ( 1 downto 0 );
    DDR_dq : inout STD_LOGIC_VECTOR ( 15 downto 0 );
    DDR_dqs_n : inout STD_LOGIC_VECTOR ( 1 downto 0 );
    DDR_dqs_p : inout STD_LOGIC_VECTOR ( 1 downto 0 );
    FIXED_IO_mio : inout STD_LOGIC_VECTOR ( 31 downto 0 );
    FIXED_IO_ddr_vrn : inout STD_LOGIC;
    FIXED_IO_ddr_vrp : inout STD_LOGIC;
    FIXED_IO_ps_srstb : inout STD_LOGIC;
    FIXED_IO_ps_clk : inout STD_LOGIC;
    FIXED_IO_ps_porb : inout STD_LOGIC
  );
  end component Z_system;
begin
Z_system_i: component Z_system
     port map (
      DDR_addr(14 downto 0) => DDR_addr(14 downto 0),
      DDR_ba(2 downto 0) => DDR_ba(2 downto 0),
      DDR_cas_n => DDR_cas_n,
      DDR_ck_n => DDR_ck_n,
      DDR_ck_p => DDR_ck_p,
      DDR_cke => DDR_cke,
      DDR_cs_n => DDR_cs_n,
      DDR_dm(1 downto 0) => DDR_dm(1 downto 0),
      DDR_dq(15 downto 0) => DDR_dq(15 downto 0),
      DDR_dqs_n(1 downto 0) => DDR_dqs_n(1 downto 0),
      DDR_dqs_p(1 downto 0) => DDR_dqs_p(1 downto 0),
      DDR_odt => DDR_odt,
      DDR_ras_n => DDR_ras_n,
      DDR_reset_n => DDR_reset_n,
      DDR_we_n => DDR_we_n,
      FIXED_IO_ddr_vrn => FIXED_IO_ddr_vrn,
      FIXED_IO_ddr_vrp => FIXED_IO_ddr_vrp,
      FIXED_IO_mio(31 downto 0) => FIXED_IO_mio(31 downto 0),
      FIXED_IO_ps_clk => FIXED_IO_ps_clk,
      FIXED_IO_ps_porb => FIXED_IO_ps_porb,
      FIXED_IO_ps_srstb => FIXED_IO_ps_srstb
    );
end STRUCTURE;

 

It is not a lot of code; just 91 lines, which define a VHDL Design Entity or Module. In this case, the entity or module happens to be the processor system. The diagram here shows a graphic representation of a typical VHDL design entity.

image

 

It consists of an entity declaration portion (the red part of the diagram), which defines only the external input/output connections from the module.

 

The rest of the file contains the architecture body, that is responsible for explaining the internals of the design entity. To do that, there are several methods possible in VHDL. One method is to declare what components are used and the names of the component pins. It is shown in blue. The connections between components, and to the outside world, are defined in the final portion shown in orange.

 

The two part architecture that uses component declarations and component instantiations, is known as a structural model. As mentioned there are other ways of defining the architecture. Vivado describes the processor system using a structural model.

 

With that information, the 91 lines of content begin to make sense. It can be seen that the file contains one component that is instantiated to create the VHDL design entity. The connections are things like the DDR memory bus, input/output pins, a reset line and a processor clock.

image

 

Building the Design

This part of the process converts everything into a hardware implementation ready for execution. In Vivado, everything in the left pane (the Flow Navigator) occurs sequentially. So by clicking on Generate Bitstream which is toward the bottom of the Flow Navigator pane, Vivado will execute everything else needed to achieve that. It would have been nice to see the software show an animation near each step (like the older Xilinx ISE software) but instead it is possible to see how far things have progressed by looking out for some text that changes at the top-right of the Vivado Design Suite.

image

 

Once the bitstream has been created (it will be a file called Z_system_wrapper.bit in this case), now the time has almost come for the hardware designer to hand off to the software developer to do their bit.

 

The software developer will want to be able to write, compile and run software in a programming language such as C. To do that, the developer needs more than the bitstream. Enough information is needed for the software development environment to be able to create startup code that will initialize the ARM processor and get things ready for executing the main code. To allow all this to occur, the hardware engineer needs to do one more thing and that is to click on File->Export->Export Hardware. This will generate some files that the software development environment can use to auto-generate the startup code which will initialize the processor in software to work with the memory and so on. Also, the bitstream can be included in the bundle of files so that the software developer can test the code for real on the hardware.

 

Exploring the Design

Before looking at the software developer’s tasks, I wanted to slightly explore what the hardware design looked like. I’m still familiarizing myself with Vivado’s capabilities, and the screenshots below are just for general interest. These are all viewable in Vivado after the design has been built.

image

 

The floorplan looked interesting; it is bare at the moment because no programmable logic is currently being used in this design. The two vertical sets of squares represent input/output pads on the chip. The large orange square is the processor system. The area to the right of the vertical sets of squares is the programmable logic area, separated into different domains. It will be fun to explore this further as the course progresses!

 

Software Development Environment (Xilinx SDK)

The software development can be done in an integrated development environment based on Eclipse. It is extremely popular with developers, and there will be lots of familiarity for them. To launch the IDE or software development kit as it is referred to by Xilinx, the menu item File->Launch SDK is used.

 

The files that are exported into the SDK/IDE can be seen using the PC’s file explorer, just for interest. The bitstream file can be seen there, as well as the various files that will allow the processor to come up and configure itself.

image

 

At this point, the developer is almost ready to start writing code! First, a board support package needs to be created which will provide the low-level functions such as the startup code (prior to running the main process) as well as basic input/output capabilities for debug using print statements to the serial console as an example. It is possible to incorporate a real-time operating system (RTOS) called FreeRTOS at this stage, but the training suggests creating the basic board support package for now.

image

 

Now that the BSP is created, the software developer can create a project and start coding.

 

Creating a Software Project

Much like any decent development environment for software, it is possible to use a wizard/template system to create the first project. It auto-compiles whenever it is saved.

image

 

Now I was finally ready to try it out on the real hardware : )

 

Running the Project

MiniZed’s boot switches were set as shown and then connected to the PC.

image

 

Using Device Manager, it was possible to see that a couple of USB Serial ports were available. One of these would be the serial console from the ARM core, but I wasn’t sure which one. I took a guess and in my case it was COM port 21. PuTTY or other serial terminal software can be used, and configured for 115200 baud with no flow control.

image

 

Next, by right-clicking on the project name in the Project Explorer pane, it was possible to select Run As -> Run Configurations and create a configuration that knew to use the USB JTAG capability to push the code into MiniZed!

image

 

The result of course was Hello World sent to the serial terminal.

image

 

The C code can now be modified as desired, and as soon as it is saved, it automatically re-compiles, and it can be executed by just clicking on the green ‘play’ icon (it will use the existing configuration to push the code to the board).

image

 

Summary

This lab exercise and hence this blog post covered a lot, but I felt it was worth it, because it really makes one feel that progress is being made. I had not thought I could get this far with Zynq so quickly to be honest.

 

I was pleasantly surprised. The underlying complexity in Vivado isn’t so much hidden, as actually just implemented in a way to make it easy for people to follow. This is still just beginning with Vivado, but I was very happy that these first steps are comfortably manageable even for beginners.

 

Thanks for following along!

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +5
    Hi Fred27 (Replying here otherwise it gets too indented, and there will be some diagrams in this comment): This is great to hear that you’re up to the Hello World stage. I totally agree, some of it is…
  • Fred27
    Fred27 over 8 years ago +2
    A great explanation. I managed to stumble my way through some of this on my own late last night. I shall try again following this and see how it goes.
  • DAB
    DAB over 8 years ago +2
    Very good update. I agree, the Vivado software appears to be very powerful and aimed at getting a novice user up to speed quickly. That said, it was a canned exercise and I expect everything to be included…
Parents
  • shabaz
    shabaz over 8 years ago

    Hi Fred27

    (Replying here otherwise it gets too indented, and there will be some diagrams in this comment):

     

    This is great to hear that you’re up to the Hello World stage. I totally agree, some of it is still ‘magic numbers’, but I think the trainers took the approach that it is better to put some detail aside for now, on the understanding that it may later make more sense, otherwise it could take a very long time to get to the stage of executing a program on the Zynq. I don’t actually mind that in some cases, it is an approach I’ve seen a few times, sometimes needed when there is too much detail to absorb otherwise. There are maybe more than 10k pages on the Zynq across many guides/manuals, so that detail is a little scary to me currently. It reminds me of my first job in a field that I was not familiar with at the time, where the standards the product were based on were 3GPP defined, and as a result ran to hundreds of thousands of pages, and for a few weeks I was prepared to ignore the heavy detail and just assume that what I was working on made some sense to the bigger picture, but then I felt frustrated, knowing that there were many unknowns, and not knowing for sure if I was delving into the correct documents (amongst thousands) or not. Even after several years I just had a vague idea, but in the end enough to be confident in my area. But you’re right, it is good to dig into this area now, since otherwise it can get too abstract… so here goes : )

     

    Regarding the UART pins and the reason for them being allocated MIO 48..49, my understanding currently is that this is due to the Zynq chip bringing out some pins directly from the Processor System, and so if no programmable logic is being used then like other ARM chips, the connections for certain I/O peripherals (IOP) like UART, I2C, I2S etc., can only come out in certain combinations, and cannot be brought out on any arbitrary pin. So, the Vivado GUI lists the valid options, and if (say) MIO 48..49 are selected for UART, then those pins are now not available for other peripherals that may have been allowed to use those pins too.

     

    The way the Processing System is implemented, the user has a choice to either connect to it from the outside world on the dedicated MIO (Multiplexed I/O) pins (and in that case only certain combinations are possible), or the user can route the peripherals (UART, I2C etc) into the programmable logic area, using some internal connections called EMIO (Extended Multiplexed I/O). If EMIO is used, then the programmable logic has access to those connections and then the connections can be routed to any pin the programmable logic can be wired to.

     

    This is explained in a Xilinx MIO and EMIO video where they use this diagram to explain it:

    image

     

    Although Vivado will automatically list the available MIO options for each peripheral, there is a table (table 2-4) buried in the 2000-page Zynq Technical Reference Manual PDF doc  

    that shows the valid combinations:

    image

     

    Only the blue shaded cells are valid for the particular Zynq chip IC package that is used on the MiniZed board (the other cells are valid for the larger packages). According to that table, the UART1 is valid on MIO pins 8..9, 12..13, 28..29, 32..33, 36..37, 48..49 and 52..52, and this matches the options in the drop-down when configuring in Vivado.

     

    The actual physical pin on the chip mapping is in a table available for the Zynq device/package, downloadable as a text or CSV file here: https://www.xilinx.com/support/package-pinout-files/zynq7000-pkgs.html

    image

    For the chip used on the MiniZed, this is the direct link: https://www.xilinx.com/support/packagefiles/z7packages/xc7z007sclg225pkg.txt

     

    So from there, searching for MIO48 and MIO49 shows these are BGA pins B12 and D13 respectively. The diagram is in the Zynq-7000 Packing Specification PDF in Figure 3-1.

    The empty unfilled diamonds are the MIO pins.

    image

    I’ve yet to fully see how to explore all this in Vivado (and hopefully the training will provide that soon, because in later labs, according to snidhi blog Week 3: Done!! Lab3 Lab4 and Lab5  the floorplan stuff is explored further). Anyway, from some limited exploration I was able to see the pins in Vivado, but currently I don’t know how use this part of the GUI:

    image

    As you say, this is reflected in the MiniZed schematic at the MiniZed documentation site :

    image

     

    Regarding the training material, I'm still exploring it, but it's good so far.

    It consists of PDF lab guides, this is an example snippet from lab 2:

    image

    Everything is clean and easy to follow and they refer off for additional reading/experiments in places.

    There are exercises and solutions too, reference material, and lots of videos covering hardware and software. The overall bundle of files is massive.

    The video/audio quality is very good as is the material they present.

    I am still exploring it so i don't have full conclusions on that currently, but so far I think it is very good material, very different from old-school training courses which supply aged black-and-white faded PDF powerpoint printouts in binders : ) I've seen a few of those in the past.. : (

    Anyway, I think it is really great you're willing to explore all this, given that it's definitely a non-trivial exercise to bring up any ARM applications processor from scratch, let along inside a chip with programmable logic. I think people spend weeks doing that with just the processor alone : ) so the training definitely moves fast in this area..

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 8 years ago

    Hi Fred27

    (Replying here otherwise it gets too indented, and there will be some diagrams in this comment):

     

    This is great to hear that you’re up to the Hello World stage. I totally agree, some of it is still ‘magic numbers’, but I think the trainers took the approach that it is better to put some detail aside for now, on the understanding that it may later make more sense, otherwise it could take a very long time to get to the stage of executing a program on the Zynq. I don’t actually mind that in some cases, it is an approach I’ve seen a few times, sometimes needed when there is too much detail to absorb otherwise. There are maybe more than 10k pages on the Zynq across many guides/manuals, so that detail is a little scary to me currently. It reminds me of my first job in a field that I was not familiar with at the time, where the standards the product were based on were 3GPP defined, and as a result ran to hundreds of thousands of pages, and for a few weeks I was prepared to ignore the heavy detail and just assume that what I was working on made some sense to the bigger picture, but then I felt frustrated, knowing that there were many unknowns, and not knowing for sure if I was delving into the correct documents (amongst thousands) or not. Even after several years I just had a vague idea, but in the end enough to be confident in my area. But you’re right, it is good to dig into this area now, since otherwise it can get too abstract… so here goes : )

     

    Regarding the UART pins and the reason for them being allocated MIO 48..49, my understanding currently is that this is due to the Zynq chip bringing out some pins directly from the Processor System, and so if no programmable logic is being used then like other ARM chips, the connections for certain I/O peripherals (IOP) like UART, I2C, I2S etc., can only come out in certain combinations, and cannot be brought out on any arbitrary pin. So, the Vivado GUI lists the valid options, and if (say) MIO 48..49 are selected for UART, then those pins are now not available for other peripherals that may have been allowed to use those pins too.

     

    The way the Processing System is implemented, the user has a choice to either connect to it from the outside world on the dedicated MIO (Multiplexed I/O) pins (and in that case only certain combinations are possible), or the user can route the peripherals (UART, I2C etc) into the programmable logic area, using some internal connections called EMIO (Extended Multiplexed I/O). If EMIO is used, then the programmable logic has access to those connections and then the connections can be routed to any pin the programmable logic can be wired to.

     

    This is explained in a Xilinx MIO and EMIO video where they use this diagram to explain it:

    image

     

    Although Vivado will automatically list the available MIO options for each peripheral, there is a table (table 2-4) buried in the 2000-page Zynq Technical Reference Manual PDF doc  

    that shows the valid combinations:

    image

     

    Only the blue shaded cells are valid for the particular Zynq chip IC package that is used on the MiniZed board (the other cells are valid for the larger packages). According to that table, the UART1 is valid on MIO pins 8..9, 12..13, 28..29, 32..33, 36..37, 48..49 and 52..52, and this matches the options in the drop-down when configuring in Vivado.

     

    The actual physical pin on the chip mapping is in a table available for the Zynq device/package, downloadable as a text or CSV file here: https://www.xilinx.com/support/package-pinout-files/zynq7000-pkgs.html

    image

    For the chip used on the MiniZed, this is the direct link: https://www.xilinx.com/support/packagefiles/z7packages/xc7z007sclg225pkg.txt

     

    So from there, searching for MIO48 and MIO49 shows these are BGA pins B12 and D13 respectively. The diagram is in the Zynq-7000 Packing Specification PDF in Figure 3-1.

    The empty unfilled diamonds are the MIO pins.

    image

    I’ve yet to fully see how to explore all this in Vivado (and hopefully the training will provide that soon, because in later labs, according to snidhi blog Week 3: Done!! Lab3 Lab4 and Lab5  the floorplan stuff is explored further). Anyway, from some limited exploration I was able to see the pins in Vivado, but currently I don’t know how use this part of the GUI:

    image

    As you say, this is reflected in the MiniZed schematic at the MiniZed documentation site :

    image

     

    Regarding the training material, I'm still exploring it, but it's good so far.

    It consists of PDF lab guides, this is an example snippet from lab 2:

    image

    Everything is clean and easy to follow and they refer off for additional reading/experiments in places.

    There are exercises and solutions too, reference material, and lots of videos covering hardware and software. The overall bundle of files is massive.

    The video/audio quality is very good as is the material they present.

    I am still exploring it so i don't have full conclusions on that currently, but so far I think it is very good material, very different from old-school training courses which supply aged black-and-white faded PDF powerpoint printouts in binders : ) I've seen a few of those in the past.. : (

    Anyway, I think it is really great you're willing to explore all this, given that it's definitely a non-trivial exercise to bring up any ARM applications processor from scratch, let along inside a chip with programmable logic. I think people spend weeks doing that with just the processor alone : ) so the training definitely moves fast in this area..

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Fred27
    Fred27 over 8 years ago in reply to shabaz

    shabaz Wow. That reply almost warranted its own blog post! Very helpful indeed.