Pi-Fest
  • Challenges & Projects
  • Design Challenges
  • Pi-Fest
  • More
  • Cancel
Pi-Fest
Blog It Came From The Synth - Mystery Melody Medley 3
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 10 Jul 2022 11:17 PM Date Created
  • Views 1866 views
  • Likes 6 likes
  • Comments 5 comments
  • doug wong
  • Pi-Fest Design Challenge
  • raspberry pi pico
  • pico
  • pi-fest
  • MIDI synthesizer
Related
Recommended

It Came From The Synth - Mystery Melody Medley 3

dougw
dougw
10 Jul 2022

Intro
This project in the Pi-Fest music technology Design Challenge aims to create a MIDI synthesizer based on a Raspberry Pi PICO. The previous blogs covered the electronic hardware design. (see links below) This blog covers the firmware. Mostly this firmware is ported from a project linked below, but that project used an Arduino which has differences from a PICO. Notably for this project PICOs have different pinouts, different serial ports and different counter/timers, among other different features. Here is the code I have been running to generate the melodies in these project blogs:.

// PICO Synthesizer
/* Ported By Doug Wong from:
 * https://dogemicrosystems.ca/wiki/Dual_AY-3-8910_MIDI_module
 */

// Uncomment to enable traiditonal serial midi
#define SERIALMIDI

// Uncomment to enable USB midi
//#define USBMIDI

// Uncomment to enable debugging output over USB serial
//#define DEBUG

#include <Arduino.h>
//#include <avr/io.h>

#include "RP2040_PWM.h" 
 
#ifdef USBMIDI
#include "MIDIUSB.h"
#endif

// We borrow one struct from MIDIUSB for traditional serial midi, so define it if were not using USBMIDI
#ifndef MIDIUSB_h
typedef struct
{
  uint8_t header;
  uint8_t byte1;
  uint8_t byte2;
  uint8_t byte3;
} midiEventPacket_t;
#endif

UART Serial2(16, 17, NC, NC);
#ifdef SERIALMIDI
#include <MIDI.h>
MIDI_CREATE_INSTANCE(HardwareSerial, Serial2, MIDI);//Serial2
#endif

typedef unsigned short int ushort;

typedef unsigned char note_t;
#define NOTE_OFF 0

typedef unsigned char midictrl_t;

// Pin driver ---------------------------------------------

static const int dbus[8] = {0, 1, 2, 3, 4, 5, 6, 7};

static const ushort
  BC2_A = 9,
  BDIR_A = 10,
  BC2_B = 12,
  BDIR_B = 13,
  nRESET = 15,
  clkOUT = 14;                  // 1MHz clock pin

static const ushort DIVISOR = 7; // Set for 1MHz clock

 // #define ayckpin    14    // 1MHz clock pin 
  
 float dutyCycle  = 50.0f;  // square wave = 50% duty cycle
 float freq = 500000.0f;    // would like 1 MHz, just testing at 500KHz
 
 RP2040_PWM* MHz; // high freq clock instance

void clocksetup() 
 { 
      MHz = new RP2040_PWM(clkOUT, freq, dutyCycle);  // setup MHz clock
      MHz ->setPWM();                                // start MHz clock
 } 

static void setData(unsigned char db) {
  unsigned char bit = 1;
  for (ushort i = 0; i < 8; i++) {
    digitalWrite(dbus[i], (db & bit) ? HIGH : LOW);
    bit <<= 1;
  }
}

static void writeReg_A(unsigned char reg, unsigned char db) {
  // This is a bit of an odd way to do it, BC1 is kept low and NACT, BAR, IAB, and DWS are used.
  // BC1 is kept low the entire time.
  
  // Inactive (BDIR BC2 BC1 0 0 0)
  digitalWrite(BDIR_A, LOW);
  digitalWrite(BC2_A, LOW);

  //Set register address
  setData(reg);

  // BAR (Latch) (BDIR BC2 BC1 1 0 0)
  digitalWrite(BDIR_A, HIGH);

  // Inactive (BDIR BC2 BC1 0 0 0)
  digitalWrite(BDIR_A, LOW);
  
  //Set register contents
  setData(db);

  // Write (BDIR BC2 BC1 1 1 0)
  digitalWrite(BC2_A, HIGH);
  digitalWrite(BDIR_A, HIGH);

  // Inactive (BDIR BC2 BC1 0 0 0)
  digitalWrite(BC2_A, LOW);
  digitalWrite(BDIR_A, LOW);
}

static void writeReg_B(unsigned char reg, unsigned char db) {
  // This is a bit of an odd way to do it, BC1 is kept low and NACT, BAR, IAB, and DWS are used.
  // BC1 is kept low the entire time.
  
  // Inactive (BDIR BC2 BC1 0 0 0)
  digitalWrite(BDIR_B, LOW);
  digitalWrite(BC2_B, LOW);

  //Set register address
  setData(reg);

  // BAR (Latch) (BDIR BC2 BC1 1 0 0)
  digitalWrite(BDIR_B, HIGH);

  // Inactive (BDIR BC2 BC1 0 0 0)
  digitalWrite(BDIR_B, LOW);
  
  //Set register contents
  setData(db);

  // Write (BDIR BC2 BC1 1 1 0)
  digitalWrite(BC2_B, HIGH);
  digitalWrite(BDIR_B, HIGH);

  // Inactive (BDIR BC2 BC1 0 0 0)
  digitalWrite(BC2_B, LOW);
  digitalWrite(BDIR_B, LOW);
}

// AY-3-8910 driver ---------------------------------------

class PSGRegs {
public:
  enum {
    TONEALOW = 0,
    TONEAHIGH,
    TONEBLOW,
    TONEBHIGH,
    TONECLOW,
    TONECHIGH,
    NOISEGEN,
    MIXER,
    
    TONEAAMPL,
    TONEBAMPL,
    TONECAMPL,
    ENVLOW,
    ENVHIGH,
    ENVSHAPE,
    IOA,
    IOB
  };
  
  unsigned char regs_A[16];
  unsigned char regs_B[16];

  unsigned char lastregs_A[16];
  unsigned char lastregs_B[16];

  void init() {
    for (int i = 0; i < 16; i++) {
      regs_A[i] = lastregs_A[i] = 0xFF;
      writeReg_A(i, regs_A[i]);

      regs_B[i] = lastregs_B[i] = 0xFF;
      writeReg_B(i, regs_B[i]);
    }
  }
  
  void update() {
    for (int i = 0; i < 16; i++) {
      if (regs_A[i] != lastregs_A[i]) {
        writeReg_A(i, regs_A[i]);
        lastregs_A[i] = regs_A[i];
      }

      if (regs_B[i] != lastregs_B[i]) {
        writeReg_B(i, regs_B[i]);
        lastregs_B[i] = regs_B[i];
      }
    }
  }

  void setTone(ushort ch, ushort divisor, ushort ampl) {
    if (ch > 2) {
      //reduce channel to usable range
      ch = ch - 3;
      //use regs_B
      regs_B[TONEALOW  + (ch<<1)] = (divisor & 0xFF);
      regs_B[TONEAHIGH + (ch<<1)] = (divisor >> 8);
      regs_B[TONEAAMPL + ch] = ampl;
      
      ushort mask = (8+1) << ch;
      regs_B[MIXER] = (regs_B[MIXER] | mask) ^ (1 << ch);

      return;
    }
    
    regs_A[TONEALOW  + (ch<<1)] = (divisor & 0xFF);
    regs_A[TONEAHIGH + (ch<<1)] = (divisor >> 8);
    regs_A[TONEAAMPL + ch] = ampl;
    
    ushort mask = (8+1) << ch;
    regs_A[MIXER] = (regs_A[MIXER] | mask) ^ (1 << ch);
  }

  void setToneAndNoise(ushort ch, ushort divisor, ushort noisefreq, ushort ampl) {
    if (ch > 2) {
      //reduce channel to usable range
      ch = ch - 3;
      //use regs_B
      regs_B[TONEALOW  + (ch<<1)] = (divisor & 0xFF);
      regs_B[TONEAHIGH + (ch<<1)] = (divisor >> 8);
      regs_B[NOISEGEN] = noisefreq;
      regs_B[TONEAAMPL + ch] = ampl;
      
      ushort mask = (8+1) << ch;
      ushort bits = (noisefreq < 16 ? 8 : 0) + (divisor > 0 ? 1 : 0);
      regs_B[MIXER] = (regs_B[MIXER] | mask) ^ (bits << ch);

      return;
    }
    
    regs_A[TONEALOW  + (ch<<1)] = (divisor & 0xFF);
    regs_A[TONEAHIGH + (ch<<1)] = (divisor >> 8);
    regs_A[NOISEGEN] = noisefreq;
    regs_A[TONEAAMPL + ch] = ampl;
    
    ushort mask = (8+1) << ch;
    ushort bits = (noisefreq < 16 ? 8 : 0) + (divisor > 0 ? 1 : 0);
    regs_A[MIXER] = (regs_A[MIXER] | mask) ^ (bits << ch);
  }

  void setEnvelope(ushort divisor, ushort shape) {
    regs_A[ENVLOW]  = (divisor & 0xFF);
    regs_A[ENVHIGH] = (divisor >> 8);
    regs_A[ENVSHAPE] = shape;

    regs_B[ENVLOW]  = (divisor & 0xFF);
    regs_B[ENVHIGH] = (divisor >> 8);
    regs_B[ENVSHAPE] = shape; 
  }
  
  void setOff(ushort ch) {
    if (ch > 2) {
      //reduce channel to usable range
      ch = ch - 3;
      //use regs_B
      ushort mask = (8+1) << ch;
      regs_B[MIXER] = (regs_A[MIXER] | mask);
      regs_B[TONEAAMPL + ch] = 0;
      if (regs_B[ENVSHAPE] != 0) {
        regs_B[ENVSHAPE] = 0;
        update(); // Force flush
      }

      return;
    }
    
    ushort mask = (8+1) << ch;
    regs_A[MIXER] = (regs_A[MIXER] | mask);
    regs_A[TONEAAMPL + ch] = 0;
    if (regs_A[ENVSHAPE] != 0) {
      regs_A[ENVSHAPE] = 0;
      update(); // Force flush
    }
  }
};

static PSGRegs psg;

// Voice generation ---------------------------------------

static const ushort
  MIDI_MIN = 24,
  MIDI_MAX = 96,
  N_NOTES = (MIDI_MAX+1-MIDI_MIN);

static const ushort note_table[N_NOTES] = {
   1911, // MIDI 24, 32.70 Hz
   1804, // MIDI 25, 34.65 Hz
   1703, // MIDI 26, 36.71 Hz
   1607, // MIDI 27, 38.89 Hz
   1517, // MIDI 28, 41.20 Hz
   1432, // MIDI 29, 43.65 Hz
   1351, // MIDI 30, 46.25 Hz
   1276, // MIDI 31, 49.00 Hz
   1204, // MIDI 32, 51.91 Hz
   1136, // MIDI 33, 55.00 Hz
   1073, // MIDI 34, 58.27 Hz
   1012, // MIDI 35, 61.74 Hz
   956, // MIDI 36, 65.41 Hz
   902, // MIDI 37, 69.30 Hz
   851, // MIDI 38, 73.42 Hz
   804, // MIDI 39, 77.78 Hz
   758, // MIDI 40, 82.41 Hz
   716, // MIDI 41, 87.31 Hz
   676, // MIDI 42, 92.50 Hz
   638, // MIDI 43, 98.00 Hz
   602, // MIDI 44, 103.83 Hz
   568, // MIDI 45, 110.00 Hz
   536, // MIDI 46, 116.54 Hz
   506, // MIDI 47, 123.47 Hz
   478, // MIDI 48, 130.81 Hz
   451, // MIDI 49, 138.59 Hz
   426, // MIDI 50, 146.83 Hz
   402, // MIDI 51, 155.56 Hz
   379, // MIDI 52, 164.81 Hz
   358, // MIDI 53, 174.61 Hz
   338, // MIDI 54, 185.00 Hz
   319, // MIDI 55, 196.00 Hz
   301, // MIDI 56, 207.65 Hz
   284, // MIDI 57, 220.00 Hz
   268, // MIDI 58, 233.08 Hz
   253, // MIDI 59, 246.94 Hz
   239, // MIDI 60, 261.63 Hz
   225, // MIDI 61, 277.18 Hz
   213, // MIDI 62, 293.66 Hz
   201, // MIDI 63, 311.13 Hz
   190, // MIDI 64, 329.63 Hz
   179, // MIDI 65, 349.23 Hz
   169, // MIDI 66, 369.99 Hz
   159, // MIDI 67, 392.00 Hz
   150, // MIDI 68, 415.30 Hz
   142, // MIDI 69, 440.00 Hz
   134, // MIDI 70, 466.16 Hz
   127, // MIDI 71, 493.88 Hz
   119, // MIDI 72, 523.25 Hz
   113, // MIDI 73, 554.37 Hz
   106, // MIDI 74, 587.33 Hz
   100, // MIDI 75, 622.25 Hz
   95, // MIDI 76, 659.26 Hz
   89, // MIDI 77, 698.46 Hz
   84, // MIDI 78, 739.99 Hz
   80, // MIDI 79, 783.99 Hz
   75, // MIDI 80, 830.61 Hz
   71, // MIDI 81, 880.00 Hz
   67, // MIDI 82, 932.33 Hz
   63, // MIDI 83, 987.77 Hz
   60, // MIDI 84, 1046.50 Hz
   56, // MIDI 85, 1108.73 Hz
   53, // MIDI 86, 1174.66 Hz
   50, // MIDI 87, 1244.51 Hz
   47, // MIDI 88, 1318.51 Hz
   45, // MIDI 89, 1396.91 Hz
   42, // MIDI 90, 1479.98 Hz
   40, // MIDI 91, 1567.98 Hz
   38, // MIDI 92, 1661.22 Hz
   36, // MIDI 93, 1760.00 Hz
   34, // MIDI 94, 1864.66 Hz
   32, // MIDI 95, 1975.53 Hz
   30, // MIDI 96, 2093.00 Hz
};

struct FXParams {
  ushort noisefreq;
  ushort tonefreq;
  ushort envdecay;
  ushort freqdecay;
  ushort timer;
};

struct ToneParams {
  ushort decay;
  ushort sustain; // Values 0..32
  ushort release;
};

static const ushort MAX_TONES = 4;
static const ToneParams tones[MAX_TONES] = {
  { 30, 24, 10 },
  { 30, 12, 8 },
  { 5,  8,  7 },
  { 10, 31, 30 }
};

class Voice {
public:
  ushort m_chan;  // Index to psg channel 
  ushort m_pitch;
  int m_ampl, m_decay, m_sustain, m_release;
  static const int AMPL_MAX = 1023;
  ushort m_adsr;

  void init (ushort chan) {
    m_chan = chan;
    m_ampl = m_sustain = 0;
    kill();
  }
  
  void start(note_t note, midictrl_t vel, midictrl_t chan) {
    const ToneParams *tp = &tones[chan % MAX_TONES];
    
    m_pitch = note_table[note - MIDI_MIN];
    if (vel > 127) {
      m_ampl = AMPL_MAX;
    }
    else {
      m_ampl = 768 + (vel << 1);
    }
    m_decay = tp->decay;
    m_sustain = (m_ampl * tp->sustain) >> 5;
    m_release = tp->release;
    m_adsr = 'D';
    psg.setTone(m_chan, m_pitch, m_ampl >> 6);
  }

  struct FXParams m_fxp;
  
  void startFX(const struct FXParams &fxp) {
    m_fxp = fxp;
  
    if (m_ampl > 0) {
      psg.setOff(m_chan);
    }
    m_ampl = AMPL_MAX;
    m_adsr = 'X';
    m_decay = fxp.timer;

    psg.setEnvelope(fxp.envdecay, 9); 
    psg.setToneAndNoise(m_chan, fxp.tonefreq, fxp.noisefreq, 31);
  }
  

  void stop() {
    if (m_adsr == 'X') {
      return; // Will finish when ready...
    }
      
    if (m_ampl > 0) {
      m_adsr = 'R';
    }
    else {
      psg.setOff(m_chan);
    }
  }
  
  void update100Hz() {
    if (m_ampl == 0) {
      return;
    }
      
    switch(m_adsr) {
      case 'D':
        m_ampl -= m_decay;
        if (m_ampl <= m_sustain) {
          m_adsr = 'S';
          m_ampl = m_sustain;
        }
        break;

      case 'S':
        break;

      case 'R':
        if ( m_ampl < m_release ) {
          m_ampl = 0;
        }
        else {
          m_ampl -= m_release;
        }
        break;

      case 'X':
        // FX is playing.         
        if (m_fxp.freqdecay > 0) { 
          m_fxp.tonefreq += m_fxp.freqdecay;
          psg.setToneAndNoise(m_chan, m_fxp.tonefreq, m_fxp.noisefreq, 31);
        }
        
        m_ampl -= m_decay;
        if (m_ampl <= 0) {
          psg.setOff(m_chan);
          m_ampl = 0;
        }
        return;
        
      default:
        break;
    }  

    if (m_ampl > 0) {
      psg.setTone(m_chan, m_pitch, m_ampl >> 6);
    }
    else {
      psg.setOff(m_chan);    
    }
  }
  
  bool isPlaying() {
    return (m_ampl > 0);
  }
  
  void kill() {
    psg.setOff(m_chan);
    m_ampl = 0;
  }
};


const ushort MAX_VOICES = 6;

static Voice voices[MAX_VOICES];

// MIDI synthesiser ---------------------------------------

// Deals with assigning note on/note off to voices

static const uint8_t PERC_CHANNEL = 9;

static const note_t
  PERC_MIN = 35,
  PERC_MAX = 50;
  
static const struct FXParams perc_params[PERC_MAX-PERC_MIN+1] = {
  // Mappings are from the General MIDI spec at https://www.midi.org/specifications-old/item/gm-level-1-sound-set
  
  // Params are: noisefreq, tonefreq, envdecay, freqdecay, timer
  
  { 9, 900, 800, 40, 50 },   // 35 Acoustic bass drum
  { 8, 1000, 700, 40, 50 },  // 36 (C) Bass Drum 1
  { 4, 0, 300, 0, 80 },      // 37 Side Stick
  { 6, 0, 1200, 0, 30  },    // 38 Acoustic snare
  
  { 5, 0, 1500, 0, 90 },     // 39 (D#) Hand clap
  { 6, 400, 1200, 11, 30  }, // 40 Electric snare
  { 16, 700, 800, 20, 30 },  // 41 Low floor tom
  { 0, 0, 300, 0, 80 },      // 42 Closed Hi Hat
  
  { 16, 400, 800, 13, 30 },   // 43 (G) High Floor Tom
  { 0, 0, 600, 0, 50 },      // 44 Pedal Hi-Hat
  { 16, 800, 1400, 30, 25 }, // 45 Low Tom
  { 0, 0, 800, 0, 40 },      // 46 Open Hi-Hat
  
  { 16, 600, 1400, 20, 25 }, // 47 (B) Low-Mid Tom
  { 16, 450, 1500, 15, 22 }, // 48 Hi-Mid Tom
  { 1, 0, 1800, 0, 25 },     // 49 Crash Cymbal 1
  { 16, 300, 1500, 10, 22 }, // 50 High Tom
};
  
  

static const int REQ_MAP_SIZE = (N_NOTES+7) / 8;
static uint8_t m_requestMap[REQ_MAP_SIZE];
  // Bit is set for each note being requested
static  midictrl_t m_velocity[N_NOTES];
  // Requested velocity for each note
static  midictrl_t m_chan[N_NOTES];
  // Requested MIDI channel for each note
static uint8_t m_highest, m_lowest;
  // Highest and lowest requested notes

static const uint8_t NO_NOTE = 0xFF;
static const uint8_t PERC_NOTE = 0xFE;
static uint8_t m_playing[MAX_VOICES];
  // Which note each voice is playing

static const uint8_t NO_VOICE = 0xFF;
static uint8_t m_voiceNo[N_NOTES];
  // Which voice is playing each note
  

static bool startNote(ushort idx) {
  for (ushort i = 0; i < MAX_VOICES; i++) {
    if (m_playing[i] == NO_NOTE) {
      voices[i].start(MIDI_MIN + idx, m_velocity[idx], m_chan[idx]);
      m_playing[i] = idx;
      m_voiceNo[idx] = i;
      return true;
    }
  }
  return false;
}
  
static bool startPercussion(note_t note) {
  ushort i;
  for (i = 0; i < MAX_VOICES; i++) {
    if (m_playing[i] == NO_NOTE || m_playing[i] == PERC_NOTE) {
      if (note >= PERC_MIN && note <= PERC_MAX) {
        voices[i].startFX(perc_params[note-PERC_MIN]);
        m_playing[i] = PERC_NOTE;
      }
      return true;
    }        
  }
  return false;
}
    
static bool stopNote(ushort idx) {
  uint8_t v = m_voiceNo[idx];
  if (v != NO_VOICE) {
    voices[v].stop();
    m_playing[v] = NO_NOTE;
    m_voiceNo[idx] = NO_VOICE;
    return true;
  }
  return false;
}

static void stopOneNote() {
  uint8_t v, chosen = NO_NOTE;

  // At this point we have run out of voices.
  // Pick a voice and stop it. We leave a voice alone
  // if it's playing the highest requested note. If it's
  // playing the lowest requested note we look for a 'better'
  // note, but stop it if none found.

  for (v = 0; v < MAX_VOICES; v++) {
    uint8_t idx = m_playing[v];
    if (idx == NO_NOTE) {// Uh? Perhaps called by mistake.
      return;
    }

    if (idx == m_highest) {
      continue;
    }

    if (idx == PERC_NOTE) {
      continue;
    }
      
    chosen = idx;
    if (idx != m_lowest) {
      break;
    }
    // else keep going, we may find a better one
  }

  if (chosen != NO_NOTE) {
    stopNote(chosen);
  }
}

static void updateRequestedNotes() {
  m_highest = m_lowest = NO_NOTE;
  ushort i,j;
    
  // Check highest requested note is playing
  // Return true if note was restarted; false if already playing 
  for (i = 0; i < REQ_MAP_SIZE; i++) {
    uint8_t req = m_requestMap[i];
    if (req == 0) {
      continue;
    }

    for (j = 0; j < 8; j++) {
      if (req & (1 << j)) {
        ushort idx = i*8 + j;
        if (m_lowest == NO_NOTE || m_lowest > idx) {
          m_lowest = idx;
        }
        if (m_highest==NO_NOTE || m_highest < idx)  {
          m_highest = idx;
        }
      }
    }
  }
}

static bool restartANote() {
  if (m_highest != NO_NOTE && m_voiceNo[m_highest] == NO_VOICE) {
    return startNote(m_highest);
  }

  if (m_lowest != NO_NOTE && m_voiceNo[m_lowest] == NO_VOICE) {
    return startNote(m_lowest);
  }

  return false;
}
  
static void synth_init () {
  ushort i;

  for (i = 0; i < REQ_MAP_SIZE; i++) {
    m_requestMap[i] = 0;
  }

  for (i = 0; i < N_NOTES; i++) {
    m_velocity[i] = 0;
    m_voiceNo[i] = NO_VOICE;
  }
    
  for (i = 0; i < MAX_VOICES; i++) {
    m_playing[i] = NO_NOTE;
  }
    
  m_highest = m_lowest = NO_NOTE;
}

static void noteOff(midictrl_t chan, note_t note, midictrl_t vel) {
  if (chan == PERC_CHANNEL || note < MIDI_MIN || note > MIDI_MAX) {
    return; // Just ignore it
  }

  ushort idx = note - MIDI_MIN;

  m_requestMap[idx/8] &= ~(1 << (idx & 7));
  m_velocity[idx] = 0;
  updateRequestedNotes();
    
  if (stopNote(idx)) {
    restartANote();
  }
}

static void noteOn(midictrl_t chan, note_t note, midictrl_t vel) {
  if (vel == 0) {
    noteOff(chan, note, 0);
    return;
  }

  if (chan == PERC_CHANNEL) {
    if (!startPercussion(note)) {
      stopOneNote();
      startPercussion(note);
    }
    return;
  }
    
  // Regular note processing now
    
  if (note < MIDI_MIN || note > MIDI_MAX) {
    return; // Just ignore it
  }

  ushort idx = note - MIDI_MIN;
    
  if (m_voiceNo[idx] != NO_VOICE) {
    return; // Already playing. Ignore this request.
  }

  m_requestMap[idx/8] |= 1 << (idx & 7);
  m_velocity[idx] = vel;
  m_chan[idx] = chan;
  updateRequestedNotes();
    
  if (!startNote(idx)) {
     stopOneNote();
     startNote(idx);
  }
}
  
static void update100Hz() {
  for (ushort i = 0; i < MAX_VOICES; i++) {
    voices[i].update100Hz();
    if (m_playing[i] == PERC_NOTE && ! (voices[i].isPlaying())) {
      m_playing[i] = NO_NOTE;
      restartANote();
    }        
  }
}

// Main code ----------------------------------------------

static unsigned long lastUpdate = 0;

void setup() {
  // Hold in reset while we set up the reset
  pinMode(nRESET, OUTPUT);
  digitalWrite(nRESET, LOW);

  pinMode(clkOUT, OUTPUT);
  digitalWrite(clkOUT, LOW);

  pinMode(BC2_A, OUTPUT);
  digitalWrite(BC2_A, LOW); // BC2 low
  pinMode(BDIR_A, OUTPUT);
  digitalWrite(BDIR_A, LOW); // BDIR low

  pinMode(BC2_B, OUTPUT);
  digitalWrite(BC2_B, LOW); // BC2 low
  pinMode(BDIR_B, OUTPUT);
  digitalWrite(BDIR_B, LOW); // BDIR low

  for (ushort i = 0; i < 8; i++) {
    pinMode(dbus[i], OUTPUT);
    digitalWrite(dbus[i], LOW); // Set bus low
  }

  delay(100);
  digitalWrite(nRESET, HIGH); // Release Reset
  delay(10);

  lastUpdate = millis();
  
  psg.init();
  for (ushort i = 0; i < MAX_VOICES; i++) {
    voices[i].init(i);
  }
  synth_init();

#ifdef DEBUG
    Serial.begin(115200);
#endif

#ifdef SERIALMIDI
  // Initiate MIDI communications, listen to all channels
  MIDI.begin(MIDI_CHANNEL_OMNI);
#endif
}

void handleMidiMessage(midiEventPacket_t &rx) {
  if (rx.header==0x9) {// Note on
    noteOn(rx.byte1 & 0xF, rx.byte2, rx.byte3);
  }
  else if (rx.header==0x8) {// Note off
    noteOff(rx.byte1 & 0xF, rx.byte2, rx.byte3);
  }
  else if (rx.header==0xB) {// Control Change
    if (rx.byte2 == 0x78 || rx.byte2 == 0x79 || rx.byte2 == 0x7B) {// AllSoundOff, ResetAllControllers, or AllNotesOff
      // Kill Voices
      for (ushort i = 0; i < MAX_VOICES; i++) {
        voices[i].kill();
      }
    }
  }
}

void loop() {
  midiEventPacket_t rx;

#ifdef USBMIDI
  rx = MidiUSB.read();

#ifdef DEBUG
  //MIDI debugging
  if (rx.header != 0) {
    Serial.print("Received USB: ");
    Serial.print(rx.header, HEX);
    Serial.print("-");
    Serial.print(rx.byte1, HEX);
    Serial.print("-");
    Serial.print(rx.byte2, HEX);
    Serial.print("-");
    Serial.println(rx.byte3, HEX);
  }
#endif

  handleMidiMessage(rx);
#endif

#ifdef SERIALMIDI
  //Check for serial MIDI messages
  //MIDI.read();
  while (MIDI.read()) {
    // Create midiEventPacket_t
    rx = 
      {
        byte(MIDI.getType() >>4), 
        byte(MIDI.getType() | ((MIDI.getChannel()-1) & 0x0f)), /* getChannel() returns values from 1 to 16 */
        MIDI.getData1(), 
        MIDI.getData2()
      };

#ifdef DEBUG
    //MIDI debugging
    if (rx.header != 0) {
      Serial.print("Received MIDI: ");
      Serial.print(rx.header, HEX);
      Serial.print("-");
      Serial.print(rx.byte1, HEX);
      Serial.print("-");
      Serial.print(rx.byte2, HEX);
      Serial.print("-");
      Serial.println(rx.byte3, HEX);
    }
#endif

    handleMidiMessage(rx);
  }
#endif

  unsigned long now = millis();
  if ((now - lastUpdate) > 10) {
    update100Hz();
    lastUpdate += 10;
  }
  
  psg.update();
}

Code Issues
There is one issue with this firmware - it is not generating the high frequency clock properly. This clock is used by the programmable sound generator chips and should be 1 MHz. Until I get that clock working, I am using an external clock.
I am certain the PICO can generate this clock simply by dividing its main clock by 125, but in the Arduino IDE how to do it is a bit of a mystery to me.
I found a library that claims it can do it, but I haven't got it figured out either.
Using that library I wrote the sketch below that does nothing except generate a high frequency clock and flash an LED. It works up to 500 KHz but ceases to have any output above 500KHz. (even though it compiles and runs with no error messages) I assume it has something to do with how big a number the Arduino IDE or library can handle, but it isn't clear to me what the work around is.
The bigger code above has the same clock code but it doesn't even generate a clock at any frequency, so I am doing something idiotic there as well. (that code also compiles and runs with no error messages)
I will continue to worry away at it, but right now I have tunnel vision on it.

#include "RP2040_PWM.h" 
#define ckpin    14    // 1MHz clock pin 
  
 float dutyCycle  = 50.0f; 
 float freq = 500000.0f;        // 1MHz , 500KHz is just a test

 RP2040_PWM* MHz; // MHz clock instance

 void setup() 
 { 
      MHz = new RP2040_PWM(ckpin, freq, dutyCycle);  // setup MHz clock
      MHz ->setPWM();                                // start MHz clock

  pinMode(LED_BUILTIN, OUTPUT); // initialize digital pin LED_BUILTIN as an output.
  pinMode(15, OUTPUT);  //test point
}

void loop() {
  digitalWrite(LED_BUILTIN, HIGH);   // turn the LED on (HIGH is the voltage level)
  digitalWrite(15, HIGH);            //test point
  delay(500);                       // wait for a second
  digitalWrite(LED_BUILTIN, LOW);    // turn the LED off by making the voltage LOW
  digitalWrite(15, LOW);             //test point
  delay(1500);                       // wait for a second
}

If you enjoy the challenge of critiquing the firmware, I am all ears.

Mystery Melody Medley 3
Here is the third Mystery Melody Medley identification video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Conclusions and Discussion of this Blog
Firmware is clearly not my strong suit. I got far enough that the synthesizer works, but I am not happy with the firmware yet. At some point I will figure it out, but right now I need to get some material published before the deadline.
Next blog will cover mechanical design of the enclosure.

Relevant Links:
Blog 1 - Introduction and circuit schematic description
Blog 2 - PCB layout and manufacturing
Blog 3 - Firmware and issues
Blog 4 - Mechanical enclosure design and features
Blog 5 - Project summary and discussion
Pi-Fest Music Contest page
AY-3-8910 Datasheet
Dual Synth link

  • Sign in to reply
Parents
  • robogary
    robogary over 4 years ago

    Home on the Range, 3 ships, the last 2 sounded familiar but couldnt place them

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 4 years ago

    Home on the Range, 3 ships, the last 2 sounded familiar but couldnt place them