Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog Pi Control Hub: Spoke 1 :Security Camera (continued)- Photo gallery of the intruders
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
  • Author Author: carmelito
  • Date Created: 29 Jul 2016 8:20 PM Date Created
  • Views 982 views
  • Likes 3 likes
  • Comments 3 comments
  • picontrolhub
  • raspberry pi zero
  • piiot
  • raspberry pi
  • piiot challenge
Related
Recommended

Pi Control Hub: Spoke 1 :Security Camera (continued)- Photo gallery of the intruders

carmelito
carmelito
29 Jul 2016

This is continuation of previous blog post , where we installed motion to stream video from the Pi Camera, which acts as live preview of the security camera.For more details check out -

Pi Control Hub: Spoke 1 :Security Camera - setting up Motion to stream video

 

As part of this blog post we will setup a simple web server on the Pi using lighttpd and  Single File PHP Gallery 4.6.1 by Kenny Svalgaard to display images that motion stores when an intruder/movement is detected.(I have used the single file PHP gallery  a couple of years back, when using the original Pi model B and the Pi Camera on a simple bird watching project for the summer and which means I can vouch for it ).  As part of the gallery as shown in the picture below, you can preview all the picture taken when movement is detected and also click on the pictures enlarge and even download the full size image to your laptop, if you have to image..

image

 

In addition, I am going to move the Pi NoIR cam + SD card + WiFi USB adapter to the Pi Zero as showing in the picture below, because I plan on using the Pi B+ on another spoke.

image

 

Here are the steps/list of commands to follow to setup lighttpd followed by single file PHP gallery

#1 SSH into your Pi and Install lighttpd

    sudo apt-get install lighttpd

 

#2 Install the PHP packages

       sudo apt-get install php5-common php5-cgi php5

    at this point also enable Fastcgi module using the command

        sudo lighty-enable-mod fastcgi-php

 

#3 Update the permissions of the www directory which was created by the install of  lighttpd

      Change the directory owner and group to

           sudo chown www-data:www-data /var/www

      Give the necessay permisions to the folder

             sudo chmod 775 /var/www

      Then add pi to the www-data group

           sudo usermod -a -G www-data pi

 

#4 Stop and Start the the lighttpd service and test

       sudo service lighttpd stop

        sudo service lighttpd start

     or you can also use - sudo service lighttpd restart , if everything is setup correctly, when you open your browser to test - http://ipaddressOfPi

image

In case you come across an error/or the page does not load, check your error logs to debug

     sudo tail /var/log/lighttpd/error.log

 

#5 Optionally, if you would like to run a test with a small html page of your own, use the following commands

      cd /var/www/html/

    rename the exist file that serves the page in the screenshot above

       sudo mv index.lighttpd.html index.lighttpd.htmlxx

    create an index.html file

        sudo nano index.html

    Copy paste the following code

     

<html>
<head>
<title>Lighttpd test</title>
</head>
<body>
<h1>Testing Lighttpd and PHP setup</h1>
<p>Yes !!! it is working.</p>
<p><?php phpinfo();?></p>
</body>
</html>

    

        ctrl+X to save the file in the nano editor

    Stop and start the lighttpd service

       sudo service lighttpd stop

       sudo service lighttpd start

image

 

#6 install php5-gd image processing libary to show the thumbnails on the web page, this is required Single File PHP Gallery

   sudo apt-get install php5-gd

 

#7 downlad the Single File PHP Gallery

     get the zip files from http://sye.dk/sfpg/

        sudo wget http://sye.dk/sfpg/Single_File_PHP_Gallery_4.6.1.zip

     Unzipping and move the files to

         sudo unzip Single_File_PHP_Gallery_4.6.1.zip -d /var/www/html

     also dont forget to rename the index.html file created in step 5

        sudo mv index.html index.htmlxx

 

 

#8 Upload acouple of picture to the html folder or take a couple of pictures using the pi camera

     use a FTP tool like filezilla to upload a couple of images to the /var/www/html

     Or if you dont have an FTP tool navigate to the  /var/www/html folder and take a couple of pictures using

         sudo raspistill -o test1.jpg

      once done open a URL in the browser http://ipaddressOfPi , where you should see the images you have just taken.

image

 

#9 Setting up the motion.conf file to point to the newly create pics folder

     Now create a new folder called pics

       sudo mkdir pics

    Stop the motion service, if you have not done it as part of the previous steps

       sudo service motion stop

   Assign ownership to the target directory for motion

       sudo chown motion /var/www/html/pics

   Now modify the following parameter in the motion.conf file

      sudo nano /etc/motion/motion.conf

    - the target direcotry the new one we created

        target_dir /var/www/html/pics

      image

    - Set a new threshold value to determine when motion is detect, i bumped mine to 3500.You will have to experiment with this value ..Basically Threshold for number of changed pixels in an          image that triggers motion detection (default: 1500).

        threshold 3500

    - And I also choose to have turn off video by setting the ffmpeg_output_movies to off

       ffmpeg_output_movie off

 

#10 Start motion service and test

         sudo service motion start

     now when you click on the pics section in the browser  http://ipaddressOfPi , you should see all the images captured by motion , when an intruder is detected

image

  <in my case i am using random things around me on my table image>, you can also click on the picture enlarge it as shown in the picture below and click the link to download the full size image to your laptop.

image

 

And yes, the steam from the pi cam is still available at http://ipaddressOfPi:8081

  • Sign in to reply
Parents
  • DAB
    DAB over 10 years ago

    Agreed, very nice post.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • carmelito
    carmelito over 10 years ago in reply to DAB

    Thanks for the comment @ DAB and clem57

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • carmelito
    carmelito over 10 years ago in reply to DAB

    Thanks for the comment @ DAB and clem57