Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog Pi Control Hub: The HUB
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
  • Author Author: carmelito
  • Date Created: 29 Aug 2016 1:18 AM Date Created
  • Views 1027 views
  • Likes 3 likes
  • Comments 1 comment
  • sense hat
  • picontrolhub
  • piiot
  • raspberry pi
  • chromium
  • piiot challenge
  • music
  • raspberrypi3
Related
Recommended

Pi Control Hub: The HUB

carmelito
carmelito
29 Aug 2016

It is now time!! to put the all the electronic components together into a nice enclosure, which I am calling the HUB image ,using some 3D printing with Wood filament and some basic wood working using a Dremel tool.Here is a gallery of the finished HUB

 

{gallery}Pi3  Control HUB

image

Front

image

Top - with the Pi Camera just out of its slot

image

Pi Camera which can be easily moved around with a flexible gear tie and a 3D printed holder

image

Bottom, sense Hat connected to Pi 3, this is to use at night in the dark..

image

Top - speakers to play music

 

 

 

As part of the build , start of by cutting a couple of Hobby wood board as shown in the pictures below

{gallery}Building the Wooden Frame

 

image

Mark the size of the components like the Pi 7 inch screen , Speakers ..

image

Use the Dremel with a cutting bit, for the 7 inch display

image

Cutting slots for the speakers

image

slot for the Sense Hat mounted on the Pi3

image

Gluing to build the frame, and leaving to dry over night

image

Adding wood putty to fill in the gaps

image

Sanding any rough edges

image

Staining and leaving in to dry for a couple of hours

image

Finishing of with Painters Touch, which gives it a nice glossy and semi waterproof finish

 

Putting the speakers together, download and 3D print the STL files attached below, using wood filament. Here I am using wood filament to 3D print, so that I can sand it and then Stain it, so that it matches with the wooden fame .

Also 3D print a holder for the Sense hat and the Raspberry Pi 3 using wood filament, here is the link to the wood filament I am using from digitmakers.ca

https://digitmakers.ca/product/3d-printer-wood-filament-natural-brown/

Suggest slicer setting to use for 3D printing with wood filament

Layer height - 0.2 mm

Infill density - 40%

Temperature - 200 C

 

{gallery} Putting the Speaker together

image

3D printing the speaker holder, you will need another copy of this ..

image

Staining the 3D printed parts. Dont forget to sand the parts before staining

image

Glue the componets together, here you can use the same wood glue used for the wooden frame

image

Adding the Grid

 

 

Now, lets add a Handle and the 3D printing part for the Pi Camera to top of the Hub frame. To hold the camera I decided to use a flexible gear tie , which means you can point the camera in any direction you want, by warping the gear tie to the handle.

 

For 3D printing the Pi Camera holder I am using black 1.75mm PLA and here are some suggested slicer setting to use for 3D printing with wood filament

Layer height - 0.3 mm

Infill density - 20%

Temperature - 205 C

 

I purchased the handle and the Gear tie at a local hardware store called HomeDepot.ca and also bought matching screws and nuts..

 

{gallery}Adding Handle and Pi Camera

image

Screwing the Handle to the top

image

3D print the Pi Camera holder

image

Camera will fit in the slot and can be pulled out the stream video when ever required

image

To hold the camera in place use a flexible gear tie

 

Adding the Pi3 , sense hat and all the other components to the inside of the hub frame. For more info on the speaker circuit and how to setup Mopidy to play music, check out the blog at

Pi Control Hub: Music with Mopidy and Home Assistant

 

{gallery} Adding Pi3 and other components inside the frame

image

Add the sense hat to the 3D printed holder

image

Cut out a piece of plastic to diffuse the RGB leds of the sense hat , I am using a cover piece from an old notebook

image

Add the Pi Screen and the Pi3 to the frame, attach the cable for the screen , here I am using the Pi camera cable to connect the Pi3 and Screen driver

image

Add the speakers and the Pi Camera

image

3D print holder for the Audio Amplifier and the Lipo charger

image

Adding Lipo, Audio Amp, switch and Lipo charger to the frame.

image

Gluing the components together

image

 

Now to run Home-Assistant on Pi touch screen as shown in the picture below, we will have to install Chrome. Chromium is not part of the default Raspbian packages , which means we will have to run the following commands to work around this

 

wget -qO - http://bintray.com/user/downloadSubjectPublicKey?username=bintray | sudo apt-key add -
echo "deb http://dl.bintray.com/kusti8/chromium-rpi jessie main" | sudo tee -a /etc/apt/sources.list
sudo apt-get update
sudo apt-get install chromium-browser rpi-youtube -y

 

image

Here is the link to the Raspberry Pi forum post,where I found this workaround

https://www.raspberrypi.org/forums/viewtopic.php?t=121195

Attachments:
STLsPiTFTPi3.zip
STLsSpeakerAudioAmpCharger.zip
STLPiCamera.zip
  • Sign in to reply
Parents
  • volly
    volly over 10 years ago

    carmelito. Cool

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • volly
    volly over 10 years ago

    carmelito. Cool