Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [Pi IoT] - Smarter Spaces #3 - Remote Horse Feeder System
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
  • Author Author: jomoenginer
  • Date Created: 9 Jul 2016 5:07 PM Date Created
  • Views 1198 views
  • Likes 2 likes
  • Comments 9 comments
Related
Recommended

[Pi IoT] - Smarter Spaces #3 - Remote Horse Feeder System

jomoenginer
jomoenginer
9 Jul 2016

So, I was able to get the iLumi controlled via a python script that in turn I was able to add to OpenHAB and could control the iLumi BR30 from an OpenHAB ColorPicker, however when I attempted to add the EnOcean Pi 902 to the Raspberry Pi 3 and performed the update/upgrade to support the device I lost both the Wi-Fi and the Bluetooth functionality of the Raspberry Pi 3.   I was able to recover the W-Fi connection on the RasPi 3 by performing a dist-upgrade and then updating the firmware on the system to 4.4.3.  This corrected the Wi-Fi issue but I am still unable to get the Bluetooth device on the RasPi 3 to enable.  The system seems to think there is no bluetooth device on the board which I know there is one since it was working prior to the upbreak.  I'll have to see if I can get this to come up again or just add a usb bluetooth dongle to the board to get past it.

This assisted me in getting the WiFi back up and working:

http://raspberrypi.stackexchange.com/questions/43474/how-to-enable-wi-fi-channel-12-on-raspberry-pi-3

 

Also, I was never able to get the RasPi to see the EnOcean Pi 902 so I was wondering if anyone knew if the device is supported with Raspberry Pi 3 and Jessie or do I need to use the RasPi B+ to connect the EnOcean Pi 902.  

  • Sign in to reply

Top Comments

  • fvan
    fvan over 10 years ago +2
    Hi Jon, i got my EnOceanPi 868 to work, including Wifi and BLE. All is described here: [Pi IoT] Alarm Clock #05: EnOcean Pi and Sensors Good luck! Frederick
  • jomoenginer
    jomoenginer over 10 years ago +1
    Still no success with getting the BLE device to enable, but I did find some more info regarding this. Apparently at kernel 4.4.9 there was a switch from ttyAMA0 to serial1; I'm currently running with 4…
  • jomoenginer
    jomoenginer over 10 years ago in reply to jomoenginer +1
    Okay, finally a bit of success. After searching the web and attempting many changes to the RasPi 3 config, I finally stumbled on the needed info to get the On Board BLE device working again on the RasPi…
Parents
  • fvan
    fvan over 10 years ago

    Hi Jon,

     

    i got my EnOceanPi 868 to work, including Wifi and BLE. All is described here: [Pi IoT] Alarm Clock #05: EnOcean Pi and Sensors

     

    Good luck!

    Frederick

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 10 years ago in reply to fvan

    Frederick,

     

    I appreciate the reply and the link to your write up for your Alarm Clock which looks very interesting.  However, My RasPi is not even seeing the EnOcean Pi device as well as the built-in BLE connection.

    I have run through your instructions up to running the EnOceanSpy tool, but when I run that command, the utility just hangs and does not return.

     

    I'll have to see what is happening with the device or just switch with a different RasPi .

     

    Thnaks,

     

    Jon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jomoenginer
    jomoenginer over 10 years ago in reply to fvan

    Frederick,

     

    I appreciate the reply and the link to your write up for your Alarm Clock which looks very interesting.  However, My RasPi is not even seeing the EnOcean Pi device as well as the built-in BLE connection.

    I have run through your instructions up to running the EnOceanSpy tool, but when I run that command, the utility just hangs and does not return.

     

    I'll have to see what is happening with the device or just switch with a different RasPi .

     

    Thnaks,

     

    Jon