Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [Pi IoT] Alarm Clock #09: Philips Hue
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
  • Author Author: fvan
  • Date Created: 20 Jul 2016 8:01 PM Date Created
  • Views 1686 views
  • Likes 4 likes
  • Comments 7 comments
  • fvan_piiot
  • piiot
  • feature_tutorial
  • philips_hue
Related
Recommended

[Pi IoT] Alarm Clock #09: Philips Hue

fvan
fvan
20 Jul 2016

  • Hue Bridge
  • OpenHAB
    • Items
    • Sitemap
    • Pairing
    • Rules
      • Night Light
      • Wake Up Light
  • Build

 

I'm back! It's been a while since my last update ... I've been moving to a new house and things were quite hectic. On the plus side, I'm getting a new office/lab and a big shed just for me. They're still full of boxes and I can't find half my things though, but that should be cleared in the coming week image

 

imageimage

 

Anyway ... The next component I wanted to integrate in my project were some philips Hue lights. These are RGB remote controlled lights. The first application I'm thinking of, is to install one light in each of my children's room and use it as a night light and wake up light. Using OpenHAB, the light woud turn on when going to bed, and be turned off by the time they fall asleep. In the morning, a similar action would be performed. Turn on the light just before they have to wake up, and a few moments later, turn it off for the rest of the day. Because these lights are RGB, they can be configured to use the theme colour of their rooms.

 

Let's get into the details of this integration image

 

Hue Bridge

 

The Philips Hue Bridge is, as the name implies, a bridge device allowing your smart devices (phone, computer, Raspberry Pi, ...) to control up to 50 Hue lights and accessories. It connects to the network via an ethernet cable and receives an IP address via DHCP. As I'll be controlling the bridge from OpenHAB, it will need to be configured with a static IP address instead. This can be done using the Hue app.

 

imageimage

 

OpenHAB

 

Porting the Hue functionality to OpenHAB is not that hard, using the Hue binding. But that would only give control of the light, as in the app on the smartphone. Although it would be possible to control remotely over the internet, rather than via the local network only.

 

Items

 

As described in the following thread, the item definition for Hue lights in OpenHAB 2.0 is slightly different. Rather than defining them like this:

 

Switch  Hue_Bulb_1_Switch    {hue="1"}
Color   Hue_Bulb_1_Color     {hue="1"}
Dimmer  Hue_Bulb_1_Dimmer    {hue="1;colorTemperature"}

Switch  Hue_Bulb_2_Switch    {hue="2"}
Color   Hue_Bulb_2_Color     {hue="2"}
Dimmer  Hue_Bulb_2_Dimmer    {hue="2;colorTemperature"}

 

The items are defined like this:

 

Switch  Hue_Bulb_1_Switch    {channel="hue:LCT007:0017882155ad:1:color"}
Color   Hue_Bulb_1_Color <colorwheel>    {channel="hue:LCT007:0017882155ad:1:color"}
Dimmer  Hue_Bulb_1_Dimmer    {channel="hue:LCT007:0017882155ad:1:color"}
Dimmer  Hue_Bulb_1_ColorTemperature    {channel="hue:LCT007:0017882155ad:1:color_temperature"}

Switch  Hue_Bulb_2_Switch    {channel="hue:LCT007:0017882155ad:2:brightness"}
Color   Hue_Bulb_2_Color <colorwheel>    {channel="hue:LCT007:0017882155ad:2:color"}
Dimmer  Hue_Bulb_2_Dimmer    {channel="hue:LCT007:0017882155ad:2:brightness"}
Dimmer  Hue_Bulb_2_ColorTemperature    {channel="hue:LCT007:0017882155ad:2:color_temperature"}

 

Sitemap

 

The sitemap is like any other integration, where you define how and where the defined items are visualised.

 

        Frame label="Lights" {
                Switch         item=Hue_Bulb_1_Switch   label="Room 1 Switch"
                Switch         item=Hue_Bulb_2_Switch   label="Room 2 Switch"
                Colorpicker    item=Hue_Bulb_1_Color    label="Room 1 Color"
                Colorpicker    item=Hue_Bulb_2_Color    label="Room 2 Color"
                Slider         item=Hue_Bulb_1_Dimmer   label="Room 1 Brightness"
                Slider         item=Hue_Bulb_2_Dimmer   label="Room 2 Brightness"
                Slider         item=Hue_Bulb_1_ColorTemperature   label="Room 1 Color Temperature"
                Slider         item=Hue_Bulb_2_ColorTemperature   label="Room 2 Color Temperature"
        }

 

 

The above configuration results in something that should look like this:

image

 

Pairing

 

Once the Hue binding was installed, OpenHAB detected the bridge automatically. In order to be able to pair with the bridge and send commands, the button on the bridge needs to be pressed. This is made clear in the "openhab.log" file.

 

After pressing the button, a unique user is created, allowing OpenHAB to interface with the bridge. The bridge then goes from OFFLINE to ONLINE, as stated in the logs:

 

2016-07-19 22:38:31.845 [INFO ] [binding.hue.handler.HueBridgeHandler] - Creating new user on Hue bridge 192.168.0.142 - please press the pairing button on the bridge.
2016-07-19 22:38:41.843 [INFO ] [binding.hue.handler.HueBridgeHandler] - Creating new user on Hue bridge 192.168.0.142 - please press the pairing button on the bridge.
2016-07-19 22:38:51.846 [INFO ] [binding.hue.handler.HueBridgeHandler] - Creating new user on Hue bridge 192.168.0.142 - please press the pairing button on the bridge.
2016-07-19 22:39:01.843 [INFO ] [binding.hue.handler.HueBridgeHandler] - Creating new user on Hue bridge 192.168.0.142 - please press the pairing button on the bridge.
2016-07-19 22:39:11.841 [INFO ] [binding.hue.handler.HueBridgeHandler] - Creating new user on Hue bridge 192.168.0.142 - please press the pairing button on the bridge.
2016-07-19 22:39:21.844 [INFO ] [binding.hue.handler.HueBridgeHandler] - Creating new user on Hue bridge 192.168.0.142 - please press the pairing button on the bridge.
2016-07-19 22:39:21.867 [INFO ] [binding.hue.handler.HueBridgeHandler] - User '9cx84jRFcbP4e7sCRm4FuYr3e7laPR55oDzTpptj' has been successfully added to Hue bridge.
2016-07-19 22:39:21.951 [INFO ] [smarthome.event.ThingUpdatedEvent   ] - Thing 'hue:bridge:0017882155ad' has been updated.
2016-07-19 22:39:31.903 [INFO ] [me.event.ThingStatusInfoChangedEvent] - 'hue:bridge:0017882155ad' changed from OFFLINE (CONFIGURATION_ERROR): Not authenticated - press pairing button on the bridge. to ONLINE
2016-07-19 22:39:31.963 [INFO ] [g.discovery.internal.PersistentInbox] - Added new thing 'hue:LCT007:0017882155ad:3' to inbox.
2016-07-19 22:39:31.965 [INFO ] [smarthome.event.InboxAddedEvent     ] - Discovery Result with UID 'hue:LCT007:0017882155ad:3' has been added.
2016-07-19 22:39:32.011 [INFO ] [smarthome.event.ThingUpdatedEvent   ] - Thing 'hue:bridge:0017882155ad' has been updated.

 

Rules

 

Now begins the fun part: defining automated events using the lights. That's where OpenHAB's powerful rules engine comes into play. Using rules, the wake up light and night light functionality can be implemented. Because both my children have the same routine in general, one set of rules can be applied for both.

 

Night Light

 

This first implementation of the night light has following properties:

  • turn on the light every single day, at 19:00
  • use color blue foor room 1, green for room 2 (children have themed rooms image)
  • use 50% brightness

 

A first timer is created at the same time, set to trigger 1 hour later, to dim the brightness to 10%.

A second timer turn the light completely off, another hour later.

 

import org.joda.time.*
import org.openhab.model.script.actions.Timer


var Timer nightLightDim
var Timer nightLightOff


rule "Night Light"
when
    Time cron "0 0 19 * * ?"   // Every day 19:00 hours
then
    // Light 1
    sendCommand(Hue_Bulb_1_Switch, ON)
    sendCommand(Hue_Bulb_1_Color, HSBType::BLUE)
    sendCommand(Hue_Bulb_1_Dimmer, 50)
    sendCommand(Hue_Bulb_1_ColorTemperature, 0)


    // Light 2
    sendCommand(Hue_Bulb_2_Switch, ON)
    sendCommand(Hue_Bulb_2_Color, HSBType::GREEN)
    sendCommand(Hue_Bulb_2_Dimmer, 50)
    sendCommand(Hue_Bulb_2_ColorTemperature, 0)


    // Timer Dim
    if(nightLightDim!=null) {
       nightLightDim.cancel()
    }
    nightLightDim = createTimer(now.plusMinutes(60)) [|
        sendCommand(Hue_Bulb_1_Dimmer, 10)
        sendCommand(Hue_Bulb_2_Dimmer, 10)
    ]


    // Timer Turn Off
    if(nightLightOff!=null) {
        nightLightOff.cancel()
    }
    nightLightOff = createTimer(now.plusMinutes(120)) [|
        sendCommand(Hue_Bulb_1_Switch, OFF)
        sendCommand(Hue_Bulb_2_Switch, OFF)
    ]
end

 

For testing purposes, I temporarily changed the cron expression to trigger within a few minutes. As expected, the rule triggered, and the lights were configured!

 

The logs show all actions being triggered within less than 100 milliseconds:

 

2016-07-20 21:36:03.346 [INFO ] [smarthome.event.ItemCommandEvent    ] - Item 'Hue_Bulb_1_Switch' received command ON
2016-07-20 21:36:03.361 [INFO ] [marthome.event.ItemStateChangedEvent] - Hue_Bulb_1_Switch changed from OFF to ON
2016-07-20 21:36:03.369 [INFO ] [smarthome.event.ItemCommandEvent    ] - Item 'Hue_Bulb_1_Color' received command 240,100,100
2016-07-20 21:36:03.377 [INFO ] [marthome.event.ItemStateChangedEvent] - Hue_Bulb_1_Color changed from 238,88,0 to 240,100,100
2016-07-20 21:36:03.402 [INFO ] [smarthome.event.ItemCommandEvent    ] - Item 'Hue_Bulb_1_Dimmer' received command 50
2016-07-20 21:36:03.407 [INFO ] [marthome.event.ItemStateChangedEvent] - Hue_Bulb_1_Dimmer changed from 0 to 50
2016-07-20 21:36:03.428 [INFO ] [smarthome.event.ItemCommandEvent    ] - Item 'Hue_Bulb_1_ColorTemperature' received command 0

 

The timer also does its work and reduces the brightness after a given amount of time, as specified in the rule:

 

2016-07-20 21:42:01.321 [INFO ] [smarthome.event.ItemCommandEvent    ] - Item 'Hue_Bulb_1_Dimmer' received command 10

 

Wake Up Light

 

The wake up light does something similar, as it turns on 15 minutes before having to wake up. The exception here is the cron expression takes into account the day of the week. Wouldn't want to wake up the kids too early during the weekend, right? image

 

var Timer wakeUpLightOff


rule "Wake Up Light"
when
    Time cron "0 45 6 * * 1-5"   // Every weekday 6:45 hours
then
    // Light 1
    sendCommand(Hue_Bulb_1_Switch, ON)
    sendCommand(Hue_Bulb_1_Color, HSBType::BLUE)
    sendCommand(Hue_Bulb_1_Dimmer, 80)
    sendCommand(Hue_Bulb_1_ColorTemperature, 0)


    // Light 2
    sendCommand(Hue_Bulb_2_Switch, ON)
    sendCommand(Hue_Bulb_2_Color, HSBType::GREEN)
    sendCommand(Hue_Bulb_2_Dimmer, 80)
    sendCommand(Hue_Bulb_2_ColorTemperature, 0)


    // Timer
    if(wakeUpLightOff!=null) {
        wakeUpLightOff.cancel()
    }
    wakeUpLightOff = createTimer(now.plusMinutes(30)) [|
        sendCommand(Hue_Bulb_1_Switch, OFF)
        sendCommand(Hue_Bulb_2_Switch, OFF)
    ]
end

 

Build

 

To build the frame of the light and be able to mount it on the beds, I experimented with a new method (new for me at least): heat forming acrylic. Applying heat to certain areas of a piece of acrylic, it can be formed in different shapes. Since this is my first time doing it, the shape is not so complex, but it turned out quite well if I may say so myself.

 

Here are some pictures of the acrylic being bent into shape:

imageimageimage

 

As you can see, it's possible to make interesting shapes out of a straight piece of acrylic. The tricky part is figuring out the best order to perform the bends in.

 

To apply heat, I used a mini blow torch and passed back and forth in a line across the section that needed to be bent. Using a different head of the tool, I carved out a hole in the top section to fit the light's socket. Handy little tool! image

 

imageimageimage

 

Now I just need to repeat this for the second bedroom!

 

With most of the desired components integrated, I'll start working on the actual alarm clock portion of the project. There's only a bit more than a month left!

 


image

 


Navigate to the next or previous post using the arrows.

image
  • Sign in to reply

Top Comments

  • rhe123
    rhe123 over 10 years ago +2
    Congrats on the move! Looks like you got yourself a nice office The frame looks neat. You're now turning on the lights at once it seems, what about turning it on/off over a period of several minutes up…
  • fvan
    fvan over 10 years ago in reply to rhe123 +2
    Thanks Robin. It's not been without hassle, but finally over. Still can't find some of my things though I've figured out the rules with basic timer, hence this first implementation. Doing some more testing…
  • fvan
    fvan over 10 years ago in reply to mcb1 +2
    Electronics and 3D printing will be done in the office, the more messy work with wood, etc ... will be for the shed. Wife will be happy, no more saw dust in the house!
Parents
  • rhe123
    rhe123 over 10 years ago

    Congrats on the move! Looks like you got yourself a nice office image

     

    The frame looks neat. You're now turning on the lights at once it seems, what about turning it on/off over a period of several minutes up to half an hour? Then you can actually simulate the sun coming up.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 10 years ago in reply to rhe123

    Thanks Robin. It's not been without hassle, but finally over. Still can't find some of my things though image

     

    I've figured out the rules with basic timer, hence this first implementation. Doing some more testing, I should be able to find a way to gradually increase the light's brightness without creating 15 different timers ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fvan
    fvan over 10 years ago in reply to rhe123

    Thanks Robin. It's not been without hassle, but finally over. Still can't find some of my things though image

     

    I've figured out the rules with basic timer, hence this first implementation. Doing some more testing, I should be able to find a way to gradually increase the light's brightness without creating 15 different timers ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • rhe123
    rhe123 over 10 years ago in reply to fvan

    Okay! Creating a set of timers using a for-loop shouldn't be a big issue I assume image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 10 years ago in reply to rhe123

    Indeed. An alternative could be to adapt the cron job which currently executes exactly once at 6:45:00 to execute multiple times by adapting the expression for the minutes.

    In that case, every time the rule is executed, the brightness could slightly be incremented, without the need for a bunch of different timers.