Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [Pi IoT] Alarm Clock #11: Clock Display
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
  • Author Author: fvan
  • Date Created: 29 Jul 2016 7:52 PM Date Created
  • Views 1599 views
  • Likes 5 likes
  • Comments 4 comments
  • fvan_piiot
  • i2c
  • piiot
  • feature_tutorial
Related
Recommended

[Pi IoT] Alarm Clock #11: Clock Display

fvan
fvan
29 Jul 2016

  • Enabling I2C
  • Connecting Hardware
    • 3.3V vs 5V ?
  • Python Library
  • 7-Segment Display
  • 8x8 LED Matrix
  • Demo

 

This post will be about the display of the actual alarm clock. It will consist of two components, visualising different information.

 

image

 

Enabling I2C

 

Both components, a 4 digit 7-segment display and a 8x8 LED matrix, make use of an I2C backpack to facilitate wiring and control.

 

To enable I2C on the Raspberry Pi, launch the "raspi-config" tool from the command line. Select the advanced options and go to the I2C menu. When asked, enable I2C. Reboot the Pi for changes to take effect.

 

imageimage

 

Install the "i2c-tools" package if not already done so, as it will help verify all is as expected:

 

pi@piiot1:~ $ sudo apt-get install i2c-tools
Reading package lists... Done
Building dependency tree
Reading state information... Done
Suggested packages:
  libi2c-dev python-smbus
The following NEW packages will be installed:
  i2c-tools
0 upgraded, 1 newly installed, 0 to remove and 0 not upgraded.
Need to get 51.3 kB of archives.
After this operation, 227 kB of additional disk space will be used.
Get:1 http://archive.raspberrypi.org/debian/ jessie/main i2c-tools armhf 3.1.1+svn-2 [51.3 kB]
Fetched 51.3 kB in 0s (65.1 kB/s)
Selecting previously unselected package i2c-tools.
(Reading database ... 123842 files and directories currently installed.)
Preparing to unpack .../i2c-tools_3.1.1+svn-2_armhf.deb ...
Unpacking i2c-tools (3.1.1+svn-2) ...
Processing triggers for man-db (2.7.0.2-5) ...
Setting up i2c-tools (3.1.1+svn-2) ...
/run/udev or .udevdb or .udev presence implies active udev.  Aborting MAKEDEV invocation.

 

You should now be able to detect I2C devices:

 

pi@piiot1:~ $ sudo i2cdetect -y 1
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:          -- -- -- -- -- -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: 70 71 -- -- -- -- -- --

 

In my case, both displays have been detected. The first one at address 0x70, the second one at 0x71.

Initially, both displays have address 0x70. It is however possible to short some pads at the back using solder, changing the address to a different value:

 

image

 

Let's take a look at how I connected them to the Pi

 

Connecting Hardware

 

3.3V vs 5V ?

 

The safest option is to connect everything using 3.3V, as the Pi's logic level is 3.3V and using 5V may damage the Pi. The connections would then look like this:

imageimage

 

 

Because the displays I used are supposed to be "super bright", powering them using 5V instead of 3.3V would result in the best brightness output. I was however worried as the Pi's I/O uses 3.3V levels. But would powering the displays using 5V damage my Pi's I2C pins?

 

Doing some research, I found an old discussion from fustini asking the same thing: Is level shifting really needed for I2C?  Ultimately, I verified the voltage on the I2C pins using a scope, and it seems it is safe (in this particular case) to power the displays using 5V instead of 3.3V and not damage my Pi's I2C pins image

 

image

 

 

Python Library

 

Adafruit has published a Python library to control most of their LED I2C "backpacks". Like the rest of their software, it can be found on GitHub: https://github.com/adafruit/Adafruit_Python_LED_Backpack

 

Installing the library is straightforward but requires some dependencies to be installed first:

 

pi@piiot1:~ $ sudo apt-get install build-essential python-dev
Reading package lists... Done
Building dependency tree
Reading state information... Done
build-essential is already the newest version.
The following extra packages will be installed:
  libpython-dev libpython2.7-dev python2.7-dev
The following NEW packages will be installed:
  libpython-dev libpython2.7-dev python-dev python2.7-dev
0 upgraded, 4 newly installed, 0 to remove and 0 not upgraded.
Need to get 18.2 MB of archives.

 

pi@piiot1:~ $ sudo apt-get install python-smbus python-imaging
Reading package lists... Done
Building dependency tree
Reading state information... Done
The following NEW packages will be installed:
  python-imaging python-smbus
0 upgraded, 2 newly installed, 0 to remove and 0 not upgraded.
Need to get 19.3 kB of archives.

 

Once the dependencies are installed, the actual library can be downloaded using the "git clone" command:

 

pi@piiot1:~ $ git clone https://github.com/adafruit/Adafruit_Python_LED_Backpack
Cloning into 'Adafruit_Python_LED_Backpack'...
remote: Counting objects: 167, done.
remote: Total 167 (delta 0), reused 0 (delta 0), pack-reused 167
Receiving objects: 100% (167/167), 43.64 KiB | 0 bytes/s, done.
Resolving deltas: 100% (110/110), done.
Checking connectivity... done.

 

Finally, after downloading the library, it ca be installed on the Pi:

 

pi@piiot1:~ $ cd Adafruit_Python_LED_Backpack/
pi@piiot1:~/Adafruit_Python_LED_Backpack $ sudo python setup.py install

 

Library installation: image

 

7-Segment Display

 

This will be used to display the most basic information an alarm clock should display: the time.

 

I wrote a small Python script taking the time, parsing the hours and minutes and concatenating them in a single value. That value is then sent to the display to be visualised. For the colon, it is simply alternated every 500ms image

 

The small script is defined below:

 

#!/usr/bin/env python

import time
from datetime import datetime
from Adafruit_LED_Backpack import SevenSegment

display = SevenSegment.SevenSegment(address=0x70, busnum=1)

colon = False

display.begin()

while True:
  now = datetime.now()

  hours = now.hour
  minutes = now.minute
  seconds = now.second

  string = str(hours) + str(minutes).zfill(2)

  colon = not colon

  display.clear()
  display.print_float(float(string), decimal_digits=0, justify_right=True)
  display.set_colon(colon)
  display.write_display()
  time.sleep(0.5)

 

To verify the placement of the colon and the time, I temporarily set the time to Japan and then back to Belgium.

 

pi@piiot1:~ $ sudo cp /usr/share/zoneinfo/Japan /etc/localtime
pi@piiot1:~ $ sudo cp /usr/share/zoneinfo/Europe/Brussels /etc/localtime

 

This is the result:

imageimage

 

Looks like the time is taken care of, on to the next display!

 

8x8 LED Matrix

 

The LED matrix will be used to display additional information in the form of icons.

 

It could display whether or not a connection to the internet is available or display the forecasted weather with simple icons. Below is an example demonstrating the connectivity check.

 

The script pings a given host and displays a cross if not reachable or nothing if reachable.

 

#!/usr/bin/env python

import time
import os
from PIL import Image
from PIL import ImageDraw
from Adafruit_LED_Backpack import Matrix8x8

display = Matrix8x8.Matrix8x8(address=0x71, busnum=1)

display.begin()

image = Image.new('1', (8, 8))
draw = ImageDraw.Draw(image)

draw.rectangle((0,0,7,7), outline=255, fill=0)
draw.line((1,1,6,6), fill=255)
draw.line((1,6,6,1), fill=255)

while True:
  host = "192.168.0.228"
  response = os.system("ping -W 1 -c 1 " + host)

  if response == 0:
    display.clear()
  else:
    display.set_image(image)

  display.write_display()
  time.sleep(0.1)

 

Check the video below to see both displays in action image

 

Demo

 

Here's a short video clip demonstrating the clock and the connectivity check. It's checking connectivity to the Pi behind it, that is being rebooted.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 


image

 


Navigate to the next or previous post using the arrows.

image
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 10 years ago +1
    power the displays using 5V instead of 3.3V and not damage my Pi's I2C pins I had the same issue with a wireless receiver using the 3v3 RFM69 devices and an I2C LCD display. Luckily the I2C is pulled up…
Parents
  • balearicdynamics
    balearicdynamics over 10 years ago

    Great post. It includes a good quick-start guide to manage I2C.

     

    Thank you!

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 10 years ago

    Great post. It includes a good quick-start guide to manage I2C.

     

    Thank you!

     

    Enrico