• Products and Partners
    Products and Partners
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
Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [Pi IoT] Alarm Clock #14: Front Panel
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
  • Author Author: fvan
  • Date Created: 8 Aug 2016 8:15 PM Date Created
  • Views 4040 views
  • Likes 5 likes
  • Comments 21 comments
  • fvan_piiot
  • piiot
  • cnc
Related
Recommended

[Pi IoT] Alarm Clock #14: Front Panel

fvan
fvan
8 Aug 2016

  • CNC
  • Gallery

 

Found some time this weekend to start the actual build of the alarm clock. I started with the front panel and thought I'd collect some feedback on the progress so far. So be sure to let me know what you think in the comments!

 

CNC

 

To make the necessary cutouts for the clock display and button, I'm using my ShapeOko2 Desktop CNC machine. It uses a Dremel to mill and is controlled via an Arduino UNO with gShield used to control the stepper motors of the CNC.

On the software side I'm using Easel, Inventables' web-based all-in-one software application for CNC milling. It combines the CAD software to create the design, the CAM software to set the tool paths, and additional software to send the resulting G-Code to the Arduino.

 

imageimage

 

Since it was my first time milling a solid board like this one, I used conservative milling speeds and depths, to avoid breaking anything or having the stepping motors skip steps.

 

The settings used were:

  • feed rate: 750mm / min
  • plunge rate: 500mm / min
  • pass depth: 1.0mm

 

This means that in the horizontal plane (X & Y), the mill moves at 750mm / minute, in the vertical plane, 500mm / minute (Z). Every layer is milled 1mm deep, so for a board like this one which is 18mm thick, 18 passes are required.

 

The entire process took about 1h30min. Apart from the occasional vacuuming of the wood dust, not interference was required image

 

Finally, if you have an Inventables account, you can access my file using the following link, allowing you to copy and modify my design to your needs: Easel - PiIoT Alarm Clock - Front

 

Gallery

 

Here's a gallery of different steps in the milling and fitting process. I've added descriptions to every picture image

 

{gallery} CNC

image

Solid Board: The starting piece, a solid board from the hardware store.

image

Passes: Unlike a 3D printer adding layers of material, the mill removes it, layer by layer.

image

Order: It is important to define the shapes to be milled in the correct order. The outside perimeter is done last to avoid the piece coming loose before milling other shapes.

image

Tabs: The piece remains attached to the board with easy to cut "tabs".

image

Sanding: With minimal sanding, the piece is cleaned up and ready for fitting.

image

Fitting: Fitting a push button, and attaching it with a nut. Enough space was foreseen for easy access.

image

Acrylic: A small acrylic plat is fitted, acting as a diffuser for the clock's display.

image

Display: The plate and display are held into place using a few drops of hot glue.

image

Result: The result from the front. What do you think?

 

With the front finished, I can now proceed with the rest of the enclosure. image

 


image

 


Navigate to the next or previous post using the arrows.

image
  • Sign in to reply

Top Comments

  • element14Dave
    element14Dave over 10 years ago +3
    I'm not sure whether or not to be more impressed with the build, or the fvan branded mouse pad. Ok, I'm more impressed with the build
  • fvan
    fvan over 10 years ago in reply to mcb1 +2
    I have purchased an actual router (DeWalt D26204K), but have to make the brackets to be able to mount it on the frame. Should be plenty powerful to try things like aluminium in the future
  • fvan
    fvan over 10 years ago +2
    Finished the next piece, a side piece, holding a speaker!
Parents
  • mcb1
    mcb1 over 10 years ago

    Looks very professional.

    I hadn't looked for I2C 7 segment displays before ... I guess I'll be doing some more internet buying ...

     

     

    Out of interest how long did the routing out process take.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 10 years ago in reply to mcb1

    The routing process took about 1h30min. I used conservative speeds, as it was the first time cutting this type of board with the CNC. I've added more info on the actual speeds and settings in the blog image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to fvan

    The routing process took about 1h30min

    That's not bad since it was a Dremel and the side loading would be high.

     

    I did note that you went across two different sections and the density would be different, so conservative is probably the best idea.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 10 years ago in reply to mcb1

    I have purchased an actual router (DeWalt D26204K), but have to make the brackets to be able to mount it on the frame. Should be plenty powerful to try things like aluminium in the future image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to fvan

    Hello Frederick,

     

    what is the price you paid for this tool ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 10 years ago in reply to balearicdynamics

    The ShapeOko 2 or the DeWalt router?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to fvan

    would something like this do, I designed for the Bosch but the only change would be the diameter of the router hole, I think I designed in Autocad123D or DesignSpark Mechanical, either way I can provide the file (I Think). All the holes are based on 20mm pitch to suite the extrusions

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to fvan

    would something like this do, I designed for the Bosch but the only change would be the diameter of the router hole, I think I designed in Autocad123D or DesignSpark Mechanical, either way I can provide the file (I Think). All the holes are based on 20mm pitch to suite the extrusions

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fvan
    fvan over 10 years ago in reply to Robert Peter Oakes

    Certainly looks similar. Would love the file if you don't mind sharing it image Thanks Peter!

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to Robert Peter Oakes

    That looks like a serious routing table ...

    It's the sort of one I need so I can go big or go home ...