PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Adapting Art to Viewers:  More on Cabinet Design, Blog #6
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
  • Author Author: fmilburn
  • Date Created: 9 Apr 2019 8:29 PM Date Created
  • Views 1859 views
  • Likes 9 likes
  • Comments 4 comments
  • picasso
  • picasso design challenge
  • raspberry pi 3 b+
  • image recognition
  • raspberry pi camera v2
  • ai
  • art
  • pi face
Related
Recommended

PiCasso Adapting Art to Viewers:  More on Cabinet Design, Blog #6

fmilburn
fmilburn
9 Apr 2019

Art is often made to appeal to a specific set of viewers.  This is the 6th blog in a series exploring the idea of using AI to recognize a viewer and adapt art to their age or interest.  The intent is to encourage early art appreciation while being attractive to all household members.

image

The project was a mess of wires and breadboards so more work was done on enclosures and mounts this week.

 

The 3D Printer has been Busy

 

The cutout on the face was a bit ragged so a bezel was made to enclose the monitor opening.

image

To hold the camera in place a bezel was fabricated for it also.  The camera is mounted with two locating pins and two screws.  The back and front is shown in the following photo.

image

A Raspberry Pi mounting plate was made that attaches to the back of the monitor.

image

For now, some things are still held in place with mounting putty as I am still thinking about the best placement and aesthetics before gluing and screwing into place.  This shot shows the second Raspberry Pi mounted and the camera in place from the back.

image

 

I thought there would be plenty of room but of course now things are getting tight and the ribbon cable for the camera is a bit short.  Little fingers are bound to pry at the wires and things and the back enclosure does not quite cover things up.

image

A call needs to be made though for when enough is enough for the first iteration though as the software needs attention as well.  The tradeoff will be between a fully functional prototype and refined physical design.  Since this is an art project, here is the beauty shot.

image

 

Upcoming Work

 

  • Take the training photos and perform image recognition training
  • Write Python script to drive the monitor and control the art output
  • Develop and obtain additional art.

 

Other Posts in this Series

PiCasso Adapting Art to Viewers: Introduction  Blog #1

PiCasso Adapting Art to Viewers: OpenCV Face Detection, Blog #2

PiCasso Adapting Art to Viewers: Cabinet Design, Blog #3

PiCasso Adapting Art to Viewers: Pi talks to Pi, Blog #4

PiCasso Adapting Art to Viewers: Grandpa Shark, Blog #5

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 7 years ago +5
    Very well done build. I love the camera hole with stylish decoration. All is harmonized and connects well. Enrico
  • genebren
    genebren over 7 years ago +4
    Frank, Nice work on your cabinet design. I really like the camera bezel! Keep up the good work! Gene
  • dubbie
    dubbie over 7 years ago +4
    Frank, A lovely beauty shot. Dubbie
Parents
  • balearicdynamics
    balearicdynamics over 7 years ago

    Very well done build. I love the camera hole with stylish decoration. All is harmonized and connects well.

     

    Enrico

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago

    Very well done build. I love the camera hole with stylish decoration. All is harmonized and connects well.

     

    Enrico

    • Cancel
    • Vote Up +5 Vote Down