PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Design Challenge - POV Globe Blog 6
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
  • Author Author: dwinhold
  • Date Created: 21 Apr 2019 11:32 PM Date Created
  • Views 807 views
  • Likes 8 likes
  • Comments 5 comments
  • picasso
  • pov globe
  • picasso design challenge
  • dwinhold
Related
Recommended

PiCasso Design Challenge - POV Globe Blog 6

dwinhold
dwinhold
21 Apr 2019

This update is the wiring of the power to the globe. The below photos and explanations of each, describe exactly what I did. I also include a video at the end.

 

First photo is of the Positive wires that power the Raspberry Pi and the LED's:

 

image

 

Next is the Negative out:

 

image

 

Next photo is of the underside at the bearings. The spindle is hand made of wood on a wood lathe. I drilled a hole down the middle for the wire to travel:

 

image

 

The last is a video of the power connected turning on LED's:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Hope you enjoyed this update. As always, any questions, comments or ideas you have, please leave a message below!!

 

Dale Winhold

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 7 years ago +4
    Good update, Dale. I have a couple of points to have some clarification on your last progress, something that IMHO may risk to introduce some weakness to the rotation. As you should reach a considerable…
  • dwinhold
    dwinhold over 7 years ago in reply to balearicdynamics +4
    Hi Enrico I like the idea of a soldered board instead, I will definately be changing that out. As for the belt, I already have the type you are mentioning. Since I have to change out the motor I will be…
  • 14rhb
    14rhb over 7 years ago +3
    Hi Dale, a great update, thank you. I like your drive setup and belt (which looks like a piece of cord). I hope all goes well and looking forward to reading about your progress. Rod
Parents
  • balearicdynamics
    balearicdynamics over 7 years ago

    Good update, Dale.

     

    I have a couple of points to have some clarification on your last progress, something that IMHO may risk to introduce some weakness to the rotation. As you should reach a considerable RPM and the globe is not small, why you don't use direct wiring and a breadboard PCB (soldered, I mean) instead of the plastic one? Also if it is relatively lightweight, as the rotation speed increase as much its mass influences a possible vibration or worst. With a soldered small PCB you can keep it perfectly aligned to the rotation axis eliminating this risk.

     

    The second is respect to the traction method. The new motor you used seems robust and reliable for the scope. As you already have trapezoidal pulleys, why don't use a trapezoidal belt instead of those I see? I mean those belts used for the car motors. You can find for cheap almost everywhere as spare parts of every diameter.

     

    Enrico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dwinhold
    dwinhold over 7 years ago in reply to balearicdynamics

    Hi Enrico

     

    I like the idea of a soldered board instead, I will definately be changing that out. As for the belt, I already have the type you are mentioning. Since I have to change out the motor I will be changing the belt as well.

     

    Thank you for the ideas

     

    Dale

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dwinhold
    dwinhold over 7 years ago in reply to balearicdynamics

    Hi Enrico

     

    I like the idea of a soldered board instead, I will definately be changing that out. As for the belt, I already have the type you are mentioning. Since I have to change out the motor I will be changing the belt as well.

     

    Thank you for the ideas

     

    Dale

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • kiri-ll
    kiri-ll over 7 years ago in reply to dwinhold

    An I like the "belt" which you use have right now image It brings an additional artistic feeling to the project!

    • Cancel
    • Vote Up +3 Vote Down