PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog When is a project finished?
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
  • Author Author: therepairatrooper
  • Date Created: 8 Jul 2019 6:06 AM Date Created
  • Views 3577 views
  • Likes 9 likes
  • Comments 12 comments
Related
Recommended

When is a project finished?

therepairatrooper
therepairatrooper
8 Jul 2019

I am asking myself this question because at this point, I have a working prototype but in that process I have also come to some conclusions.

 

In terms of finished, I have completed the window frame, connected my security camera and demonstrated the project working. Based on the conclusions below, this particular project is completed but opens doors for a more advanced project.

 

In reaching this end point, the following conclusions have become apparent:

 

1. That in order to appear natural, a much higher resolution source is required, which would also require a 4K monitor and a PI able to drive it.

2. A 32" TV is too small to be a convincing window, unless it was in perhaps a small prison cell

3. This concept has merit beyond creating a fake window. Windows with embedded lcd films in them could be used to provide someone on the 24th floor of a tower with a view of a park, rather than another building.

  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +8
    4 thresholds = done : nothing significant left to learn potential satisfaction from further progress is insignificant the result of progress has no use nobody else is interested 4 thresholds = pause :…
  • dubbie
    dubbie over 7 years ago +7
    When is a project finished? A very philosophical question. It's a bit like asking 'How long is a piece of string?' Of all the projects I have been involved with I do not think any of them could be classed…
  • Jan Cumps
    Jan Cumps over 7 years ago +7
    (not talking for my professional life. Paycheck blurs the border): my projects are finished; When I can't be bothered searching for them when I have an improvement idea. When I don't come up with improvements…
Parents
  • dougw
    dougw over 7 years ago

    4 thresholds = done :

    • nothing significant left to learn
    • potential satisfaction from further progress is insignificant
    • the result of progress has no use
    • nobody else is interested

     

    4 thresholds = pause :

    • cost of progress is higher than can be justified or higher than other desirable projects
    • too busy with other higher value projects
    • it interferes with my team sports schedule
    • "somebody" needs me for something else

     

    8 thresholds = keep going :

    • it is fun
    • it is interesting
    • it is educational
    • it is useful
    • it creates respect
    • it is a commitment
    • "somebody" would be pleased
    • bull-headed stubbornness
    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to dougw

    dougw  wrote:

     

    4 thresholds = done :

    ...

    • nobody else is interested

     

    In that case I should throw away my Hercules microcontrollers and stop blogging about functional safety designs.

    Only one person is interested and we talk over Google Hangouts anyways ...

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 7 years ago in reply to Jan Cumps

    For me all 4 done thresholds need to be satisfied before I totally pack it in.

    Any of the 4 pause thresholds could cause a pause.

    Any of the 8 go thresholds could cause a go.

     

    Jan Cumps Your projects are all superb references and a great addition to element14 content. I usually glance through them with various levels of diligence depending on the subject matter, and I try to make a mental note to dig into them in more detail when I have a similar application. It is invaluable that the extra detail is there when you need it.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 7 years ago in reply to dougw

    I second that Doug.  Also, your thresholds are pretty much the same as mine when I come to think about it.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to Jan Cumps

    For me too, that's not a threshold either, although it's nice to get feedback from time to time of course.

    Some people don't immediately know what is/will be interesting to them or not : )

    I'm on a Linux mailer (a regional one), and I frequently hear from the grapevine "what is this hardware stuff Shabaz is discussing, why is it on this mailer.. I want off this mailer I thought it was a Linux mailer, and this isn't Linux!". Sometimes one has to walk someone down a road to let them see the relevance to computing and Linux (despite it sometimes seeming obvious). And also reminds me that despite the best efforts in the world with title creation and first photo/sentences, it can still switch off a percentage of people who should in theory be part of the target audience : (  (Admittedly I have not tried a title like "Free money and Linux", that might work : )

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 7 years ago in reply to Jan Cumps

    For me too, that's not a threshold either, although it's nice to get feedback from time to time of course.

    Some people don't immediately know what is/will be interesting to them or not : )

    I'm on a Linux mailer (a regional one), and I frequently hear from the grapevine "what is this hardware stuff Shabaz is discussing, why is it on this mailer.. I want off this mailer I thought it was a Linux mailer, and this isn't Linux!". Sometimes one has to walk someone down a road to let them see the relevance to computing and Linux (despite it sometimes seeming obvious). And also reminds me that despite the best efforts in the world with title creation and first photo/sentences, it can still switch off a percentage of people who should in theory be part of the target audience : (  (Admittedly I have not tried a title like "Free money and Linux", that might work : )

    • Cancel
    • Vote Up +5 Vote Down