Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog Smart Range Hood - Any Pi Chefs out there cook their Pi yet? Blog post # 11
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
  • Author Author: aspork42
  • Date Created: 24 Mar 2018 3:19 AM Date Created
  • Views 1163 views
  • Likes 10 likes
  • Comments 5 comments
  • home automation
  • smart range hood
  • pi chef*
  • raspberry pi
Related
Recommended

Smart Range Hood - Any Pi Chefs out there cook their Pi yet? Blog post # 11

aspork42
aspork42
24 Mar 2018

The goal - some improvements over a common range hood.

 

aka Smart Range Hood. See blog post #1 for the complete build process.

 

Cooked Pi anyone?

This will be a quick post of joy, excitement, tragedy, and triumph.

Last night I thought I was ready to install the components into the hood. We only have one week left and I want to get things moving. I finalized most the remaining loose ends and went about the final installation. Once mounted, I plugged in the Pi - and bad things started happening! I hadn’t hooked up any mains voltage yet, but my pcb started to flicker on and off. The LEDs were flashing; the buzzer was going crazy.

I unplugged the Pi Power and started looking around. I checked for sorts between power and ground but didn’t have any. I looked around some more and finally found that the 40-pin header for the screen was plugged in 1 pin over - aaaaaarrrrggggghhhh!!!! How much magic smoke got out???

 

image

 

image

 

An artist’s recreation of the mistake.

 

This happened late at night so I decided to stop and sleep on things. I unplugged everything and went to bed.

 

Since there is only a week left to finish, I broke down on Friday and took a half day from work. I came home and started diagnosing the issues. I didn’t know how much damage there was. If I was to need any new components, I had to get them on order very quickly. I am actually traveling for work next week so won’t really be able to work on the project after Tuesday; so any delays or setbacks would be very bad...

 

The first thing I found was that after seating the header properly, the Pi came alive; but only partially worked. The screen was backlit but there was no image. I had temperature data from the DHT but no analog sensor data. The DHT is hooked right to a GPIO but the analog sensor is on the I2C bus. I tried scanning the bus for devices over SSH but got an error instead of a list of devices. See the video below for an example.

 

Since none of the devices showed, I figured that the Pi itself was cooked and perhaps the I2C pins were ruined on the Broadcom CPU. I pulled the SD card and put it in another Pi. I used a spare blank circuit board to test with. I still got errors trying to scan for devices; with zero and with one I2C devices installed. I switched the screen output over to HDMI and started looking around. I hooked up the scope and found that there was no Data or Clock signals present when I tried scanning; which should not be the case. And this was tested with nothing plugged in; just the pcb with no devices attached.

 

I finally found that in the Config menu, I2C and SPI were somehow disabled... strange - they worked 10 minutes before I had the problem. I re-enabled them and could see the devices properly again. I switched back over to the original Pi and the full PCB. The Pi was still alive!

 

The screen was the only casualty. I found that the buttons still work, and I still get a touchscreen interrupt when you tap it, but no video.

I ordered a new screen and will have it next week... could have been a lot worse!

 

Here is a video of the debug process.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

And here is a video of the installed Smarts!!!

(new screen to come)

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Yahoo!

So with that, I think I have a complete project! Still some minor loose ends to tie up, but I have done what I set out to do. I wil have a better summary in another blog post to talk about all the individual items.

 

Oh - one more breakdown- my 3D printed had the new improved cover for the air baffle printing; but the part warped off the bed and broke my Z-Probe mount image so that is down until I can fix it... but I think I am mostly done with it image

 

image

  • Sign in to reply

Top Comments

  • ogorman.amela
    ogorman.amela over 8 years ago +2
    Oh no!!! I am happy to report that the range hood still works -- turns on automatically when the burners are on and it detects heat (or something like that). Pretty swanky... =) Is it done yet?
  • DAB
    DAB over 8 years ago +1
    Now you know why most professional systems use keyed connectors. I to have plugged the flat ribbon cable connectors in wrong, so you are not alone in that respect. With the RPi, you have mostly low voltage…
  • genebren
    genebren over 8 years ago +1
    Excellent update and congratulations on so much of the project working. I have also suffered through the misaligned header/connectors before. Fortunately for you the damage was limited and you could check…
Parents
  • three-phase
    three-phase over 8 years ago

    Well done for overcoming the problems encountered. Hopefully smooth silting from here onwards.

     

    Kind regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 8 years ago

    Well done for overcoming the problems encountered. Hopefully smooth silting from here onwards.

     

    Kind regards