Experimenting with Polymer Capacitors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Polymer Capacitors
  • More
  • Cancel
Experimenting with Polymer Capacitors
Blog Results and conclusion
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: neuromodulator
  • Date Created: 19 Jun 2019 10:08 PM Date Created
  • Views 2947 views
  • Likes 6 likes
  • Comments 7 comments
Related
Recommended

Results and conclusion

neuromodulator
neuromodulator
19 Jun 2019

Results: Capacitance temperature dependence

 

The first thing that I wanted to test was how the temperature affects the capacitance of the different capacitors. I performed a temperature sweep from ambient temperature to ~80 °C, and then back to ambient temperature.

imageimageimage

 

It can be seen that the temperature curve looks like a stairway at higher temperatures, this was caused by the lack of precision of the MyDAQ ohmmeter. The temperature curve was not identical in all 3 measurements either (as it was controlled  manually), this could be fixed through concurrent measurement of capacitances through multiple channels or through a better timing and control of initial liquid temperature, volume of liquid, etc. I found that the aluminium polymer capacitor does not appear to respond linearly to the temperature, in opposition to the tantalum polymer and hybrid polymer capacitors. This observation are more evident when looking at the temperature/capacitance plots.

imageimageimage

 

Besides the lack of linearity, the aluminium capacitance/temperature plot also shows another interesting feature, the capacitance stays higher for the same temperature when the temperature is dropping than when it is rising, more experiments need to be done to better understand the behavior of the aluminium measured capacitance. In order to compare the capacitance variation of capacitors I normalized the capacitances so that at ambient temperature (25 ºC) the capacitances are 1:

image

The hybrid polymer capacitor showed the lowest slope (in the tested temperature range), or said differently temperature affected its capacitance less than the capacitance of the other capacitors. The polymer aluminum capacitor appears show lower capacitance variation than the polymer tantalum capacitor on a defined temperature range, but more tests need to be done to really confirm this.


Results: Leakage current


To measure the leakage current of the capacitors I first kept the capacitors for >1 h at 5 V in order to minimize the current flow due to dielectric absorption, then I measured the current at the same voltage (5 V) with the DMM while sweeping the temperature.

 

imageimageimage

 

All capacitors showed completely different magnitudes of current leakage, and appeared to reach the maximum leakage current before the maximum temperature, an effect that is especially noticeable in the polymer aluminium capacitor. The reason this occurs may be related to the lower dT/dt before reaching maximum temperature, but more tests would have to be done to confirm this. While the polymer tantalum capacitor appeared to display very little stochasticity, the polymer aluminium and hybrid polymer capacitors displayed higher stochasticity during the leakage current drop and rise respectively. All capacitors displayed a lower leakage current when cooling than when heating (at the same reference temperature), this can be better appreciated in the leakage current/temperature plots.

imageimageimage

Even though the polymer aluminium "triangular" pattern appears very different to the patterns of the other capacitors, this could be the result of differences in the temperature curves, and not a property inherent to the capacitor. Again, a more consistent generation of the temperature curve, or the use of a multichannel system could help in doing a better comparison between the capacitors. To compare the curves the leakage current was normalized at the initial ambient temperature (25 °C).

image

 

It can be seen that the polymer tantalum leakage current has the highest sensitivity to temperature and increases 20 times, while the other 2 capacitors increase less than 5 times.

 

 

Results: Dielectric absorption

 

Dielectric absorption is an effect caused by the "alignment" and "delignment" of the molecular dipoles of the capacitor dielectric caused by the application of an electric field. If a constant voltage is applied to a capacitor, molecular dipoles will slowly orient themselves to the electric field, and this of course requires electrical charges. When the capacitor is discharged the opposite happens, charges are given back. If a capacitor is charged and then short-circuited momentarily, voltage will build up across the terminals.

 

To observe the effect I kept capacitors at 5V for >1 h and then I began recording their voltage with the DMM set at 10 GigaOhm input impedance and briefly (~0.5 s) manually shorted the capacitor terminals.

image

As the shorting was done manually, its not possible to draw any conclusion on which capacitor gets more voltage back as minor differences in the time the capacitor stays shorted have a great impact in how much of the original voltage gets back. Still its possible to observe that they build up their voltage at different speeds, with the tantalum appearing to show the fastest dynamic. One way this test could be improved is by using an MCU and a transistor to precisely time the capacitor terminal shorting period.

 

 

Conclusions

 

As much as I would have liked to test all the 17 capacitors, that would have been too time consuming with a single channel system. For that reason, I explored 3 type of capacitors with similar values, but of course not identical, making the comparison not very fair. As I was not sure what results I would get out of the experiments or even if the experiments would work, the experiments were a bit crude and meant to be more of an exploration than a rigorous characterization. These results could be seen as the first iteration of a more rigorous capacitor characterization, follow-up iterations would have to use more precise timing to improve repeatability of the experiments, be repeated multiple times to reduce noise and measure stochasticity and improve temperature measurement.

 

Maybe more important than trying to draw any definitive conclusion on the polymer capacitors, what I showed in this design challenge is one way to perform the experiments to characterize capacitors and how much instrumental precision is required to do so. The Atlas ESR meter for instance was not capable of detecting variations of the ESR caused by temperature variation (any eventual variation was below the precision of the instrument). Hopefully these experiments were interesting to anyone thinking about characterizing capacitors or just interested in the parameters that I measured.

 

Finally, I would like to thank E14 for allowing me to participate in this design challenge as I really had a lot of fun participating!

  • Sign in to reply

Top Comments

  • aspork42
    aspork42 over 7 years ago +6
    Nice job on the tests! You got some real world data here to consider. Yeah - these tests can be challenging to set up accurately when doing semi-manual data collection. You could have considered using…
  • michaelkellett
    michaelkellett over 7 years ago +4
    Nice report and a lot of work. Can you post any pictures, and explain how you controlled and measured temperature (I'm looking for a reason for the leakage leading the temperature.) !!! Just seen your…
  • three-phase
    three-phase over 7 years ago +4
    Interesting set of results to your experiments. I have been wondering why the Polymer capacitors appear to be running warmer than electrolytic in my amplifier circuit. I think some more experimentation…
Parents
  • shabaz
    shabaz over 7 years ago

    Very interesting results!

    I wonder if some of the short-term fluctuation (not the overall trend) in the hybrid capacitor leakage current measurement is due to electrolyte moving inside (no idea, just a guess!).

    image

    It's great to see that these types of measurements, and greater scrutiny and understanding of components, are achievable nowadays with modern not crazily-expensive equipment!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 7 years ago

    Very interesting results!

    I wonder if some of the short-term fluctuation (not the overall trend) in the hybrid capacitor leakage current measurement is due to electrolyte moving inside (no idea, just a guess!).

    image

    It's great to see that these types of measurements, and greater scrutiny and understanding of components, are achievable nowadays with modern not crazily-expensive equipment!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • neuromodulator
    neuromodulator over 7 years ago in reply to shabaz

    Those fluctuations are pretty odd I agree, and I was not able to find any info on the net nor a similar plot. Oddly enough those fluctuations appear to occur when the aluminum cools and don't appear to occur on the tantalum at all. I'm also wondering if its stochastic or deterministic, I suspect its the former but the experiment would have to be repeated as identical as possible to see if the fluctuations repeat themselves or not.