Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog QuadCOP - More construction Pictures
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: screamingtiger
  • Date Created: 25 Aug 2015 4:27 AM Date Created
  • Views 3138 views
  • Likes 3 likes
  • Comments 25 comments
  • quadcop_project
  • design_challenge
  • rasberry_pi
  • sci_fi_your_pi
  • quadcopter
Related
Recommended

QuadCOP - More construction Pictures

screamingtiger
screamingtiger
25 Aug 2015

Previous Posts Here:

http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/authors/screamingtiger?ICID=DCH-SciFiPi-challengers

 

I have mounted the camera in the head, and have the head moving!  I don't have the servo secure yet so that is why it is wobbly.  I posted a vid below on a preview of how it works.  I just controlled it with my radio but in flight the Raspberry Pi (RPFS) will use it to "Scan" around.

 

Cut a hole for they eye

 

image

 

Pi camera mounted with hot glue

image

 

lens pokes through

image

 

Servo, needs hard wood mounts, just held on with glue for now.

 

image

 

A preview.  Note the plastic eye cover, made from a Christmas Ornament.

image

Watch the Vid of the head.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • screamingtiger
    screamingtiger over 11 years ago in reply to DAB +2
    For my purpose, I wanted 360 degree rotation but I would need another Magnometer but I only have 1 that works on hand. My original specs say the quad will do a 360 degree sensor sweep, I changed that to…
  • jw0752
    jw0752 over 11 years ago +1
    The way he turns his head back and forth reminds me of how I would feel if you were attaching me to a quadcopter. Very nice pictures. Was the pretty lady your very very understanding and supportive wife…
  • balearicdynamics
    balearicdynamics over 11 years ago +1
    Very nice !!! It's almost finished Enrico
Parents
  • DAB
    DAB over 11 years ago

    Good post.

     

    It reminded me of the time I drove a helicopter FLIR camera based upon its flight vectors.

    I used five degree steps to keep the movement smooth and then one degree steps once I had the FLIR looking down the flight vector.

     

    Those were good days, especially during flight test with the UH53.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to DAB

    For my purpose, I wanted 360 degree rotation but I would need another Magnometer but I only have 1 that works on hand.  My original specs say the quad will do a 360 degree sensor sweep, I changed that to be a 180 degree. The quad wont rotate, just the head.  The head will only moved when stopped but I may add some "bling" movements so it looks around while moving to the next waypoint and while being flown manually.

     

     

    the head will have a sonic sonsor and motion detector on it as well.

     

    Basically the same algorithm I used on my B-25 bomber turret but for that I used Arduino, but the ChipKit can handle it!  It will have a smooth motion with variable speeds.  I am considering putting my Luxeon LED setup on it too so it acts like a search light.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to mcb1

    The promised GPS vertical accuracy is supposedly quite poor however most devices that claim reasonable accuracy on their "z" axis  actually combine the barometric sensor data to give a more accurate final "GPS" value .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to Problemchild

    As a matter of fact, I have serious suspects about the reliability of the GPS vertical accuracy and the best solution maybe an altimetric sensor. The problem of the height stabilisation was one of the bigger issues in all the generations of the AR-Drone devices as I have explained in a post above.

     

    Some other high profile (and very high price) drones, including the DJI Phantom if I am not wrong, consider also the parameters returned by a very reactive accelerometers that is used to compensate the z-axis offset of a given altitude based on the small movements detected and their relative speed.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to balearicdynamics

    Yeah the inputs from all the sensors are used to compensate for the GPS inaccuracy. Also they have an elaborate calibration procedure for those sensors at the beginning of the flight . finally of course  the craft doesn't need to to really know where it is in absolute terms but relative to the start so if it's wrong it doesn't matter as long as it's consistently wrong in it's measurements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to Problemchild

    What I have experienced until now with drones, is that the aspect that seems more complex, to make them flying, as a matter it is the less problematic and simple. True it is easier than making fly a traditional aero model. Then when the aero model flies 95% of the effort is done while when a drone flies (almost any thing included a rick can fly as drones) it is only done 10%-20% of the job.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to balearicdynamics

    Well since I have a bit more time before I fly I may give the xtrinsic board one more shot.  I was playing with the pressure sensor.  Had a hard time not getting it to lock up, but I was using the code they provide in Python.

     

    I agree GPS is not going to be perfect but its what I got.  The sonic sensors will keep it from hitting the ground.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • screamingtiger
    screamingtiger over 11 years ago in reply to balearicdynamics

    Well since I have a bit more time before I fly I may give the xtrinsic board one more shot.  I was playing with the pressure sensor.  Had a hard time not getting it to lock up, but I was using the code they provide in Python.

     

    I agree GPS is not going to be perfect but its what I got.  The sonic sensors will keep it from hitting the ground.