Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog QuadCOP - More construction Pictures
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: screamingtiger
  • Date Created: 25 Aug 2015 4:27 AM Date Created
  • Views 3149 views
  • Likes 3 likes
  • Comments 25 comments
  • quadcop_project
  • design_challenge
  • rasberry_pi
  • sci_fi_your_pi
  • quadcopter
Related
Recommended

QuadCOP - More construction Pictures

screamingtiger
screamingtiger
25 Aug 2015

Previous Posts Here:

http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/authors/screamingtiger?ICID=DCH-SciFiPi-challengers

 

I have mounted the camera in the head, and have the head moving!  I don't have the servo secure yet so that is why it is wobbly.  I posted a vid below on a preview of how it works.  I just controlled it with my radio but in flight the Raspberry Pi (RPFS) will use it to "Scan" around.

 

Cut a hole for they eye

 

image

 

Pi camera mounted with hot glue

image

 

lens pokes through

image

 

Servo, needs hard wood mounts, just held on with glue for now.

 

image

 

A preview.  Note the plastic eye cover, made from a Christmas Ornament.

image

Watch the Vid of the head.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • screamingtiger
    screamingtiger over 11 years ago in reply to DAB +2
    For my purpose, I wanted 360 degree rotation but I would need another Magnometer but I only have 1 that works on hand. My original specs say the quad will do a 360 degree sensor sweep, I changed that to…
  • jw0752
    jw0752 over 11 years ago +1
    The way he turns his head back and forth reminds me of how I would feel if you were attaching me to a quadcopter. Very nice pictures. Was the pretty lady your very very understanding and supportive wife…
  • balearicdynamics
    balearicdynamics over 11 years ago +1
    Very nice !!! It's almost finished Enrico
Parents
  • DAB
    DAB over 11 years ago

    Good post.

     

    It reminded me of the time I drove a helicopter FLIR camera based upon its flight vectors.

    I used five degree steps to keep the movement smooth and then one degree steps once I had the FLIR looking down the flight vector.

     

    Those were good days, especially during flight test with the UH53.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to DAB

    For my purpose, I wanted 360 degree rotation but I would need another Magnometer but I only have 1 that works on hand.  My original specs say the quad will do a 360 degree sensor sweep, I changed that to be a 180 degree. The quad wont rotate, just the head.  The head will only moved when stopped but I may add some "bling" movements so it looks around while moving to the next waypoint and while being flown manually.

     

     

    the head will have a sonic sonsor and motion detector on it as well.

     

    Basically the same algorithm I used on my B-25 bomber turret but for that I used Arduino, but the ChipKit can handle it!  It will have a smooth motion with variable speeds.  I am considering putting my Luxeon LED setup on it too so it acts like a search light.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to screamingtiger

    Great video Joey,

     

    it perfectly gives the idea of what will be the result of the quadcopter !

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to screamingtiger

    Hi Joey

    How are you going to implement the motion detector? I would be useful for my project as well.. My idea was to use OpenCV, but may be you have an approach that requires less computing power

     

    Regards

    Ambrogio

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to amgalbu

    For my project I planned on using a PIR sensor.  However I haven't tested it yet and I am not sure it will work since the QuadCop probably will not be able to hold perfectly still.  I think the same issue would happen if I used Open CV.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to screamingtiger

    Joey, you mean a presence / movement sensor to detect the presence of objects in the path or to manage the drone at the same height while flying?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to screamingtiger

    Joey, you mean a presence / movement sensor to detect the presence of objects in the path or to manage the drone at the same height while flying?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • screamingtiger
    screamingtiger over 11 years ago in reply to balearicdynamics

    I have a PIR for motion detection and a sonic sensor for ground detection.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to screamingtiger

    Joey,

     

    this is fine but I have experienced in past with drones a potential issue - that probably can be solved before with a proper workaround. The sonic sensor detects the height from ground supposing a variable but continuous ground surface. I mean for example the drone while flying at a fixed height of 5 meters from ground while going over a hill.

    The problem unfortunately occur if you try adopting the same method flying the drone on a top terrace at the third floor of a house. As the drone goes outside the terrace, the sonic sensor detect a ground height sort of out-of-scale Depending on the software can try to compensate with not perfectly predictable fly-down or lose the control because the sensor is really in a range of unexpected values or something else. Just a warning to take in account.

     

    Hope this can be useful. Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to balearicdynamics

    For altitude, I will be using the GPS readings.  This is to keep me 10 foot or so up in the air.  The ground sonic sensor is for landing or obstacle avoidance.  Its really on good for 2 feet or so.

     

    The assumption is the take off and landing areas are clear.

     

    BTW, if I am over a house there is a serious issue!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to screamingtiger

    For altitude, I will be using the GPS readings

    Are you sure it will be accurate enough ??

     

    Barometric pressure (corrected at takeoff) could be much more accurate, but you do have airflow disturbance that it would need to be protected from.

     

    The sensors sent with the Robot kit are good for distance to 5.5m ( 18 feet).

    http://www.element14.com/community/groups/stemacademy/blog/2015/08/13/virtual-eye-system--post-3--testing-and-calibration

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to mcb1

    I think it will be accurate enough for 10+ feet, but if not then the position itself is not accurate I guess?  I did attempt to use the pressure sensor on the xtrinisic board but no compatible with RPi 2 at this time.  I did get it working but not very reliably.  On the RPI B+ it works great!