Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Sci Fi Your Pi: PiDesk - Guide: Controlling NeoPixels with the Raspberry Pi A+/B+
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 20 May 2015 10:46 AM Date Created
  • Views 3183 views
  • Likes 4 likes
  • Comments 15 comments
  • design_challenge
  • touch_motion_controls
  • touch_motion_control
  • sci_fi_your_pi
Related
Recommended

Sci Fi Your Pi: PiDesk - Guide: Controlling NeoPixels with the Raspberry Pi A+/B+

fvan
fvan
20 May 2015

  • Introduction
  • Software
  • Hardware
  • Demo

 

Introduction

 

Addressable LEDs or NeoPixels are typically used in combination with an Arduino or similar microcontroller, due to the timing critical signal required to control them. An SBC such as the Raspberry Pi is not suited for such realtime GPIO activities, as the Linux operating system runs other tasks in parallel. Or at least that was the case until Jeremy Garff found a way to use the DMA (Direct Memory Access) module to transfer bytes of memory between different parts of the processor, without using the CPU and thus not being interrupted by the Pi's OS.

 

image This procedure works for all Raspberry Pi models except version 2!

 

Software

 

Jeremy Garff has written a library called "rpi_ws281x", which can be found on his GitHub page: https://github.com/jgarff/rpi_ws281x. It makes use of the Pi's BCM2835's PWM module to drive the controllable WS281X LEDs found in NeoPixel strips and rings. The folks at Adafruit have created a Python wrapper for the library along with some Python example scripts, making it look and feel like the Arduino NeoPixels library. So if you're familiar with NeoPixels on the Arduino, you should be up and running with this version in no time.

 

To compile and install the library, follow the steps below.

 

First, install the dependencies required to download and install the library:

sudo apt-get update
sudo apt-get install build-essential python-dev git scons swig

 

Next, download the files and build the library:

git clone https://github.com/jgarff/rpi_ws281x.git
cd rpi_ws281x
scons

 

Finally, install the Python wrapper:

cd python
sudo python setup.py install

 

As you can see, these steps are very straightforward.

 

Hardware

 

Hooking up the NeoPixels to the Raspberry Pi is extremely easy, just make sure the power supply used is properly rated for the number of NeoPixels you intend to use. For testing, I used a 5V/4A power supply to power the Pi and the NeoPixels (12 and 60 LEDs).

 

image

Make sure the ground signals of the NeoPixel strip/ring and the Raspberry Pi are connected. If they are not, the LEDs won't function properly and will light up in unpredictable patterns.

 

Even though the LED strip/ring operates at 5V and the Pi's GPIO at 3.3V, it appears that it is possible to drive the LEDs without having to use logic level conversion.

 

 

Demo

 

I tested two components:

  • an Adafruit NeoPixel ring with 12 LEDs
  • an addressable WS2811 60 LED strip from eBay

 

Both performed as expected using the sample script (strandtest.py), which I edited to configure the correct number of LEDs:

 

# LED strip configuration:
LED_COUNT      = 60      # Number of LED pixels.
LED_PIN        = 18      # GPIO pin connected to the pixels (must support PWM!).
LED_FREQ_HZ    = 800000  # LED signal frequency in hertz (usually 800khz)
LED_DMA        = 5       # DMA channel to use for generating signal (try 5)
LED_BRIGHTNESS = 255     # Set to 0 for darkest and 255 for brightest
LED_INVERT     = False   # True to invert the signal (when using NPN transistor level shift)

 

As you can see, it is also possible to edit other parameters to match the LEDs used, but also parameters such as brightness.

imageimage

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 11 years ago +1
    Great work!
  • DAB
    DAB over 11 years ago +1
    Great blog. You have given me some ideas for a project I have. Thanks DAB
  • fvan
    fvan over 11 years ago in reply to balearicdynamics +1
    Hi Enrico, I believe I bought this one from Pimoroni in the UK: http://shop.pimoroni.com/products/adafruit-neopixel-ring-24-x-rgb-led-w-integrated-drivers You can choose between 24, 16 and 12 LEDs. They…
  • fabiola
    fabiola over 3 years ago

    Hellow! I know your blog post was over 7 years but I have trouble installing 'scons' is there a way you specifically did it? I know you won't remeber so that's fine

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to balearicdynamics

    Dig out the datasheets for WS2812 or just the driver chip WS2811.

    They are a RGB driver that features a 'pass thru' for the data.

     

    Reminds me of some clever strobe based devices years ago that did a similar thing.

    The first one takes the first chunk of data, and passes the rest on, the next takes the first chunk it sees ....etc.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to balearicdynamics

    I finally got my whole kit, all I am missing is the A+ which we wont be getting, but I guess we are supposed to get an Eagle license, I hope they send that out I really need some good software.

     

    I got 4 packages total to get the whole kit. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago in reply to screamingtiger

    Hi Joey,

     

    the strip was bought on eBay a little more than a year ago. Search for WS2811/WS2812 LED strips, you'll find plenty variants with 30, 60 or more LEDs/meter.

     

    I know my setup bypasses the fuses and that's also why I didn't put it like that in the drawing. It's just something I quickly do when I don't have my microUSB power supply at hand. Thanks for looking out though image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to screamingtiger

    Joey,

     

    I have not yet investigated in depth (but I have received just not the news that my order has been shipped from UK of one of these stuff). One of the "secrects" is that these strips are controlled by one side by a specific chip that is I suppose the one that manage the entire lighting system. This implies also that these are not only a LEDs strip like the Christmas tree lights but something more sophisticated with signals on a flat circuit and some resistore here and there image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>