Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Sci Fi Your Pi: PiDesk - Guide: Magic Lamp with wireless charger, Adafruit Trinket & NeoPixels
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 21 Jun 2015 5:36 PM Date Created
  • Views 3199 views
  • Likes 7 likes
  • Comments 17 comments
  • design_challenge
  • touch_motion_controls
  • touch_motion_control
  • sci_fi_your_pi
Related
Recommended

Sci Fi Your Pi: PiDesk - Guide: Magic Lamp with wireless charger, Adafruit Trinket & NeoPixels

fvan
fvan
21 Jun 2015

Concept

 

The idea for this little project is to have a lamp which can be turned on or off simply by moving it on a desk.

 

A wireless charging base is built into the desk's surface, and a circuit with microcontroller and LEDs gets powered wirelessly using the charging coil.

 

Components & Circuit


image

The electronic components used in this project are the following:

  • Adafruit Trinket 5V
  • Adafruit NeoPixel Ring with 12 LEDs
  • Qi Wireless Charger Base
  • Qi Wireless Charger Accept


The Qi Wireless Charger was bought on eBay for a couple of euros. According to the specs, it is capable of outputting 5V/1A, which should be more than sufficient for this simple circuit.Connecting everything together is simple:

  • the coil's positive terminal is connected to the Trinket & NeoPixel USB+/PWR pins
  • the coil's negative terminal is connected to the Trinket & NeoPixel GND pins
  • the Trinket's #0 pin is connected to the NeoPixel IN pin

 

Program & Testing


The Trinket is programmed using the Arduino IDE in order to animate the NeoPixel Ring. But before this can be done, the necessary libraries need to be installed.Adafruit already has excellent tutorials covering this on their learning system:

  • Adding support for Adafruit boards
  • Installing the NeoPixel library

 

Once the hardware is supported and the library installed, it is possible to program the Trinket. An example program is provided with the NeoPixel library, called "strandtest". This sketch cycles through different animations and colors and is perfect to understand how the NeoPixel Ring is being animated.

 

Below are some animated gifs (you may need to click to see the animation) showing a quick tests with the wireless charger first and then with the Trinket and NeoPixel Ring.

 

imageimage

 

Assembly & Demo

 

To hold the electronics, a simple housing is required. This can be done using a readily available container or can be custom created using cardboard, plastic, or even using 3D printing. I opted for the latter and created a simple hollow cylinder just big enough to hold all the parts. The wireless charger coil is at the bottom and the NeoPixel Ring at the top. I'm also using a crystal ball on top of the circuit to diffuse the light.

 

imageimage

 

I hid the wireless charger base in the desk's surface, under my cutting mat. When the circuit is placed above the charger, it lights up without requiring a wired power source. Magic.

 

imageimage

 

Because of the crystal ball sitting on top the NeoPixel Ring, some effects are also reflected on the ceiling, gradually changing color.

 

Video

 

The video below provides an overview from start to completion, to end with a demo of the magic lamp.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

  • Sign in to reply

Top Comments

  • sleuz
    sleuz over 11 years ago in reply to balearicdynamics +3
    Hi Enrico Thanks to Mark mcb1 making me aware of this interesting topic. I know that the WPC Consortium just released a higher specification for the qi-standard. You can now transmit/receive up to 15 Watt…
  • mcb1
    mcb1 over 11 years ago in reply to balearicdynamics +2
    Enrico I hadn't come across it until Simon Luez was nice enough to have a conversation about the Qi charger I then entered the Beyond The Phone ( http://www.element14.com/community/community/design-challenges…
  • fvan
    fvan over 11 years ago in reply to balearicdynamics +2
    Your wife is a toothbrush ?
Parents
  • mcb1
    mcb1 over 11 years ago

    Come on admit it....

    You really wanted that 90's disco thing with the light on the ceiling, and the desk has nothing to do with it.

     

    I can think of a couple of uses for embedded chargers  ...good idea.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    Me too Mark, my concern - as I am 100% ignorant on inductive chargers - is if this can work with higher powers or only for very low energy. I am fascinated by this method when I bought a super-cheap electrical toothbrush that charges wirelessly so it is totally waterproof.

     

    image Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago in reply to mcb1

    The delay is due to the Trinket not starting the program the first 10 seconds, checking if it is being programmed instead.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    Mark,

     

    despite that you are spending very bad words on my toothbrush, thank you for the very useful links.

     

    BTW I have a so intelligent toothbrush that he call me from the bath when it is more than 5 minutes after every meal! (or is my wife? Should investigate)

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago in reply to balearicdynamics

    Your wife is a toothbrush ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to fvan

    Great logic deduction! You are a genius. Ha

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sleuz
    sleuz over 11 years ago in reply to balearicdynamics

    Hi Enrico

     

    Thanks to Mark mcb1 making me aware of this interesting topic.

     

    I know that the WPC Consortium just released a higher specification for the qi-standard. You can now transmit/receive up to 15 Watt.

    They are also working on even higher powers as you can see in the video below for kitchen appliances. But this will take a bit more until it will be available.

     

    Hope this helps a little.

     

     

    Regards

    Simon

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sleuz
    sleuz over 11 years ago in reply to balearicdynamics

    Hi Enrico

     

    Thanks to Mark mcb1 making me aware of this interesting topic.

     

    I know that the WPC Consortium just released a higher specification for the qi-standard. You can now transmit/receive up to 15 Watt.

    They are also working on even higher powers as you can see in the video below for kitchen appliances. But this will take a bit more until it will be available.

     

    Hope this helps a little.

     

     

    Regards

    Simon

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to sleuz

    Tank you too Simon.


    Enrico