Smart Spaces Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Smart Spaces Design Challenge
  • More
  • Cancel
Smart Spaces Design Challenge
Forum NO connection to chips debug port on the MCXN236?
  • Forum
  • Projects
  • Info
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Smart Spaces Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 38 subscribers
  • Views 1434 views
  • Users 0 members are here
  • FRDM MCXN236
Related

NO connection to chips debug port on the MCXN236?

skruglewicz
skruglewicz 11 months ago

I’m still having problems with the MCXN236 . Can't find the probe 

CONSOLE log:

LinkServer RedlinkMulti Driver v25.6 (Jun 26 2025 19:34:05 - crt_emu_cm_redlink build 1017)
Found chip XML file in C:/nxp/workspace/frdmmcxn236_hello_world/Debug\MCXN236.xml
( 5) Remote configuration complete
Reconnected to the existing LinkServer process.
Connecting to probe 2 core 0 (using server started externally) reports:
'Ee(42). Could not connect to core.'
Retrying...
Reconnected to the existing LinkServer process.
Server OK but no connection to probe 2 core 0 (after 3 attempts) - Ee(42). Could not connect to core.
Failed on connect: Ee(42). Could not connect to core.
No connection to chip's debug port

image

 I'm dead in the water with the MCXN236 and can not develop my project without it Does any one know why thus is happening? Is my board defective? 

any help here would be appreciated.

Thanks 

Steve K

  • Sign in to reply
  • Cancel

Top Replies

  • skruglewicz
    skruglewicz 10 months ago +3 verified
    UPDATE STATUS on the problem Success What was the reason? Turns out there were multiple versions of the MCU-Link firmware on my troubled PC. And as I found two Common Causes of Persistent Debugging…
  • skruglewicz
    skruglewicz 11 months ago +2
    skruglewicz said: I’m still having problems with the MCXN236 . Can't find the probe CONSOLE log: LinkServer RedlinkMulti Driver v25.6 (Jun 26 2025 19:34:05 - crt_emu_cm_redlink build 1017) Found…
  • balajivan1995
    balajivan1995 11 months ago +1
    1. Close every other projects, and select debug option. 2. Sometimes the IDE will hang trying to open the linkserver. In that case, close the IDE, locate the axf or hex file and flash it using standalone…
Parents
  • skruglewicz
    0 skruglewicz 11 months ago
    skruglewicz said:

    I’m still having problems with the MCXN236 . Can't find the probe 

    CONSOLE log:

    LinkServer RedlinkMulti Driver v25.6 (Jun 26 2025 19:34:05 - crt_emu_cm_redlink build 1017)
    Found chip XML file in C:/nxp/workspace/frdmmcxn236_hello_world/Debug\MCXN236.xml
    ( 5) Remote configuration complete
    Reconnected to the existing LinkServer process.
    Connecting to probe 2 core 0 (using server started externally) reports:
    'Ee(42). Could not connect to core.'
    Retrying...
    Reconnected to the existing LinkServer process.
    Server OK but no connection to probe 2 core 0 (after 3 attempts) - Ee(42). Could not connect to core.
    Failed on connect: Ee(42). Could not connect to core.
    No connection to chip's debug port

    image

     I'm dead in the water with the MCXN236 and can not develop my project without it Does any one know why thus is happening? Is my board defective? 

    any help here would be appreciated.

    Thanks 

    Steve K

    I am currently facing a critical and complete standstill in my project development due to a severe and unresolved issue with the MCXN236 device. To be absolutely clear, this development board or component is entirely non-functional; it is, in effect, a useless brick. All attempts to utilize the device have failed, rendering it completely unusable for its intended purpose. Consequently, I am dead in the water, as the lack of a working MCXN236 has created an insurmountable bottleneck, making any further progression on my project impossible until this fundamental hardware issue is resolved. This is not a minor setback; the device is fundamentally broken and cannot be leveraged for any stage of my necessary development work.

    Here are the four troubleshooting steps I attempted to fix the "No connection to chip's debug port" error with your NXP FRDM-MCXN236 board, along with the reported status for each:

    #

    Task

    Details from Document

    Status

    1

    Close every other project, and select the debug option.

    This step was an initial suggestion to prevent the IDE/LinkServer from hanging or conflicting.

    Attempted, no luck.

    2

    Standalone Flash Tool (LinkFlash)

    Used the LinkFlash utility found in the LinkServer folder of the MCUXpresso installation, including running the command ./LinkServer gui maint.

    Did NOT work. Same Ee(42). Could not connect to core. error.

    3

    Update the firmware

    Both the ISP Jumper Method (A) and the Jumper-less Method (B) (using MCUXpresso IDE v11.10+) were attempted for the MCU-Link debug probe firmware update.

    Did NOT work.

    4

    Boot/ISP jumper using SW3

    Attempted to enter ISP/Bootloader Mode on the FRDM-MCXN236 using the correct button sequence (hold SW3, hold RESET, reconnect USB, release RESET, release SW3) to allow for mass erase or recovery.

    Did NOT work either.

    The persistent error across all attempts was: Ee(42). Could not connect to core. and No connection to the chip's debug port.


    Thanks balajivan1995 or all your suggestions, but unfortunately your suggestions di not fix the problem. 

    I'm closing my question but the debug Probe is still not working. I cannot use the board. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • skruglewicz
    0 skruglewicz 11 months ago
    skruglewicz said:

    I’m still having problems with the MCXN236 . Can't find the probe 

    CONSOLE log:

    LinkServer RedlinkMulti Driver v25.6 (Jun 26 2025 19:34:05 - crt_emu_cm_redlink build 1017)
    Found chip XML file in C:/nxp/workspace/frdmmcxn236_hello_world/Debug\MCXN236.xml
    ( 5) Remote configuration complete
    Reconnected to the existing LinkServer process.
    Connecting to probe 2 core 0 (using server started externally) reports:
    'Ee(42). Could not connect to core.'
    Retrying...
    Reconnected to the existing LinkServer process.
    Server OK but no connection to probe 2 core 0 (after 3 attempts) - Ee(42). Could not connect to core.
    Failed on connect: Ee(42). Could not connect to core.
    No connection to chip's debug port

    image

     I'm dead in the water with the MCXN236 and can not develop my project without it Does any one know why thus is happening? Is my board defective? 

    any help here would be appreciated.

    Thanks 

    Steve K

    I am currently facing a critical and complete standstill in my project development due to a severe and unresolved issue with the MCXN236 device. To be absolutely clear, this development board or component is entirely non-functional; it is, in effect, a useless brick. All attempts to utilize the device have failed, rendering it completely unusable for its intended purpose. Consequently, I am dead in the water, as the lack of a working MCXN236 has created an insurmountable bottleneck, making any further progression on my project impossible until this fundamental hardware issue is resolved. This is not a minor setback; the device is fundamentally broken and cannot be leveraged for any stage of my necessary development work.

    Here are the four troubleshooting steps I attempted to fix the "No connection to chip's debug port" error with your NXP FRDM-MCXN236 board, along with the reported status for each:

    #

    Task

    Details from Document

    Status

    1

    Close every other project, and select the debug option.

    This step was an initial suggestion to prevent the IDE/LinkServer from hanging or conflicting.

    Attempted, no luck.

    2

    Standalone Flash Tool (LinkFlash)

    Used the LinkFlash utility found in the LinkServer folder of the MCUXpresso installation, including running the command ./LinkServer gui maint.

    Did NOT work. Same Ee(42). Could not connect to core. error.

    3

    Update the firmware

    Both the ISP Jumper Method (A) and the Jumper-less Method (B) (using MCUXpresso IDE v11.10+) were attempted for the MCU-Link debug probe firmware update.

    Did NOT work.

    4

    Boot/ISP jumper using SW3

    Attempted to enter ISP/Bootloader Mode on the FRDM-MCXN236 using the correct button sequence (hold SW3, hold RESET, reconnect USB, release RESET, release SW3) to allow for mass erase or recovery.

    Did NOT work either.

    The persistent error across all attempts was: Ee(42). Could not connect to core. and No connection to the chip's debug port.


    Thanks balajivan1995 or all your suggestions, but unfortunately your suggestions di not fix the problem. 

    I'm closing my question but the debug Probe is still not working. I cannot use the board.