Smart Spaces Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Smart Spaces Design Challenge
  • More
  • Cancel
Smart Spaces Design Challenge
Forum NO connection to chips debug port on the MCXN236?
  • Forum
  • Projects
  • Info
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Smart Spaces Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 38 subscribers
  • Views 1434 views
  • Users 0 members are here
  • FRDM MCXN236
Related

NO connection to chips debug port on the MCXN236?

skruglewicz
skruglewicz 11 months ago

I’m still having problems with the MCXN236 . Can't find the probe 

CONSOLE log:

LinkServer RedlinkMulti Driver v25.6 (Jun 26 2025 19:34:05 - crt_emu_cm_redlink build 1017)
Found chip XML file in C:/nxp/workspace/frdmmcxn236_hello_world/Debug\MCXN236.xml
( 5) Remote configuration complete
Reconnected to the existing LinkServer process.
Connecting to probe 2 core 0 (using server started externally) reports:
'Ee(42). Could not connect to core.'
Retrying...
Reconnected to the existing LinkServer process.
Server OK but no connection to probe 2 core 0 (after 3 attempts) - Ee(42). Could not connect to core.
Failed on connect: Ee(42). Could not connect to core.
No connection to chip's debug port

image

 I'm dead in the water with the MCXN236 and can not develop my project without it Does any one know why thus is happening? Is my board defective? 

any help here would be appreciated.

Thanks 

Steve K

  • Sign in to reply
  • Cancel

Top Replies

  • skruglewicz
    skruglewicz 10 months ago +3 verified
    UPDATE STATUS on the problem Success What was the reason? Turns out there were multiple versions of the MCU-Link firmware on my troubled PC. And as I found two Common Causes of Persistent Debugging…
  • skruglewicz
    skruglewicz 11 months ago +2
    skruglewicz said: I’m still having problems with the MCXN236 . Can't find the probe CONSOLE log: LinkServer RedlinkMulti Driver v25.6 (Jun 26 2025 19:34:05 - crt_emu_cm_redlink build 1017) Found…
  • balajivan1995
    balajivan1995 11 months ago +1
    1. Close every other projects, and select debug option. 2. Sometimes the IDE will hang trying to open the linkserver. In that case, close the IDE, locate the axf or hex file and flash it using standalone…
Parents
  • skruglewicz
    +1 skruglewicz 10 months ago

    UPDATE STATUS on the problem 

    Success

    What was the reason?

    Turns out there were multiple versions of the MCU-Link firmware on my troubled PC. And as I found two Common Causes of Persistent Debugging Connection Failures may be the reason for persistent debugging problems:

    • Corrupted or Conflicting USB/Debug Drivers: Drivers (MCU-Link / CMSIS-DAP / WinUSB) on the original PC may be corrupted or conflicting. This can result from prior installations of probes from NXP, SEGGER, PE Micro, or others.
    • Stale LinkServer Instance or Configuration: The IDE may be repeatedly reusing a stale or mismatched LinkServer instance or configuration on the original PC. This allows the probe to enumerate, but the SWD connection to the target core never actually establishes.

    What I did to get it working without getting the Error.

    I went into add/remove programs and noticed there were 3 versions of the MCU-Link Firmware install on my PC
    Here is the program screen showing 3 versions!

    image

    I uninstalled all but
    Mcu-Llnk firmware V3.148
    MCUXpresso ID V25.6
    I didn't need the other tools.

    image

    Now debug does not get the error as I described and works all the time?
    SUCCESS !!! I'm back on track with debugging on the MCXN236

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • skruglewicz
    +1 skruglewicz 10 months ago

    UPDATE STATUS on the problem 

    Success

    What was the reason?

    Turns out there were multiple versions of the MCU-Link firmware on my troubled PC. And as I found two Common Causes of Persistent Debugging Connection Failures may be the reason for persistent debugging problems:

    • Corrupted or Conflicting USB/Debug Drivers: Drivers (MCU-Link / CMSIS-DAP / WinUSB) on the original PC may be corrupted or conflicting. This can result from prior installations of probes from NXP, SEGGER, PE Micro, or others.
    • Stale LinkServer Instance or Configuration: The IDE may be repeatedly reusing a stale or mismatched LinkServer instance or configuration on the original PC. This allows the probe to enumerate, but the SWD connection to the target core never actually establishes.

    What I did to get it working without getting the Error.

    I went into add/remove programs and noticed there were 3 versions of the MCU-Link Firmware install on my PC
    Here is the program screen showing 3 versions!

    image

    I uninstalled all but
    Mcu-Llnk firmware V3.148
    MCUXpresso ID V25.6
    I didn't need the other tools.

    image

    Now debug does not get the error as I described and works all the time?
    SUCCESS !!! I'm back on track with debugging on the MCXN236

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer