Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog A Very Compact Christmas Display - Part 045
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 5 Jan 2014 4:36 AM Date Created
  • Views 1819 views
  • Likes 1 like
  • Comments 11 comments
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • psoc_4200
  • compact_xmas_display
  • ws2811
  • smarter_life
  • camera
  • psoc
Related
Recommended

A Very Compact Christmas Display - Part 045

COMPACT
COMPACT
5 Jan 2014

A Floral Bokeh

image

 

Here is a picture of the Ring with white selected.

 

The following are self portraits done using the Light Ring without the flash enabled and with the camera hand held.

 

image

With the first attempt you can see the reflection from the Light Ring.

 

imageimage

 

With the second and third attempts I have bokeh. http://en.wikipedia.org/wiki/Bokeh

Deliberate and artistic bluring (Well not really.)

I now need to invest in a decent Macro Lens or adapter and make a diffuser for the Light Ring for better close ups.

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 12 years ago in reply to DAB +1
    DAB You are right, and I used to think that lens worked well from their lowest to their highest aperture until I read this. http://www.kenrockwell.com/nikon/50-comparison/f-stops.htm He has some other…
Parents
  • vsluiter
    vsluiter over 12 years ago

    Interesting discussion!

    I used to have a Canon Powershot which had great macro focus (~1cm!!). I now have a Olympus PEN E-P3, which is great for most stuff, but not for macro with its stock lens (14-42mm Zuiko). I tried to reverse mount a Pentax lens (with 49mm-reverse to Micro4/3 converter), but because the focal distance is shorter, it didn't magnify enough. In the end I bought close-up filters, which give a reasonable result. One of the benefits is that the lens doesn't get in the way of the flash. And indeed, I normally use some white cardboard to reflect the flash.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vsluiter
    vsluiter over 12 years ago

    Interesting discussion!

    I used to have a Canon Powershot which had great macro focus (~1cm!!). I now have a Olympus PEN E-P3, which is great for most stuff, but not for macro with its stock lens (14-42mm Zuiko). I tried to reverse mount a Pentax lens (with 49mm-reverse to Micro4/3 converter), but because the focal distance is shorter, it didn't magnify enough. In the end I bought close-up filters, which give a reasonable result. One of the benefits is that the lens doesn't get in the way of the flash. And indeed, I normally use some white cardboard to reflect the flash.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 12 years ago in reply to vsluiter

    Victor

    Adding filters is a very cheap way to get results, nut anything you add removes or reduces the lens sharpness, etc.

    Proper extension tubes or proper lens reverse rings don't reduce the lens performance, but as you found need to be for that combination.

     

    I haven't tried my reverse adapter on the 3100/3200, but I did on earlier film camera with fantastic results.

     

    I don't bother with the camera flash for anything macro. I either use natural light (with long exposure if necessary) or a remote flash.

    You can buy flashes very cheap (or do what Monte has done with leds) that you can use external to the camera.

     

    Mark