Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog PSoC 4 Tricopter (Smarter Life Challenge) part #11
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yuritikhonov
  • Date Created: 3 Jan 2014 3:20 PM Date Created
  • Views 1514 views
  • Likes 2 likes
  • Comments 5 comments
  • RoadTest
  • tricopter
  • psoc4
  • Multiwii
  • smarter_life_challenge
  • smarter_life
  • smart_tricopter
  • smart_control_and_diagnostics
  • arduino
  • quadcopter
Related
Recommended

PSoC 4 Tricopter (Smarter Life Challenge) part #11

yuritikhonov
yuritikhonov
3 Jan 2014

If you like my project vote for "A Smarter Tricopter - Yuri Tikhonov" image

 

Happy New Year and Merry Cristmas!

image

What was done over the past few days:

  • hidden power wiring was set (real puzzle...)
  • ESC's were set, connected and tuned.
  • Rx & LiPo (temporarily on plastic clamps) were set.
  • software for PSoC 4 was modified, now it "works fine on the machine".

 

Slight difficulty with ESC was the next: after soldering it turned out that one of the motors rotated in the wrong direction, good still, that ESCs of "HobbyKing BlueSeries" support software change for direction of rotation. Now motors rotate like this:

image

Mounted ESC:

image

After all wiring installation I got a nasty surprise: PSoC burned out! Probably I fused something and the smoke poured from the board! However, I was not upset: as you know from post #2, I ordered 4pcs PSoC 4 in LQFP package, so the board was brought back to life.

image

During setup of the firmware, the servo suddenly stopped working! Judging by the sound the engine was working, but not the drive shaft. The problem was quite exotic: I applied to the input of the servo a "specific" signal, which cranked the gear! After dismantling the drive and installing the gear in place, the drive started to work again image

image

And then flashed an evil thought: what about running the tricopter at home!! And why not? Basically everything works, the control system behaves exactly as I wanted, the unit is assembled,  the motors are spinning. I put the propellers in place, started engines and ... I stopped. Oh, no! I can not suddenly destroy the machine,  in which I invested so much time, effort and soul!


You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

So, it was decided to postpone the launch until after the holidays, during this time I want to fully test and calibrate all unit systems . Also, to run the machine at home is very dangerous: dimensions of the device 100x90cm, sharp propellers 25cm each rotate at >12000rpm, this is not a joke. Safety first!

 

The next post will be likely the final, I can not believe, how quickly time flies Only yesterday the unit was not yet even in my thoughts and here today it is already waiting in the wings.

 

See you soon, comrades!

                                                                                                                                              

#linkdescription
1PSoC 4 Tricopter Part #1Introduction
2PSoC 4 Tricopter Part #2Purchase of components from Farnell and HobbyKing
3PSoC 4 Tricopter Part #3PSoC firmware: upTime & Rx
4PSoC 4 Tricopter Part #4PSoC firmware: UART & MultiWii GUI
5PSoC 4 Tricopter Part #5PSoC firmware: EEPROM emulation
6PSoC 4 Tricopter Part #6PSoC firmware: Servo & ESC control
7PSoC 4 Tricopter Part #7PSoC firmware: IMU, LED's & PID
8PSoC 4 Tricopter Part #8Hardware: PCB
9PSoC 4 Tricopter Part #9Hardware: tricopter's frame
10PSoC 4 Tricopter Part #10Hardware: YAW mechanics & motors
11PSoC 4 Tricopter Part #11Hardware: ESC's, wires & misc
12PSoC 4 Tricopter Part #12Final: The first fly

 

If you like my project vote for "A Smarter Tricopter - Yuri Tikhonov" image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    Hi Yuri, Good update. It looks like you are ready for test flights outdoors, so I look forward to seeing your creation fly in the sky. DAB
  • DAB
    DAB over 12 years ago in reply to yuritikhonov +1
    Yes, it is always a stressful time to see your baby take flight into the wild open skies. Just keep your faith and take as many precautions as you can. No matter what happens, you did a very good job on…
  • vsluiter
    vsluiter over 12 years ago +1
    I've never done anything with flying hardware, but I can understand your eagerness to start flying! For me, it wouldn't be the first time to ruin something by going too fast, and not overthinking stuff…
Parents
  • vsluiter
    vsluiter over 12 years ago

    I've never done anything with flying hardware, but I can understand your eagerness to start flying!

    For me, it wouldn't be the first time to ruin something by going too fast, and not overthinking stuff first. Very good of you to take precautions...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yuritikhonov
    yuritikhonov over 12 years ago in reply to vsluiter

    Thanks for you comment Victor! I have compiled a list of problems and now I am struggling with them! When I can be sure that my tricopter ready to fly, then we will fly into the skyimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • yuritikhonov
    yuritikhonov over 12 years ago in reply to vsluiter

    Thanks for you comment Victor! I have compiled a list of problems and now I am struggling with them! When I can be sure that my tricopter ready to fly, then we will fly into the skyimage