Start a Movement Challenge
  • Challenges & Projects
  • Design Challenges
  • Start a Movement Challenge
  • More
  • Cancel
Start a Movement Challenge
Forum RangeDetect Rover 1# Unboxing and Roadtest to TMC5272-EVAL-KIT and TRINAMIC stepper motor
  • Blog
  • Forum
  • Projects
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Start a Movement Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 47 subscribers
  • Views 522 views
  • Users 0 members are here
Related

RangeDetect Rover 1# Unboxing and Roadtest to TMC5272-EVAL-KIT and TRINAMIC stepper motor

fyaocn
fyaocn over 1 year ago

1# Roadtest to TMC5272-EVAL-KIT and TRINAMIC stepper motor

Table of Contents

  • 1 Introduction 
  • 2 TMC5272-EVAL-KIT and TRINAMIC stepper motor
  • 3 TMCL-IDE
  • 4 Drive the stepper motor and Next to do

1 Introduction 

The TMC5272 is a Step/Dir Driver for Two-Phase Bipolar Stepper Motors up to 0.8 A (RMS) (1.12 A (PEAK)).  TMC5272-EVAL-KIT and  Landungsbruecke with with bridge Board can run with TMCL-IDE to rest the performance and function of the TMC5272. One RINAMIC Stepper Motor, Single Shaft, Hybrid, 42 mm, Bipolar, 1.8 °, 27 N-cm, 1 A is used as stepper motor in this road test.

Refer to TMC5272-EVAL Evaluation Board | Analog Devices and LANDUNGSBRUECKE Evaluation Board | Analog Devices for more details.

image

2 TMC5272-EVAL-KIT and TRINAMIC stepper motor

The TMC5272-EVAL allows evaluation of the TMC5272 in combination with the ADI TRINAMIC evaluation board system, or as a stand-alone board. It uses the standard schematic and offers several options in order to test different modes of operation. The TMC5272 is a Step/Dir Driver for Two-Phase Bipolar Stepper Motors up to 0.8 A RMS (1.5 A peak). The board is full functions with high performance and easy control. With features as,
CoolStepTm
Passive Braking
Short Detection
Slope Control
StallGuard2Tm
MicroPlyerTm
DcStepTm
Position Mode
Velocity Mode
Dual Encoder
2x 2-phase stepper motor up to 0.8 A (RMS) coil current (1.12 A (PEAK))
Supply Voltage 2.1 to 20 V DC
SPI and Single Wire UART
Encoder Interface with alt. functions
1 to 256 microsteps
StealthChop2 silent PWM mode
StallGuard4 sensorless motor load detection
TriCoder Sensorless Standstill Steploss Detection and Full Step Encoder

There functions are good for smooth  and precise control for high end tasks in industrial, medical and consumer products.

image

And this the parameter and function for this stepper motor.

image

3 TMCL-IDE

TMCL-IDE  is best used in this road test and help understanding the how the above features works. The hardware is configurated below, one pink clipper on the shaft can show how the stepper motor runs.

image

This the short video for the stepper motor in velocity mode,

image

Start the TMCL-IDE, 

image

if the board is not automatic recognized, manually select it. or it is in direct mode only

image

The board connect the TMIC-IDE in serial port, all function is opened for roadtest,

image

Here is settings, the drive board is unknown, so manually selected as well.

image

update the firmware for driver board first,

image

wait until if completed successfully.

imageimage

All the function can be control and traced in registers,

image

Functions in GUI for easy control 

image

IN direct mode, the registers are read or write directly for fast control

image

Now connect and plug 12V DC power, the ADC readings show the input voltages and some info.

image

adjust the reference current setting to make the calibration button green. In this case the settings is 0.1A

image

The feedback current sensing shows 0.1A as well,

image

For advance control in coolsteps and stallGuard

image

Square PWM waveform is normally used, and it can be configurated in sinus mode as this part shows,

image

The stepper motor can be controlled in position mode or velocity mode, 256 steps per round and the position is defined in steps

image

Here is the control GUI

image

this is velocity mode GUI

image

The velocity can be controlled as smooth as it can be , change the number or simple pull the virtual button, feel how the TMC5272 drive the stepper motors.

image

4 Drive the stepper motor and Next to do

This roadtest is easy and pleasant, try the TMCL-IDE with reading the reference manual. High performance of TMC5272 can easily be found out. My proposal is drive the rover with stepper motor, in fact , it can be more fit for precise control in millimeters or even smaller. Next step shall be build the rover and setting the range detect sensors.

 

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 1 year ago

    Looks straight forward.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 1 year ago

    Looks straight forward.